RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Help us select RoadTest kits
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 73 replies
  • Subscribers 2766 subscribers
  • Views 6739 views
  • Users 0 members are here
  • RoadTest
  • international
  • rectifier
  • freescale
  • matrix
  • avago
  • development
  • ir
  • maxim
  • national
  • hawkboard
  • kits
Related

Help us select RoadTest kits

awinning
awinning over 16 years ago
Hi,

We'd like to hear your thoughts on dev kits in the market just now. What  kits interest you, or would you maybe like to see on future RoadTests?  Are there any other type of products you'd like to see on RoadTest?  (before anyone suggests, there's no chance of an iPad appearing in the  near term future image )

To get the conversation started we've pasted 9 possible kits below. Tell  us which of these interest you the most and why? As a disclaimer, I'm  not promising to give away the most popular, but we'll certainly talk to  the manufacturers and your views will help us greatly!


1. National Semiconductor’s LM26420 evaluation board demonstrates the  company's LM26420 based solution.

2. International Rectifier's IRS2540 IRS2540/1 buck converter based  development board helps develop HB-LED applications

3. ST's STM3210E-SK/HT helps start development for the company's ARM  core-based microcontrollers.

4. Maxim's MAX9830A evaluation kit uses a filterless class D amplifier to  drive a mono bridge-tied-load speaker.

5. Matrix Multimedia's EB018 E-blocks CAN bus board allows investigation  of the CAN bus protocol.

6. Avago's HFBR-0410HFBR-0410 fiber optics evaluation kit allows first hand  experience with simple DC to 5MBd TTL compatible components.

7. Freescale's RD1986MMA2260DRD1986MMA2260D TRIAX 3-axis acceleration sensing demo  board combines demos available for accelerometer applications.

8. Microchip’s DM183026 mTouch capacitive evaluation kit helps develop  touch sense applications using PIC16F or PIC24F MCUs.

9. Innovate Software Solutions Hawkboard is an open community board with a  feature set based on the TI OMAP L138 processor.
  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 16 years ago

    Hello,

     

    as was previously mentioned FPGA is the technology we would like to evaluate, but it is not so easy to do some board by yourself. Mainly because of FPGA manufacturer  obsession of GPIO pin number. Almost all devices are in BGA case style.

     

    I see a big potential with a connection FPGA core together with MCU core (Cortex-M3 as a best choice).

     

    There are two devices I would like to see in Road Test:

     

    1) Actel's SmartFusionTm Evaluation Kit

    http://www.actel.com/products/hardware/devkits_boards/smartfusion_eval.aspx

     

    2) Cypress PSoC 5 (when it will be released)

    http://www.cypress.com/?id=2233

     

    I know PSoC isn't exactly the same thing as I've described above, but it is similar and also interesting.

     

     

    W.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 16 years ago

    Hello,

     

    as was previously mentioned FPGA is the technology we would like to evaluate, but it is not so easy to do some board by yourself. Mainly because of FPGA manufacturer  obsession of GPIO pin number. Almost all devices are in BGA case style.

     

    I see a big potential with a connection FPGA core together with MCU core (Cortex-M3 as a best choice).

     

    There are two devices I would like to see in Road Test:

     

    1) Actel's SmartFusionTm Evaluation Kit

    http://www.actel.com/products/hardware/devkits_boards/smartfusion_eval.aspx

     

    2) Cypress PSoC 5 (when it will be released)

    http://www.cypress.com/?id=2233

     

    I know PSoC isn't exactly the same thing as I've described above, but it is similar and also interesting.

     

     

    W.