Products
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
RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Review : PICKit 3 evaluation kit.
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 16 replies
  • Subscribers 2755 subscribers
  • Views 2991 views
  • Users 0 members are here
Related

Review : PICKit 3 evaluation kit.

e14 Contributor
e14 Contributor over 16 years ago

I receivemy Pickit 3 evaluation kit some days ago.
After open the UPS box, can I also inspect this kit.
It is composed by one Microchip Pickit3 programmer/Debugger, some PICs MCUs, one PIC18F46J50 USB Demo Board
and one supplementary 18F48K20 nanoWatt XLP Demo board.
3 CDs comes also with all software and documentation need to start "playing" with this kit.

 

image

First test, Open my allready installed MPLAB, open the Generic HID custom demo, compile an connect the Pickit3 to the PIC18F46J50 USB Demo Board.
Programming is very fast and I can test this board in less than 3 minutes.

 

Second test, trying to programm 18F48K20 nanoWatt XLP Demo board. Looking in CD for samples programms, (also found in a zip file),
I also found one tutorial for programming this board with Pickit3.
Reading, erasing and checking this board is Ok, but programming seems to be impossible. One question on the Microchip forum
and I got the solution : MPLAB v8.43 (the version I have allready installed isn't compatible with this  board).
Download and install the last version. All running fine.

 

Actually, I read the "PICkit_3_lessons_UG41370c.pdf" and learn using the MCUs and PICKit3.
Lessons are very clear and progressive, programming and debugging are well explain.
I'm currently testing interrupt, so I'll have to update this review next time I progress.

  • Sign in to reply
  • Cancel
Parents
  • icserny
    icserny over 16 years ago

    Hi!

     

    I would like to know how useful the PICkit3 device is in the development. Does it have any utility program like PICkit2 which can be used as a Logic Tool, Logic analyzer and UART communication tool as well?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • icserny
    icserny over 16 years ago

    Hi!

     

    I would like to know how useful the PICkit3 device is in the development. Does it have any utility program like PICkit2 which can be used as a Logic Tool, Logic analyzer and UART communication tool as well?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • YT2095
    YT2095 over 14 years ago in reply to icserny

    I must be really rather Dull and Boring, I`v only ever used my PICKIT2 for programming and rarely to never use MPLAB unless I need to optimise some code to try and steal back a little Memory space.

    so naturally I`m intruiged to hear that this little black box can do so much more!

    does anyone have a few Links where I can learn more about this, it sounds like the basis for a good tinkering session on a cold winters evening that I can add to my list.

     

    Cheers image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • billabott
    billabott over 14 years ago in reply to icserny

    I don't know, but I have to believe that it does.  Anyway my good friends here at element14 gave me a special gift of a PICKIT 2 a short while ago and I just started learning about its abilities.  I have been looking at the YouTube videos made by kdarrah1234.  He is fantastic and I am amazed at this device.  His presentation about PICKIt 2  Logic Tool Overview shows how to use the logic tool feature while it is connected to an arduino.  Now I can see its usefulness and great value for any microprocessor circuit.  Outstanding!