Products
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
RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Review : PICKit 3 evaluation kit.
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 16 replies
  • Subscribers 2755 subscribers
  • Views 3002 views
  • Users 0 members are here
Related

Review : PICKit 3 evaluation kit.

e14 Contributor
e14 Contributor over 16 years ago

I receivemy Pickit 3 evaluation kit some days ago.
After open the UPS box, can I also inspect this kit.
It is composed by one Microchip Pickit3 programmer/Debugger, some PICs MCUs, one PIC18F46J50 USB Demo Board
and one supplementary 18F48K20 nanoWatt XLP Demo board.
3 CDs comes also with all software and documentation need to start "playing" with this kit.

 

image

First test, Open my allready installed MPLAB, open the Generic HID custom demo, compile an connect the Pickit3 to the PIC18F46J50 USB Demo Board.
Programming is very fast and I can test this board in less than 3 minutes.

 

Second test, trying to programm 18F48K20 nanoWatt XLP Demo board. Looking in CD for samples programms, (also found in a zip file),
I also found one tutorial for programming this board with Pickit3.
Reading, erasing and checking this board is Ok, but programming seems to be impossible. One question on the Microchip forum
and I got the solution : MPLAB v8.43 (the version I have allready installed isn't compatible with this  board).
Download and install the last version. All running fine.

 

Actually, I read the "PICkit_3_lessons_UG41370c.pdf" and learn using the MCUs and PICKit3.
Lessons are very clear and progressive, programming and debugging are well explain.
I'm currently testing interrupt, so I'll have to update this review next time I progress.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 16 years ago

    I installed the mplab - with option install all - from the disc and connected the pickit3 and demoboard, but in mplap there was an error message that the device where not found.

    So I downloaded and installed the latest version off mplab from Microchip homepage. Still got the same error - solution one has to turn on the power for the demoboard to be recognized. Next step was testing the tutorial lessons. Now I found the C-compiler missing. After a search on Microchips homepage - the link on the disc did not work- I downloaded and installed a demo of MCC18. Trying to comlpete lesson 1 LED i discovered that there only is one type off header file - the tutorial is made for older version. When trying to run build all I keep getting this error

    Error - could not find file 'c018i.o'. The file is in its apropriate directory, and all envirement variables are set properly. Has any one got a clue ?

     

    Carsten Doerwald

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago in reply to e14 Contributor

    Hello,

     

    Could you check the linker path ?

    Do you have selected the good .lkr file for your PIC

     

     

    Have you set all directories in the project settings ?

     

    I've take a look tonight.

     

    Regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago in reply to e14 Contributor

    Finally got it working. Had to add directory and search path manualy in:  build options for project "lesson 1 led" in project menu.

     

    Have a nice week end

     

    Carsten Doerwald

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • MicrochipRTCfr
    MicrochipRTCfr over 16 years ago in reply to icserny

    Hi,

     

    The Pickit3 should gradually have the same utilities as the Pickit2 image.

    Make sure you always have the latest firmware (Pickit3 homepage).

    Actually most of the time installing a new MPLAB version might also update your Pickit3 to add some features.

     

    regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • icserny
    icserny over 16 years ago in reply to e14 Contributor

    Hi Carstein,

     

    You can set the default search path & directories permamently by using the Project/Set Language Tool Locations menu point.

     

    For the Microchip C18 Toolsouite you should set the Include, Library and Linker-Script search paths and directories.

     

    Regards: István Cserny

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago in reply to e14 Contributor
    Carsten, could you drop me an email on this product.  I would like to check it out.  why did you have to add directory and search path?
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 16 years ago in reply to e14 Contributor
    Carsten, could you drop me an email on this product.  I would like to check it out.  why did you have to add directory and search path?