RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Review : PICKit 3 evaluation kit.
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 16 replies
  • Subscribers 2760 subscribers
  • Views 2964 views
  • Users 0 members are here
Related

Review : PICKit 3 evaluation kit.

e14 Contributor
e14 Contributor over 16 years ago

I receivemy Pickit 3 evaluation kit some days ago.
After open the UPS box, can I also inspect this kit.
It is composed by one Microchip Pickit3 programmer/Debugger, some PICs MCUs, one PIC18F46J50 USB Demo Board
and one supplementary 18F48K20 nanoWatt XLP Demo board.
3 CDs comes also with all software and documentation need to start "playing" with this kit.

 

image

First test, Open my allready installed MPLAB, open the Generic HID custom demo, compile an connect the Pickit3 to the PIC18F46J50 USB Demo Board.
Programming is very fast and I can test this board in less than 3 minutes.

 

Second test, trying to programm 18F48K20 nanoWatt XLP Demo board. Looking in CD for samples programms, (also found in a zip file),
I also found one tutorial for programming this board with Pickit3.
Reading, erasing and checking this board is Ok, but programming seems to be impossible. One question on the Microchip forum
and I got the solution : MPLAB v8.43 (the version I have allready installed isn't compatible with this  board).
Download and install the last version. All running fine.

 

Actually, I read the "PICkit_3_lessons_UG41370c.pdf" and learn using the MCUs and PICKit3.
Lessons are very clear and progressive, programming and debugging are well explain.
I'm currently testing interrupt, so I'll have to update this review next time I progress.

  • Sign in to reply
  • Cancel
  • cteixeira
    cteixeira over 14 years ago in reply to YT2095

    YT2095 Has you can see more and more people like the pickit2  image ... You cannot make lot of things, but is cheap and do the job. With that you can programm almost all the Pic familie and debug them.

    I tested the ICD2 and it is very slow comparing with the pickit2, and the connectors are just made for it... unlike pickit2 it mini USB and the 6 pin header...

     

    I just used this with MPLAB, two times... after that just pickit2 tool to programm/erase the microcontrollers and then command line in Linux or now... the MPLAB X IDE.. it is working and in Linux is running...

    Some additional tools have been develloped, like the scope or comunication analyser for pickit2, I never use them but I think it is a plus... you bought an programmer and you can use that like an simple scope.

     

    I ask to compare the version 3 vs version 2, because when Microchip launch the Pickit 3, the new features just are:

     

    Habilitity to programm one or two new families;

    Speed in programming;

     

    Any of them when they lauch this to the market are enough or make me change my version 2 to the new one... and from the lastest comments, I can see pickit3 still have some problems/ or complications against the previous version.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • nermash
    nermash over 14 years ago in reply to pjclarke

    I think that they are using bootloader in the mcu inside which doesn't get overwriten on fw updates, thus enabling easy recovery from fw update disasters? At least on PICKIT2...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • pjclarke
    pjclarke over 14 years ago in reply to YT2095

    The PICKit3 is slowly becoming more and more like the PICKit2. There is now a command line tool which is usefull for production automated programming as well as a PICKit3 Scripting tool that turns the PICKit 3 into a sort of PICKit2.

     

    This new tool allows you to use the same looking PICKit2 programmer and has things like the Logic tool. The UART tool is not available as yet however Microchip are adding this soon. How long soon is I don't know but the UART is on the tools menu.

     

    I'm using the new script type tool now in my own production area without problems.

     

    I think the only issue I have with the PICKit3 is that in MPLAB when switching between families of chips it still has to download new firmware unlike on the PICKit2 - a step backwards in my view that leaves the unit open to getting damaged firmware (and had happen).

     

    Paul

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • YT2095
    YT2095 over 14 years ago in reply to icserny

    I must be really rather Dull and Boring, I`v only ever used my PICKIT2 for programming and rarely to never use MPLAB unless I need to optimise some code to try and steal back a little Memory space.

    so naturally I`m intruiged to hear that this little black box can do so much more!

    does anyone have a few Links where I can learn more about this, it sounds like the basis for a good tinkering session on a cold winters evening that I can add to my list.

     

    Cheers image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • cteixeira
    cteixeira over 14 years ago

    If you can compare the pickit3 with pickit2 would be awesome... I own an pickit2 and I like it it does the job... program/ debug / and like billabott said, Logic tool overview is an extra very useful.

    So if you can describe any extra feature pickit3 has more than pickit2 I would appreciate.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • WiteTigr
    WiteTigr over 14 years ago in reply to billabott

    Yes I just reviewed the videos you suggested and you are right he is very informative.  I especially like how he gets "off subject" and shows a couple of other "features" that it can do as well.  That is just what we need to know.  Thanks for the information!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • billabott
    billabott over 14 years ago in reply to icserny

    I don't know, but I have to believe that it does.  Anyway my good friends here at element14 gave me a special gift of a PICKIT 2 a short while ago and I just started learning about its abilities.  I have been looking at the YouTube videos made by kdarrah1234.  He is fantastic and I am amazed at this device.  His presentation about PICKIt 2  Logic Tool Overview shows how to use the logic tool feature while it is connected to an arduino.  Now I can see its usefulness and great value for any microprocessor circuit.  Outstanding!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago

    Hi is this kit up for review?

     

    If it is, I would love to get my hands on it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • MicrochipRTCfr
    MicrochipRTCfr over 16 years ago in reply to icserny

    Hi,

     

    The Pickit3 should gradually have the same utilities as the Pickit2 image.

    Make sure you always have the latest firmware (Pickit3 homepage).

    Actually most of the time installing a new MPLAB version might also update your Pickit3 to add some features.

     

    regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • icserny
    icserny over 16 years ago in reply to e14 Contributor

    Hi Carstein,

     

    You can set the default search path & directories permamently by using the Project/Set Language Tool Locations menu point.

     

    For the Microchip C18 Toolsouite you should set the Include, Library and Linker-Script search paths and directories.

     

    Regards: István Cserny

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>