Products
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
RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Hawkboard - first look
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 2751 subscribers
  • Views 652 views
  • Users 0 members are here
Related

Hawkboard - first look

michaelkellett
michaelkellett over 16 years ago

Several members of this group suggested the hawkboard as a roadtest candidate.

 

Since I have just bought one I can give my first impressions.

 

What you get is the board and the cardboard box -  no disc, no documentation (none at all !!!!!!!).

 

The board design looks OK but beware quality - mine has a tombstoned capacitor (C108) near the VGA connector - its pretty obvious so it means that the board was not optically inspected after assembly which is worrying. This cap is connected to a pin called "comp" on the LCD/VGA video controller.

 

I don't know if the VGA/LCD works because:

 

You have to go and trawl on the web for any information at all and there is very little user experience. I found no reference to step by step how to connect an LCD display, a SATA drive etc.

 

There is no obvious way of making the board do anything much. It has some kind of linux loaded but it isn't easy to work out what from the stuff on the web. If you connect a terminal via the RS232 port it boots up a linux - no doubt if you are expert with this the mass of start up info will mean something to you. My next step is to connect a hard drive because it seems to try and make the SATA port work. It is not obvious to me that it has any video drivers.

 

So my first impression is potentially nice board but....................

 

     without a proper manual and instructions it's not much use - I don't have time or inclination to reverse engineer what should come with it.

 

If any one has got further I would be very pleased to hear from them.

  • Sign in to reply
  • Cancel
Parents
  • michaelkellett
    michaelkellett over 16 years ago

    Update:

     

    The VGA does work - at least it shows a logo screen on power up and turns blue with penguins in the corners when Linux boots.

     

    I can't make it ping annother computer (i get a network unreachable error) - probably because I need to set the IP address and mask but I have no idea how.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcx
    mcx over 16 years ago in reply to michaelkellett

    Just wondering if you have heard of the BeagleBoard. It is a similar, but more powerful board with a bigger community.

     

    http://whatnicklife.blogspot.com/2010/03/dog-and-birds-hawkboards-and.html

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 16 years ago in reply to mcx

    The Beagleboard is nice but has no SATA port (and it costs more). It might still be the way to go but the project spec is still demanding a hard drive so I will need to persuade people that an SD card is OK instead.

     

    Thanks for the link to the Ubuntu install - I had seen the original that is referred to but the mods are interesting.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • michaelkellett
    michaelkellett over 16 years ago in reply to mcx

    The Beagleboard is nice but has no SATA port (and it costs more). It might still be the way to go but the project spec is still demanding a hard drive so I will need to persuade people that an SD card is OK instead.

     

    Thanks for the link to the Ubuntu install - I had seen the original that is referred to but the mods are interesting.