Products
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
RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum TDK-Lambda LS100-12 Review
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 2751 subscribers
  • Views 709 views
  • Users 0 members are here
  • tdk
  • review
  • lambda
Related

TDK-Lambda LS100-12 Review

danteo
danteo over 16 years ago

TDK-Lambda  LS100-12LS100-12

 

- Excellent housing and heatsnik, strong and easy to mount. Easy to open. Good cooling

- At  first look I thought I'll find something loose inside but was L6  and L8 - small ferrite rings.

- Good quality components (Rubycon MXG and YXH capacitors...)

- 3 year warranty

 

Some tests:

 

Param.Specs.Found
Out Voltage Range10,8-13,2v9,2-14,3v /4,5A
Load Regulation96mV100mV @ 8,6A, 10mV@4A
Short circuit testmax 30s5s, 10s .... ok

Noise:  with 8,5 - 5 - 4,5 - 3,5A no noise, with 110mA - some noise. Still searching...

 

A very good product at a fair price.

 

Thanks for ... opportunity and PSU.

  • Sign in to reply
  • Cancel
  • danteo
    danteo over 16 years ago

    After more than 1 month from the first power-on:

     

    - stable voltage

    - no excessive heat

    - no problems after short-circuits

    - no problems after long no-load time

     

    A good, reliable power source.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago

    I agree with Danteo. Good power supply at a fair price.

     

    I am away from home most of the time so I have been using it as a "portable" prototyping power supply for my personnal projects for about two weeks now. I take it with me in my suite case with the parts I need. It is pretty light weight for the rated output and came with a nice little box I use to protect it while travelling. The only thing is I don't have a portable oscilloscope si I didn't check the load regulation. I am working on a project with microcontrollers and power LEDs so the 8,5 amp capacity is very interesting. I didn't take it to more than 2 amps yet, but I sure will!

     

    It makes it possible for me to work on projects I have been delaying for a long time because of the lack of time. For the price, I should have bought it before!

     

    Mario