RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum If you had a Altera Cyclone IV Dev Kit, what would you build?
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 44 replies
  • Subscribers 2762 subscribers
  • Views 4912 views
  • Users 0 members are here
Related

If you had a Altera Cyclone IV Dev Kit, what would you build?

awinning
awinning over 16 years ago

Hi,

 

As mentioned in the RoadTest for the DK-STRT-4CGX15N-0B Dev kit, we would like you to tell us what you would build if you had the opportunity. When the RoadTest closes I will choose a short list and create a poll for you to vote in. Winners of the poll will receive the kits,

 

Good Luck,

Ally

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 16 years ago

    Well, here's my idea...

     

    A couple of years ago I bought a pair of broken HP Laserjet III printers for scrap. One had a blown laser, the other had a fried power supply and a thick coating of disintegrated air filter all over its innards. I stripped them for spares, and the spares ended up in my "Quality Used Parts" box.

     

    Fast forward a few years, and I'm running a photo-lab at work (think "One Hour Photo"). The machine we're using is a Fuji Frontier, a massive hulk of a machine which uses three lasers to expose a sheet of photo paper, then processes it in RA-4 chemistry to produce a print. On one particularly slow day, I started thinking: what if I took the laser scanner off the Laserjet, bolted on a 405nm BluRay laser diode (instead of the infra-red diode the LJ3 uses as-standard), and used black and white photo paper (which is VERY sensitive to blue light). Could I build my own B&W printer (though obviously without the process chemistry -- I'd do the processing using developing trays)?

     

    This would involve:

      - Sending analog data (~12 bits per pixel) to the laser at around 30MHz

      - Keeping the scanner motor running at a fixed speed within a decent tolerance

      - Transferring data to/from a host PC or an SD Card

      - (possibly) JPEG decoding

      - LUT processing (applying a lookup table to the data sent to the laser in order to correct the black and white points)

      - Keeping track of where the sheet of paper is in the mechanism, and driving the three stepper motors accordingly

     

    No doubt there would be a lot of "fun" involved in making this work on a commercial MCU. In the LJ3, most of this sort of work was done by a set of microcontrollers and ASICs...

     

    Still, looks like a fun project. And definitely a candidate for a "weirdest project" award image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago in reply to e14 Contributor

    Phil, how about a 3D laser printer for acrylic cubes image

     

    So you would have 2 or 3 lasers that form a dot when all are aimed to the same spot but that they are not hot enough to do anything individually.

     

     

     

    Elias

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 16 years ago in reply to e14 Contributor

    Phil, how about a 3D laser printer for acrylic cubes image

     

    So you would have 2 or 3 lasers that form a dot when all are aimed to the same spot but that they are not hot enough to do anything individually.

     

     

     

    Elias