RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Upcoming events
  • Blogs
  • RoadTest Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 21 replies
  • Subscribers 2568 subscribers
  • Views 2120 views
  • Users 0 members are here
  • texas
  • microchip
  • freescale
  • instruments
  • stmicroelectronics
  • maxim
  • st
  • hawkboard
  • ti
  • agilent
Related

Upcoming events

awinning
awinning over 15 years ago

Hey guys,

 

I've been asked by a few of you to tell you what is coming up in advance. I can't give a precise calendar, because we wait till items are available to send before we run the events. There are a couple of products, which I am not sure are released yet...yeah, you could actually have dev kits at the time of release! In those cases I've blocked out the product name. There are also more products added ad hoc, so there may be some tests that are not on the calendar.

 

Basically don't shoot the messanger if these run late or if more products appear unexpectedly! image I'll try keep it updated as much as I can. You can also add suggestions in this thread. Hopefully there will be a few replies and updates here, so remember you can choose not to get email notification from the thread if you don't wish

 

Ally

 

Sep

 

NSC LED Buck Controller Eval. Board
ADI T045 RFIF
Maxim max2829evkit
Maxim max2830evkit
Austriamicrosystems AS5311-DB


Oct

 

ST STM32Discovery
Maxim MAX2769
TI DK-LM3S9B96
Innovate Software Solutions HawkBoard
Freescale  Wait and see image 


Nov

 

Microchip Another surprise
Maxim MAX2664
TI TMS320C2000
TI TMDSDCDC2KIT
Agilent  New DMM

 

Dec

 

Freescale
Got a very cool product pencilled in here, but not allowed to say too much...Keep checking, you won't regret it! image

 

 

Feb

 

Maxim MAX2209

  • Sign in to reply
  • Cancel
  • PBrunner
    PBrunner over 15 years ago in reply to Former Member

    Have you found all the details you were looking for on the K60 ? This is for sure a cool device with everything in it.

    I am thinking about setting up an "ask the expert " session on these products by beg of Dec but in case you do not want to wait, send me your questions

     

    Regarding Dev tools availability, the lucky guys coming to Electronica will be able to see it running and maybe even more image

     

    Stay tuned. More details to come

     

    Peggy

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • awinning
    awinning over 15 years ago in reply to obones
    Hi Olivier...let me work on that. I know one sensor manufacturer that is desperate to be involved in RoadTest, but don't really do dev kits as such.
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • awinning
    awinning over 15 years ago in reply to awinning

    Just a couple of updates. Apparantly I got two different Freescale part numbers mixed up, which to you means an extra RoadTest very soon

     

    And the Analog Devices part image is actually  SOT89 RF IF

     

     

    u
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • obones
    obones over 15 years ago in reply to awinning

    Hi Olivier...let me work on that. I know one sensor manufacturer that is desperate to be involved in RoadTest, but don't really do dev kits as such.

     

    Thanks, very appreciated. I have quite loose requirements though, so if you want me to discuss them, I can start a new thread in the discussions here or in the projects group you mentioned earlier

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • awinning
    awinning over 15 years ago in reply to obones
    Its fine, I think here is as good a place as any? Give me an idea what you need and I'll give it a go
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 15 years ago in reply to PBrunner

    I found most information in an area of the Freescale website. I guess that would be all the information available at this time?

    If known what sort of prices/price range would the K family be?

     

    Regards.

    http://www.freescale.com/webapp/sps/site/homepage.jsp?code=KINETIS

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • obones
    obones over 15 years ago in reply to awinning

    Well, ok, here is a short description of what I would need.

    The use would be for a situation where I need to mesure the distance from the sensor of an object moving toward or away from it without noticeable lateral movement (and I don't want to measure it anyway). The object is always different but all possible combinations are showing an almost flat square surface of 20 centimers side and cannot be tempered with so the sensor has to work on its own.

    With this measurement, I want to give feedback (visual, audible, to a supervisory system...) of that distance considering that anything closer than 5 centimeter is considered "too close" and anything farther than 200cm (approximately) is considered "too far".

    I don't need great precision, and if I was to use an ADC for reading the analog value, 8 bit would be enough giving me a resolution of roughly 1cm. Note that I would prefer a linear sensor but it doesn't have to be. For instance, it could be that the greatest precision is obtainable between 5 and 100cm (80% of values for instance) and less precise farther than 100cm. I would need however to distinguish between the "too close" and "too far" states.

    As the system will have to run on batteries in most installations, I would like it to consume as little energy as possible with the possible help of microcontroller turning it on and off on a regular basis. Having a microcontroller on the board is almost granted for the whole system to work, so it should not be a problem to add the management of the sensor.

     

    For this kind situation, I know of laser, infrared and ultrasonic sensors but I'm not sure what would be best suited considering the "low current" requirement. Nor do I know if there is a better kind of sensor.

     

    So if anything comes to mind to anyone, please do not hesitate to point me in the right direction.

     

    Regards

    Olivier

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • awinning
    awinning over 15 years ago in reply to obones

    Hey Olivier,

     

    I am working on this at the moment. I have an idea I'm puting to our sensor guys, and if they go for it, you should hear something soon,


    Ally

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • obones
    obones over 15 years ago in reply to awinning
    Thanks a lot for your help. Whatever the outcome, I appreciate your efforts.
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • PBrunner
    PBrunner over 15 years ago in reply to Former Member

    Sorry Alan for my late reply. Kinetis products will be many and there will be a lot of different derivatives in each of the sub families (K10, K20, K30, K40, K60). The lowest version will be priced below 1$.

     

    Peggy

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>