RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Fluke 233 Meter Review - Important Follow-up
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 45 replies
  • Subscribers 2759 subscribers
  • Views 14176 views
  • Users 0 members are here
Related

Fluke 233 Meter Review - Important Follow-up

Zad
Zad over 15 years ago

I have had my Fluke 233 just over 4 months now, over which time it has  had pretty light use. Which is why what I am about to say is a bit of a  surprise.

In my review I wrote:

Batteries.  400  hours  estimated life is  excellent. That probably works out at 3 to 4  years  usage for me. But,  when they go, it does mean potentially 5  batteries  have to be replaced.

I have used it for maybe 5 hours use  at the outside, and not at all for the past month or so (sadly, my  engineering has mostly been on paper or PC recently). That doesn't sound  much, but it adds up to quite a few voltage and resistance  measurements.Anyway, I came to use my Fluke 233 today and this met me:

 

http://i222.photobucket.com/albums/dd237/Zadpics/FlatBattery.jpg

 

Pretty much running on empty! Removing the remote head results in a BATT  warning and no measurements are possible. If I am going to be  installing a new set of 5 batteries every 4 months then it becomes a very expensive meter! I had thought that using high energy density AA  cells was a good idea (the cells it came with were brand new Duracells  with a very long use-by date), but maybe Fluke are covering up some  nasty quiescent current use. Swapping out the batteries allowed me to test  the off-load voltages, which were all around 0.95-0.96 Volts, so that rules out a rogue cell failure. My investigations with my trusty Fluke 77 (battery age 4 years) revealed the following:

Body power consumption, power ON = 3 to 6mA
Body power consumption, power OFF = 0.9 to 1.1mA
Display unit, power ON = 3 to 3.6mA
Display unit, power OFF = 1mA

 

Looking at http://www1.duracell.com/oem/Pdf/new/MX1500_US_UL.pdf the nominal capacity for <5mW drain is 1600 to 2300mAh (to 1 volt). 2300mAh at 1mA, is 95.8 days...

 

You  will note that an "on" life of 3mA is 766 hours, and 6mA is 383 hours,  which averages close to the specified taget of "around 400 hours".  Presuming you use your meter 24 hours a day, and don't actually switch  it off...

 

Given the recently found RF vulnerability in the Fluke 87 V, it does   make me wonder if Fluke are taking their eye off the ball. It surely cannot be right that a   meter eats a set of 5 cells in 4 months, especially given such light   usage. This is certainly not the sort of meter to leave in your tool case, because chances are that the batteries will be flat when you need it.

 

If any other Fluke 233 owners have experienced any similar failures, please let me know!

 

If any Fluke reps see this: Is there a known fault with the 233? Because this does look like a bit of a killer design issue.

 

Mike

  • Sign in to reply
  • Cancel
Parents
  • gbrettell
    gbrettell over 15 years ago

    I have experienced the same problems with my unit (as Mike & Patrick have noted above) ... I have used my unit very 'lightly' ... total "ON" time is probably < 20-hours.  I always turn if off when I am not using it to conserve on batteries ... well, so I THOUGHT.  image

     

    The batteries are being slowly depleated even without use ... seems like a design flaw (or oversight).  I wonder if there is a way to fix this with a firmware update that would power down the unit completely?

     

    Gregory

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Zad
    Zad over 15 years ago in reply to gbrettell

    I'm glad I checked this forum today, I think the auto-email thing ceased to function a few months ago. I think it is about time for me to follow this up directly with Fluke. This is now at least 4 people who I know of that have experienced unacceptably short battery life. I'm not sure they can be flash upgraded, as neither section has anything resembling a JTAG connector. There are some test points, but they look more analogue in nature. Let us see what Fluke have to say.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to Zad

    Hello Viewers, The 233 is unique in its design and implementation with its wireless display utilizing both iR and RF communication between the meter base and the remote display. While docked the meter utilizes iR communication and when the display and base are separated RF communication is used. When new the meter is shipped with paper tabs inserted into the battery compartment for both the base and the display to keep the batteries disconnected from the meters power supplies. This is to insure that the batteries have a full charge and the customer gets the longest battery life possible. The reason for a short battery shelf life is that when the meter is turned off and the display is mated, the iR communication is still active. This was done by design to give the user the most flexibility when using their 233 meter. The design allows the user to power on and to wake up the meter while the display and body are disconnected. It simplifies the meters operation. This use model was important to customers during our initial research for the 233. The alternative would have been to have two separate power buttons, one for the base and one for the display. Our research indicated that this was a less attractive solution to our implementation of one power up option for both parts. The trade off is the unit consumes more power but gives the users more flexibility. If the meter were to go into battery save mode and the iR communication were not active, the display and meter body would need to be re-connected before the display could power up. This option and two separate power up processes were not attractive in our research. To optimize the battery life, for intermittent use or extended periods of storage, it is recommended that the paper tabs be re-inserted into the battery compartments or the batteries be removed completely. Jim Newell Sales & Application Engineer Fluke Corporation

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to daveleb55

    Hi David,

     

    When it was a new feature 8 years ago, I guess they thought it was best for the customer if they tried to make the workflow toward using it like a traditional multimeter, i.e. just turn the dial and go. That was a challenge to do with low energy, if there are no contacts to be exposed. There are techniques but probably 8-10 years ago (when they started designing it) the chipsets didn't wake up transmit and receive functions fast enough to keep energy consumption down and power-on response time high.

    I don't know about other users, but I too would rather prioritise battery life with a slight workflow change (such as a manual switch to power on the IR-wireless adaptor or remote display).

     

    Fast-forward to today, and with the introduction of technologies like Bluetooth LE, manufacturers have got a way to provide a much improved capability on their newer designs, allowing both a local display and a remote display (either a custom unit, or a mobile phone). As I understand, many of the wireless adaptors or remote displays now have a separate power button - Fluke's IR3000 has that, as does Keysight's wireless adaptors too.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • daveleb55
    daveleb55 over 7 years ago in reply to e14 Contributor

    Dear Mr. Newell,

     

    You've got to be joking. "Put the paper tabs back in" or "take the batteries out???"

     

    You guys are supposed to be ENGINEERS. you can't figure out how to preserve battery life??

     

    Fluke has had a decades long reputation for superior products. I guess that's over now.

     

    Very disappointing.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • daveleb55
    daveleb55 over 7 years ago in reply to e14 Contributor

    Dear Mr. Newell,

     

    You've got to be joking. "Put the paper tabs back in" or "take the batteries out???"

     

    You guys are supposed to be ENGINEERS. you can't figure out how to preserve battery life??

     

    Fluke has had a decades long reputation for superior products. I guess that's over now.

     

    Very disappointing.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • shabaz
    shabaz over 7 years ago in reply to daveleb55

    Hi David,

     

    When it was a new feature 8 years ago, I guess they thought it was best for the customer if they tried to make the workflow toward using it like a traditional multimeter, i.e. just turn the dial and go. That was a challenge to do with low energy, if there are no contacts to be exposed. There are techniques but probably 8-10 years ago (when they started designing it) the chipsets didn't wake up transmit and receive functions fast enough to keep energy consumption down and power-on response time high.

    I don't know about other users, but I too would rather prioritise battery life with a slight workflow change (such as a manual switch to power on the IR-wireless adaptor or remote display).

     

    Fast-forward to today, and with the introduction of technologies like Bluetooth LE, manufacturers have got a way to provide a much improved capability on their newer designs, allowing both a local display and a remote display (either a custom unit, or a mobile phone). As I understand, many of the wireless adaptors or remote displays now have a separate power button - Fluke's IR3000 has that, as does Keysight's wireless adaptors too.