RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Fluke 233 Meter Review - Important Follow-up
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 45 replies
  • Subscribers 2758 subscribers
  • Views 14377 views
  • Users 0 members are here
Related

Fluke 233 Meter Review - Important Follow-up

Zad
Zad over 15 years ago

I have had my Fluke 233 just over 4 months now, over which time it has  had pretty light use. Which is why what I am about to say is a bit of a  surprise.

In my review I wrote:

Batteries.  400  hours  estimated life is  excellent. That probably works out at 3 to 4  years  usage for me. But,  when they go, it does mean potentially 5  batteries  have to be replaced.

I have used it for maybe 5 hours use  at the outside, and not at all for the past month or so (sadly, my  engineering has mostly been on paper or PC recently). That doesn't sound  much, but it adds up to quite a few voltage and resistance  measurements.Anyway, I came to use my Fluke 233 today and this met me:

 

http://i222.photobucket.com/albums/dd237/Zadpics/FlatBattery.jpg

 

Pretty much running on empty! Removing the remote head results in a BATT  warning and no measurements are possible. If I am going to be  installing a new set of 5 batteries every 4 months then it becomes a very expensive meter! I had thought that using high energy density AA  cells was a good idea (the cells it came with were brand new Duracells  with a very long use-by date), but maybe Fluke are covering up some  nasty quiescent current use. Swapping out the batteries allowed me to test  the off-load voltages, which were all around 0.95-0.96 Volts, so that rules out a rogue cell failure. My investigations with my trusty Fluke 77 (battery age 4 years) revealed the following:

Body power consumption, power ON = 3 to 6mA
Body power consumption, power OFF = 0.9 to 1.1mA
Display unit, power ON = 3 to 3.6mA
Display unit, power OFF = 1mA

 

Looking at http://www1.duracell.com/oem/Pdf/new/MX1500_US_UL.pdf the nominal capacity for <5mW drain is 1600 to 2300mAh (to 1 volt). 2300mAh at 1mA, is 95.8 days...

 

You  will note that an "on" life of 3mA is 766 hours, and 6mA is 383 hours,  which averages close to the specified taget of "around 400 hours".  Presuming you use your meter 24 hours a day, and don't actually switch  it off...

 

Given the recently found RF vulnerability in the Fluke 87 V, it does   make me wonder if Fluke are taking their eye off the ball. It surely cannot be right that a   meter eats a set of 5 cells in 4 months, especially given such light   usage. This is certainly not the sort of meter to leave in your tool case, because chances are that the batteries will be flat when you need it.

 

If any other Fluke 233 owners have experienced any similar failures, please let me know!

 

If any Fluke reps see this: Is there a known fault with the 233? Because this does look like a bit of a killer design issue.

 

Mike

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Hello Mike and everyone else who wrote about the problem with the Fluke 233 using up batteries.   I contacted Fluke and they also know about the issue.  It is underwarranty and they will either fix your meter or give you a new one and a free calibration as well.   Contact them, give them the serial number of the unit and they will tell you where to send it.   I sent my to Everett, WA.

     

    Also, I want to let everyone know.  I service and sell Fluke hand held test equipment.  I live in Elkhart, IN, USA.   Let me know if I can be of service

     

    Best Regards,

    Perry

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • danteo
    danteo over 14 years ago in reply to e14 Contributor

    Thank you Perry,

     

    I have the same problem, I will contact Fluke.

     

    Regards,

    Dan

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to danteo

    Hey Dan,

     

    Thanks for the note.  Let me know how things turn out with Fluke.   I have some friends that work there and if the service department does not do you right, I'd like to know so I can follow up with them.

     

    Best Regards,

    Perry

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to danteo

    Hey Dan,

     

    Thanks for the note.  Let me know how things turn out with Fluke.   I have some friends that work there and if the service department does not do you right, I'd like to know so I can follow up with them.

     

    Best Regards,

    Perry