RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Fluke 233 Meter Review - Important Follow-up
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 45 replies
  • Subscribers 2759 subscribers
  • Views 14174 views
  • Users 0 members are here
Related

Fluke 233 Meter Review - Important Follow-up

Zad
Zad over 15 years ago

I have had my Fluke 233 just over 4 months now, over which time it has  had pretty light use. Which is why what I am about to say is a bit of a  surprise.

In my review I wrote:

Batteries.  400  hours  estimated life is  excellent. That probably works out at 3 to 4  years  usage for me. But,  when they go, it does mean potentially 5  batteries  have to be replaced.

I have used it for maybe 5 hours use  at the outside, and not at all for the past month or so (sadly, my  engineering has mostly been on paper or PC recently). That doesn't sound  much, but it adds up to quite a few voltage and resistance  measurements.Anyway, I came to use my Fluke 233 today and this met me:

 

http://i222.photobucket.com/albums/dd237/Zadpics/FlatBattery.jpg

 

Pretty much running on empty! Removing the remote head results in a BATT  warning and no measurements are possible. If I am going to be  installing a new set of 5 batteries every 4 months then it becomes a very expensive meter! I had thought that using high energy density AA  cells was a good idea (the cells it came with were brand new Duracells  with a very long use-by date), but maybe Fluke are covering up some  nasty quiescent current use. Swapping out the batteries allowed me to test  the off-load voltages, which were all around 0.95-0.96 Volts, so that rules out a rogue cell failure. My investigations with my trusty Fluke 77 (battery age 4 years) revealed the following:

Body power consumption, power ON = 3 to 6mA
Body power consumption, power OFF = 0.9 to 1.1mA
Display unit, power ON = 3 to 3.6mA
Display unit, power OFF = 1mA

 

Looking at http://www1.duracell.com/oem/Pdf/new/MX1500_US_UL.pdf the nominal capacity for <5mW drain is 1600 to 2300mAh (to 1 volt). 2300mAh at 1mA, is 95.8 days...

 

You  will note that an "on" life of 3mA is 766 hours, and 6mA is 383 hours,  which averages close to the specified taget of "around 400 hours".  Presuming you use your meter 24 hours a day, and don't actually switch  it off...

 

Given the recently found RF vulnerability in the Fluke 87 V, it does   make me wonder if Fluke are taking their eye off the ball. It surely cannot be right that a   meter eats a set of 5 cells in 4 months, especially given such light   usage. This is certainly not the sort of meter to leave in your tool case, because chances are that the batteries will be flat when you need it.

 

If any other Fluke 233 owners have experienced any similar failures, please let me know!

 

If any Fluke reps see this: Is there a known fault with the 233? Because this does look like a bit of a killer design issue.

 

Mike

  • Sign in to reply
  • Cancel
Parents
  • gbrettell
    gbrettell over 15 years ago

    I have experienced the same problems with my unit (as Mike & Patrick have noted above) ... I have used my unit very 'lightly' ... total "ON" time is probably < 20-hours.  I always turn if off when I am not using it to conserve on batteries ... well, so I THOUGHT.  image

     

    The batteries are being slowly depleated even without use ... seems like a design flaw (or oversight).  I wonder if there is a way to fix this with a firmware update that would power down the unit completely?

     

    Gregory

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • gbrettell
    gbrettell over 12 years ago in reply to gbrettell

    Regarding the 233 ... At the time, I had just accepted the poor battery life ... then got frustrated and started to research the internet for a solution.  Sure enough ... Fluke will update the firmware at no charge (and provide calibration).  You are responsible for the shipping charges to send the item to them, however.

     

    It is better to call them:  888.993.5853 ... I experienced problems with their website.

     

    The "music on hold" is very distorted (if you call them and are put on hold) .. I brought this to their attention and they just kind of laughed it off ("yeah, I've heard that before").  You would think that a company that is associated with precision measurement equipment would have a more professional telephone system.

     

    I will update this post when I receive the meter back from Fluke.

     

    Gregory

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to gbrettell

    Well, I must say Fluke is trying hard. The concept of Fluke 233 is very good and I hope they keep this product alive for a long time like the 87V. I hope they don't think the CNX series can replace this.

     

    Yes, there is a firmware update to improve the battery life. However, I think (I am not able to get confirmation from Fluke), there is also a hardware change for those serial nos >22500000. There is also a slight change in the way you wake up the display when it goes to sleep if it is not docked.

    The supplementary manual can be found here:

    http://assets.fluke.com/manuals/233_____umeng0009.pdf

     

    "Change #4

    On page 13, replace the Battery Saver section with the following:

    Battery SaverTm(Sleep Mode) Units with S/N <224999999

    The Meter powers-down (Sleep mode) if there is no function change, range change, or button push for

    20 minutes. The lowest power drain occurs when the display module is docked with the Meter base. When

    the display is docked and the Meter is in sleep mode or off, a power drain continues from intermittent

    communication between the radios.

    To wake up the Meter, push a button or turn the function switch.

    To disable the Sleep mode, hold down the g button while turning the Meter on. The Sleep mode is always

    disabled in the MIN MAX AVG mode.

    To optimize battery life, it is recommended one battery be removed from the meter base and display for

    extended periods of storage or intermittent use.

    Battery SaverTm(Sleep Mode) Units with S/N >225000000

    The Meter powers-down (Sleep mode) if there is no function change, range change, or button push for

    20 minutes.

    To wake up the Meter, Remate the display or turn the function switch.

    To disable the Sleep mode, hold down the g button while turning the Meter on. The Sleep mode is always

    disabled in the MIN MAX AVG mode"

     

    Now although I say Fluke tries hard, I think their customer surveys are not up to standard. Either that or they are not telling the customers the entire story such that they get what the customers wanted but at the expense of something greater; just like the case of Fluke 233 and some other product which I prefer not to bring it up.

    Regardless, I hope you have some good results to share with us. Thanks.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to gbrettell

    Well, I must say Fluke is trying hard. The concept of Fluke 233 is very good and I hope they keep this product alive for a long time like the 87V. I hope they don't think the CNX series can replace this.

     

    Yes, there is a firmware update to improve the battery life. However, I think (I am not able to get confirmation from Fluke), there is also a hardware change for those serial nos >22500000. There is also a slight change in the way you wake up the display when it goes to sleep if it is not docked.

    The supplementary manual can be found here:

    http://assets.fluke.com/manuals/233_____umeng0009.pdf

     

    "Change #4

    On page 13, replace the Battery Saver section with the following:

    Battery SaverTm(Sleep Mode) Units with S/N <224999999

    The Meter powers-down (Sleep mode) if there is no function change, range change, or button push for

    20 minutes. The lowest power drain occurs when the display module is docked with the Meter base. When

    the display is docked and the Meter is in sleep mode or off, a power drain continues from intermittent

    communication between the radios.

    To wake up the Meter, push a button or turn the function switch.

    To disable the Sleep mode, hold down the g button while turning the Meter on. The Sleep mode is always

    disabled in the MIN MAX AVG mode.

    To optimize battery life, it is recommended one battery be removed from the meter base and display for

    extended periods of storage or intermittent use.

    Battery SaverTm(Sleep Mode) Units with S/N >225000000

    The Meter powers-down (Sleep mode) if there is no function change, range change, or button push for

    20 minutes.

    To wake up the Meter, Remate the display or turn the function switch.

    To disable the Sleep mode, hold down the g button while turning the Meter on. The Sleep mode is always

    disabled in the MIN MAX AVG mode"

     

    Now although I say Fluke tries hard, I think their customer surveys are not up to standard. Either that or they are not telling the customers the entire story such that they get what the customers wanted but at the expense of something greater; just like the case of Fluke 233 and some other product which I prefer not to bring it up.

    Regardless, I hope you have some good results to share with us. Thanks.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Magura
    Magura over 12 years ago in reply to e14 Contributor

    Regarding Fluke's customer service, I think you're spot on.

     

    They always offer to look into the issues, or take the product in for a check.

    Unfortunately the result usually brings little to nothing, and leaves the customers as they were.

     

    I posted earlier in this thread about battery issues with the Fluke 12x series scopemeters.

    Same story.

    After that I decided to sort the issue myself, and reported back to Fluke how to solve it.

    That's like half a year ago by now, but nothing has changed. They keep shipping a product they know is flawed, even though the fix is rather simple and surely easily implemetable.

    In this case the fix was to change the type of rechargeable batteries.