RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Fluke 233 Meter Review - Important Follow-up
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 45 replies
  • Subscribers 2758 subscribers
  • Views 14347 views
  • Users 0 members are here
Related

Fluke 233 Meter Review - Important Follow-up

Zad
Zad over 15 years ago

I have had my Fluke 233 just over 4 months now, over which time it has  had pretty light use. Which is why what I am about to say is a bit of a  surprise.

In my review I wrote:

Batteries.  400  hours  estimated life is  excellent. That probably works out at 3 to 4  years  usage for me. But,  when they go, it does mean potentially 5  batteries  have to be replaced.

I have used it for maybe 5 hours use  at the outside, and not at all for the past month or so (sadly, my  engineering has mostly been on paper or PC recently). That doesn't sound  much, but it adds up to quite a few voltage and resistance  measurements.Anyway, I came to use my Fluke 233 today and this met me:

 

http://i222.photobucket.com/albums/dd237/Zadpics/FlatBattery.jpg

 

Pretty much running on empty! Removing the remote head results in a BATT  warning and no measurements are possible. If I am going to be  installing a new set of 5 batteries every 4 months then it becomes a very expensive meter! I had thought that using high energy density AA  cells was a good idea (the cells it came with were brand new Duracells  with a very long use-by date), but maybe Fluke are covering up some  nasty quiescent current use. Swapping out the batteries allowed me to test  the off-load voltages, which were all around 0.95-0.96 Volts, so that rules out a rogue cell failure. My investigations with my trusty Fluke 77 (battery age 4 years) revealed the following:

Body power consumption, power ON = 3 to 6mA
Body power consumption, power OFF = 0.9 to 1.1mA
Display unit, power ON = 3 to 3.6mA
Display unit, power OFF = 1mA

 

Looking at http://www1.duracell.com/oem/Pdf/new/MX1500_US_UL.pdf the nominal capacity for <5mW drain is 1600 to 2300mAh (to 1 volt). 2300mAh at 1mA, is 95.8 days...

 

You  will note that an "on" life of 3mA is 766 hours, and 6mA is 383 hours,  which averages close to the specified taget of "around 400 hours".  Presuming you use your meter 24 hours a day, and don't actually switch  it off...

 

Given the recently found RF vulnerability in the Fluke 87 V, it does   make me wonder if Fluke are taking their eye off the ball. It surely cannot be right that a   meter eats a set of 5 cells in 4 months, especially given such light   usage. This is certainly not the sort of meter to leave in your tool case, because chances are that the batteries will be flat when you need it.

 

If any other Fluke 233 owners have experienced any similar failures, please let me know!

 

If any Fluke reps see this: Is there a known fault with the 233? Because this does look like a bit of a killer design issue.

 

Mike

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    Hi Perry,

    Thanks for sharing the information on how to check firmware version.

     

    As for the problem definition, I do not know exactly what Fluke did but as you can see from the supplementary manual which I posted Sep 19 above, it appears that there is a difference in how you wake up the meter when it is undocked.

    For brand new units, S/N >22500000, you will not be able to wake the meter by just turning the function switch or pushing a button.

    For units with S/N <24999999, you can wake the unit by turning the function switch or push a button.

    I was not able to get any confirmation whether with the upgraded firmware for S/N <24999999, does the waking up behavior changed or does it remain the same as before; i.e. you can wake it up just by turning the function switch or pressing a button. Please note I am only referring to the case whereby the display is undocked.

     

    Now, if indeed there is a difference between S/N<2499999 and S/N>2500000 in the way the display wakes up when undocked, then I would be inclined to say there is indeed a hardware difference. I'm not saying it is a problem but I think there is a change in the hardware design.

     

    eplanz

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to Zad

    Hey Everyone,

     

    Sorry that some of you have had problems with Fluke.  I for one think they are not only the best when it comes to test equipment.   The problem with the meter is not hardware.   It is firmware, the problem is fixed when they reprogram the meter to turn off.   That happens whit firmware revision 2.0   If you want to check your meter to see what revision you have, it's easy.

     

    "Hold down the "hold", turn meter to vdc. After a few seconds the display comes up with V1.00, V1.01 or V2.00. V2.00 has the battery fix."

     

    Let me know if I can be of help.

     

    Kind Regards,

    Perry

     

    Sent from my iPad

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Zad
    Zad over 12 years ago in reply to gbrettell

    Thanks for the heads-up on this.

     

    I have tried twice to contact Fluke's customer support concerning this issue. On neither occasion have I received a reply. I don't really fancy spending money on-hold on the phone or sending it off only for there to be 'no fault found', so I think I will just leave it in it's box on the shelf where it is now, and bring it out when I need a spare meter. The real fix would be to increase the current limiting resistor on the IR transmitter. It only has to work over a distance of 1cm or so when the unit is docked. Beyond that, it is classed as undocked and it switches to the RF link anyway.

     

    I get the feeling that this is a result of parent company Danaher's cost-cutting in action.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Magura
    Magura over 12 years ago in reply to e14 Contributor

    Regarding Fluke's customer service, I think you're spot on.

     

    They always offer to look into the issues, or take the product in for a check.

    Unfortunately the result usually brings little to nothing, and leaves the customers as they were.

     

    I posted earlier in this thread about battery issues with the Fluke 12x series scopemeters.

    Same story.

    After that I decided to sort the issue myself, and reported back to Fluke how to solve it.

    That's like half a year ago by now, but nothing has changed. They keep shipping a product they know is flawed, even though the fix is rather simple and surely easily implemetable.

    In this case the fix was to change the type of rechargeable batteries.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to gbrettell

    Well, I must say Fluke is trying hard. The concept of Fluke 233 is very good and I hope they keep this product alive for a long time like the 87V. I hope they don't think the CNX series can replace this.

     

    Yes, there is a firmware update to improve the battery life. However, I think (I am not able to get confirmation from Fluke), there is also a hardware change for those serial nos >22500000. There is also a slight change in the way you wake up the display when it goes to sleep if it is not docked.

    The supplementary manual can be found here:

    http://assets.fluke.com/manuals/233_____umeng0009.pdf

     

    "Change #4

    On page 13, replace the Battery Saver section with the following:

    Battery SaverTm(Sleep Mode) Units with S/N <224999999

    The Meter powers-down (Sleep mode) if there is no function change, range change, or button push for

    20 minutes. The lowest power drain occurs when the display module is docked with the Meter base. When

    the display is docked and the Meter is in sleep mode or off, a power drain continues from intermittent

    communication between the radios.

    To wake up the Meter, push a button or turn the function switch.

    To disable the Sleep mode, hold down the g button while turning the Meter on. The Sleep mode is always

    disabled in the MIN MAX AVG mode.

    To optimize battery life, it is recommended one battery be removed from the meter base and display for

    extended periods of storage or intermittent use.

    Battery SaverTm(Sleep Mode) Units with S/N >225000000

    The Meter powers-down (Sleep mode) if there is no function change, range change, or button push for

    20 minutes.

    To wake up the Meter, Remate the display or turn the function switch.

    To disable the Sleep mode, hold down the g button while turning the Meter on. The Sleep mode is always

    disabled in the MIN MAX AVG mode"

     

    Now although I say Fluke tries hard, I think their customer surveys are not up to standard. Either that or they are not telling the customers the entire story such that they get what the customers wanted but at the expense of something greater; just like the case of Fluke 233 and some other product which I prefer not to bring it up.

    Regardless, I hope you have some good results to share with us. Thanks.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • gbrettell
    gbrettell over 12 years ago in reply to gbrettell

    Regarding the 233 ... At the time, I had just accepted the poor battery life ... then got frustrated and started to research the internet for a solution.  Sure enough ... Fluke will update the firmware at no charge (and provide calibration).  You are responsible for the shipping charges to send the item to them, however.

     

    It is better to call them:  888.993.5853 ... I experienced problems with their website.

     

    The "music on hold" is very distorted (if you call them and are put on hold) .. I brought this to their attention and they just kind of laughed it off ("yeah, I've heard that before").  You would think that a company that is associated with precision measurement equipment would have a more professional telephone system.

     

    I will update this post when I receive the meter back from Fluke.

     

    Gregory

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    >**************************Disclaimer**************************

    >The contents of this e-mail and any file transmitted with it are confidential and intended solely for the individual or entity to whom they are addressed. 

    >The content may also contain legal, professional or other privileged information. If you received this e-mail in error, please destroy it immediately. 

    >You should not copy or use it for any purpose nor disclose its contents to any other person. The views stated herein do not necessarily represent the view of the Company.

    >Please ensure you have adequate virus protection before you open or detach any documents from this transmission. The Company does not accept any liability for  viruses.

    >Premier Farnell plc

    >150 Armley Road Leeds

    >LS12 2QQ

    >Telephone +44 (0) 870 129 8608

    >Fax +44 (0) 870 129 8610

    >Registered in England

    >Company Number 876412

    >Registered Office: Farnell House, Forge Lane, Leeds LS12 2NE

    >************************************************************

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Thank you for the follow up note.   I must have been tired when I wrote the post.  The battery drain

    problem has been fixed by Fluke.  It was not a software fix, it was a firmware fix.   The fix was

    was implemented with serial number 138xxxxx.

     

    If you have a Fluke 233 with a lower serial number, I suggest contacting Fluke and seeing if they

    will fix your meter and apply the update.   I personally have been very pleased with Fluke and the

    products they make and the services they provide.

     

    Please let me know if I can be of help.

     

    Best Regards,

    Perry

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Hi Perry,

    Thanks for sharing with us that there is a software fix for the battery drain issue.

    I am still not quite clear after reading your message below what fluke has done to solve this issue.

    You mentioned that "Also, the mode for 138xxx and below turns the meter all the way off after the battery get to low." Should it be 138xxx and above turns the meter all the way off after the battery get to low?

    Is this specifically the fix?

     

    Also, I'm confused by the following "The lowest power drain occurs when the display module is docked with the Meter base. When the display is docked and the Meter is in sleep mode or off, a power drain continues from intermittent communication between the radios."

    Is Fluke trying to tell us to enable or disable sleep mode in order to not let the batteries drain?

     

    Finally and if you don't mind, I'm assuming you already have a unit with the fix. How did you estimate the battery life to be 400 hours? That's presumably several years worth of battery life. This is a sincere question and I am not challenging you.

    Thanks for your help.

     

    ============================================================================================

     

     

    "I found that typical battery life is 400 hours using alkaline batteries.   I also found the note below that should be helpful in extending battery life.

     

    Also, the mode for 138xxx and below turns the meter all the way off after the battery gets to low.  Originally, the meter did not turn off and completely drained the batteries and caused them to leak in the battery compartment.

     

    I hope this helps.

     

    Regards,

     

    Perry

     

     

     

    On page 13, replace the Battery Saver section with the following: Battery SaverTM(Sleep Mode)

     

    The Meter powers-down (Sleep mode) if there is no function change, range change, or button push for 20 minutes. The lowest power drain occurs when the display module is docked with the Meter base. When the display is docked and the Meter is in sleep mode or off, a power drain continues from intermittent communication between the radios.

     

    To wake up the Meter, push a button or turn the function switch.

     

    To disable the Sleep mode, hold down the g button while turning the Meter on. The Sleep mode is always disabled in the MIN MAX AVG mode.

     

    To optimize battery life, it is recommended one battery be removed from the meter base and display for extended periods of storage or intermittent use. "

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • danteo
    danteo over 14 years ago in reply to Zad

    I got a reply, I was sent to a local Fluke partner.

    I didn't send the meter because I'm using it and I don't konw exactly how long it takes the whole process.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>