RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Fluke 233 Meter Review - Important Follow-up
  • Blogs
  • RoadTest Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 45 replies
  • Subscribers 2671 subscribers
  • Views 12679 views
  • Users 0 members are here
Related

Fluke 233 Meter Review - Important Follow-up

Zad
Zad over 15 years ago

I have had my Fluke 233 just over 4 months now, over which time it has  had pretty light use. Which is why what I am about to say is a bit of a  surprise.

In my review I wrote:

Batteries.  400  hours  estimated life is  excellent. That probably works out at 3 to 4  years  usage for me. But,  when they go, it does mean potentially 5  batteries  have to be replaced.

I have used it for maybe 5 hours use  at the outside, and not at all for the past month or so (sadly, my  engineering has mostly been on paper or PC recently). That doesn't sound  much, but it adds up to quite a few voltage and resistance  measurements.Anyway, I came to use my Fluke 233 today and this met me:

 

http://i222.photobucket.com/albums/dd237/Zadpics/FlatBattery.jpg

 

Pretty much running on empty! Removing the remote head results in a BATT  warning and no measurements are possible. If I am going to be  installing a new set of 5 batteries every 4 months then it becomes a very expensive meter! I had thought that using high energy density AA  cells was a good idea (the cells it came with were brand new Duracells  with a very long use-by date), but maybe Fluke are covering up some  nasty quiescent current use. Swapping out the batteries allowed me to test  the off-load voltages, which were all around 0.95-0.96 Volts, so that rules out a rogue cell failure. My investigations with my trusty Fluke 77 (battery age 4 years) revealed the following:

Body power consumption, power ON = 3 to 6mA
Body power consumption, power OFF = 0.9 to 1.1mA
Display unit, power ON = 3 to 3.6mA
Display unit, power OFF = 1mA

 

Looking at http://www1.duracell.com/oem/Pdf/new/MX1500_US_UL.pdf the nominal capacity for <5mW drain is 1600 to 2300mAh (to 1 volt). 2300mAh at 1mA, is 95.8 days...

 

You  will note that an "on" life of 3mA is 766 hours, and 6mA is 383 hours,  which averages close to the specified taget of "around 400 hours".  Presuming you use your meter 24 hours a day, and don't actually switch  it off...

 

Given the recently found RF vulnerability in the Fluke 87 V, it does   make me wonder if Fluke are taking their eye off the ball. It surely cannot be right that a   meter eats a set of 5 cells in 4 months, especially given such light   usage. This is certainly not the sort of meter to leave in your tool case, because chances are that the batteries will be flat when you need it.

 

If any other Fluke 233 owners have experienced any similar failures, please let me know!

 

If any Fluke reps see this: Is there a known fault with the 233? Because this does look like a bit of a killer design issue.

 

Mike

  • Sign in to reply
  • Cancel

Top Replies

  • glenn71
    glenn71 over 6 years ago +3
    I wish I had done more research before I forked out $300+ on the 233/A. I too only get 3-4 months of use even when using Energizer ultimate lithium batteries. It does become expensive quickly. Not real…
  • Former Member
    Former Member over 15 years ago +1
    Hello Mike, Coincidentally, the batteries of my Fluke 233 died last week, after approximately 4 months of light use. As I suspected in my review and which you confirmed above, it is not possible to turn…
  • gbrettell
    gbrettell over 15 years ago +1
    I have experienced the same problems with my unit (as Mike & Patrick have noted above) ... I have used my unit very 'lightly' ... total "ON" time is probably < 20-hours. I always turn if off when I am…
  • Zad
    Zad over 13 years ago in reply to danteo

    Dan,

     

    I sent my email to ukservicedesk@fluke.com late Thursday night. Nothing heard back yet, but these things can take time to get passed around to the right people.

     

    My serial number is 1131xxxx too.

     

    Mike.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 13 years ago in reply to danteo

    Dan,

     

    I am not sure where you are located.   The best way I find to get service

    is to use Fluke's web site and set up an on line RMA.   Indicate the meter

    is underwarranty and expain the problem with with the meter killing

    batteries.  Also, be sure to request calibration it's free with repair in

    this case.   Actually the only cost you should have it shipping the meter

    to Fluke  and that is it.

     

    Let me know if you need anything more.

     

    Best Regards,

    Perry

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 13 years ago in reply to Former Member

    Thanks for the support Perry

     

    It inspires confidence in a product when after sales service happens.

     

    Regards Don

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • danteo
    danteo over 13 years ago in reply to Former Member

    Hi Perry,

     

    I live in Italy, and maybe the local Fluke CS is in vacation now image.

    I will wait for an answer.

     

    Thanks,

    Dan

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Zad
    Zad over 13 years ago in reply to Zad

    Still no reply from UK Fluke Service here.

     

    Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • danteo
    danteo over 13 years ago in reply to Zad

    I got a reply, I was sent to a local Fluke partner.

    I didn't send the meter because I'm using it and I don't konw exactly how long it takes the whole process.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 13 years ago in reply to Former Member

    Hi Perry,

    Thanks for sharing with us that there is a software fix for the battery drain issue.

    I am still not quite clear after reading your message below what fluke has done to solve this issue.

    You mentioned that "Also, the mode for 138xxx and below turns the meter all the way off after the battery get to low." Should it be 138xxx and above turns the meter all the way off after the battery get to low?

    Is this specifically the fix?

     

    Also, I'm confused by the following "The lowest power drain occurs when the display module is docked with the Meter base. When the display is docked and the Meter is in sleep mode or off, a power drain continues from intermittent communication between the radios."

    Is Fluke trying to tell us to enable or disable sleep mode in order to not let the batteries drain?

     

    Finally and if you don't mind, I'm assuming you already have a unit with the fix. How did you estimate the battery life to be 400 hours? That's presumably several years worth of battery life. This is a sincere question and I am not challenging you.

    Thanks for your help.

     

    ============================================================================================

     

     

    "I found that typical battery life is 400 hours using alkaline batteries.   I also found the note below that should be helpful in extending battery life.

     

    Also, the mode for 138xxx and below turns the meter all the way off after the battery gets to low.  Originally, the meter did not turn off and completely drained the batteries and caused them to leak in the battery compartment.

     

    I hope this helps.

     

    Regards,

     

    Perry

     

     

     

    On page 13, replace the Battery Saver section with the following: Battery SaverTM(Sleep Mode)

     

    The Meter powers-down (Sleep mode) if there is no function change, range change, or button push for 20 minutes. The lowest power drain occurs when the display module is docked with the Meter base. When the display is docked and the Meter is in sleep mode or off, a power drain continues from intermittent communication between the radios.

     

    To wake up the Meter, push a button or turn the function switch.

     

    To disable the Sleep mode, hold down the g button while turning the Meter on. The Sleep mode is always disabled in the MIN MAX AVG mode.

     

    To optimize battery life, it is recommended one battery be removed from the meter base and display for extended periods of storage or intermittent use. "

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 13 years ago in reply to Former Member

    Thank you for the follow up note.   I must have been tired when I wrote the post.  The battery drain

    problem has been fixed by Fluke.  It was not a software fix, it was a firmware fix.   The fix was

    was implemented with serial number 138xxxxx.

     

    If you have a Fluke 233 with a lower serial number, I suggest contacting Fluke and seeing if they

    will fix your meter and apply the update.   I personally have been very pleased with Fluke and the

    products they make and the services they provide.

     

    Please let me know if I can be of help.

     

    Best Regards,

    Perry

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 13 years ago in reply to Former Member

    >**************************Disclaimer**************************

    >The contents of this e-mail and any file transmitted with it are confidential and intended solely for the individual or entity to whom they are addressed. 

    >The content may also contain legal, professional or other privileged information. If you received this e-mail in error, please destroy it immediately. 

    >You should not copy or use it for any purpose nor disclose its contents to any other person. The views stated herein do not necessarily represent the view of the Company.

    >Please ensure you have adequate virus protection before you open or detach any documents from this transmission. The Company does not accept any liability for  viruses.

    >Premier Farnell plc

    >150 Armley Road Leeds

    >LS12 2QQ

    >Telephone +44 (0) 870 129 8608

    >Fax +44 (0) 870 129 8610

    >Registered in England

    >Company Number 876412

    >Registered Office: Farnell House, Forge Lane, Leeds LS12 2NE

    >************************************************************

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gbrettell
    gbrettell over 12 years ago in reply to gbrettell

    Regarding the 233 ... At the time, I had just accepted the poor battery life ... then got frustrated and started to research the internet for a solution.  Sure enough ... Fluke will update the firmware at no charge (and provide calibration).  You are responsible for the shipping charges to send the item to them, however.

     

    It is better to call them:  888.993.5853 ... I experienced problems with their website.

     

    The "music on hold" is very distorted (if you call them and are put on hold) .. I brought this to their attention and they just kind of laughed it off ("yeah, I've heard that before").  You would think that a company that is associated with precision measurement equipment would have a more professional telephone system.

     

    I will update this post when I receive the meter back from Fluke.

     

    Gregory

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
<>