RoadTests & Reviews
  • Products & Partners
  • More
RoadTests & Reviews
RoadTest Forum Review – Tenma 72-7222 Digital Clamp Multimeter
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 2745 subscribers
  • Views 4068 views
  • Users 0 members are here
  • RoadTest
  • element-14
  • tronixstuff
  • tenma
  • review
  • 72-7222
Related

Review – Tenma 72-7222 Digital Clamp Multimeter

tronixstuff
tronixstuff over 15 years ago

Hello element-14 members

 

The purpose of this article is to examine the Tenma 72-722272-7222 Digital Clamp Multimeter supplied for review by element-14/Farnell/Newark. The Tenma is a strongly featured yet inexpensive piece of test equipment – and considerably good value when you consider there is a current clamp for measuring high AC currents. So let’s have a look and see what we have.

 

Initial Impression

The Tenma arrives in a retail box, and generally nicely packaged. Naturally this has nothing to do with the performance of the meter at all, but at least they made an effort:

 

image

 

Opening up we find a nicely rounded group of items: the meter itself, some no-name AAA cells, test leads, a thermocouple for temperature measurement, a surprisingly articulate and well-written user manual, and the unit itself – all within a nice pouch. Wow – a pouch. Agilent? Fluke? All that money for a DMM and you don’t include a pouch?

 

image

 

Recent test equipment reviewers have made pulling apart the unit part of the review – so here goes… the back comes off easily:

 

image

 

No user-replaceable fuses… instead a PTC. A closer look at the PCB:

 

image

 

A very neat and organised PCB layout. There are plastic tabs that hold the PCB in along with a screw, however the case flexed too much for me to warrant removing the PCB completely. The spring for the clamp meter is locked in nicely and very strong, it won’t give up for a long time. Pulling the clamp base out reveals the rest of the PCB:

 

image

 

Installation of the battery is two stage procedure, first you need to remove a screw and then slide out the rear door:

 

image

 

… then insert the AAA cells into a frame, which is then inserted inside the unit:

 

image

 

The physical feel of the unit is relative to the purchase price, the plastic is simple and could be quite brittle if the unit was dropped from a height. The user manual claims the unit can be dropped from up to a height of one metre. Onto carpet? Yes. Concrete? Perhaps not. However like all test equipment one would hope the user would take care of it whenever possible. The clamp meter is very strong due to the large spring inside the handle, which can be opened up to around 28mm. The included leads are just on one meter long including the length of the probe:

 

image

 

The leads are rated to Category I 1000V (overkill – the meter can’t go that high) and 600 V Category II – “This category refers to local-level electrical distribution, such as that provided by a standard wall outlet or plug in loads (for example, 115 AC voltage for U.S. or 200 AC voltage for Europe). Examples of Measurement Category II are measurements performed on household appliances, portable tools, and similar modules” – definition from from National Instruments.  Unlike discount DMMs from unknown suppliers you can trust the rating to be true – otherwise element-14 wouldn’t be selling it.

 

Unit Specifications

 

  • Voltage Measuring Range DC:200mV, 2V, 20V, 200V, 600V
  • Voltage Measuring Range AC:2V, 20V, 200V, 600V
  • Current Measuring Range AC:2A, 20A, 200A, 400A
  • Resistance Measuring Range:200ohm, 2kohm, 20kohm, 200kohm, 2Mohm, 20Mohm
  • Temperature Measuring Range:-40°C to +1000°C
  • DMM Response Type:True RMS
  • DMM Functions:AC Current, AC/DC Voltage, Resistance, Temperature
  • Ranging:Auto
  • Display Count:1999
  • AC Current Range Accuracy:± (1.5% + 5d)
  • AC Voltage Range Accuracy:± (1.2% + 5d)
  • Accuracy:± (1.0% + 3d)
  • Current AC Max:400A
  • Current Range AC:2A, 20A, 200A, 400A
  • DC Voltage Range Accuracy1:± (0.8% + 1d)
  • Resistance Range Accuracy:± (1.0% + 2d)
  • Temperature Measuring Range:-40°C to +1000°C

 

The only measurement missed out on is DC current, however there is the Tenma 72-7224 which has DC current and frequency ranges. Finally, all the modes and buttons can be selected while holding the meter with one hand – for both left- and right-handed folk.

 

Measurement experience

Measurements were compared against my Fluke 233. First, AC voltage from the mains:

 

image

 

Next, a few DC voltage measurements:

 

image

 

image

 

image

 

image

 

Now for some resistance measurements. Higher values near the maximum of 20M Ohm can take around four seconds to measure:

 

image

 

image

 

Forward voltage of a 1N4004 diode:

 

image

 

Now off to the kitchen for some more measurements – first with the thermocouple:

 

image

 

The boiling water test – 100 degrees Celsius (you can also select Fahrenheit if so inclined):

 

image

 

And now to test out the AC current clamp meter function with a 10A kettle at boiling point. First, using the 20A current range:

 

image

 

And then again on the 400A current range:

 

image

 

As always, it’s best to use the multimeter range that more closely corresponds with the current under test. The meter also has a continuity test with a beeper, however it was somewhat slow and would often take around one second to register – so nothing too impressive on that front. The meter can record the maximum value with the grey button, or hold a reading using the yellow button.

 

Conclusion

The Tenma 72-722272-7222 works as advertised, and as expected. It is a solid little unit that if looked after should last a few years at a minimum. It certainly has a few limitations, such as the 1999 count display, lack of backlight, and the average continuity function. But don’t let that put you off. For the price – under Au$30 – it is a certified deal. If you need a clamp current meter for odd jobs or a casual-use multimeter and you are on a limited budget, the Tenma will certainly prove a worthwhile purchase. Full-size images are available on Flickr.

 

The element-14 part number is 128363903, Newark is 01N4891, or search for "72-7222".

 

Thank you for reading and if you have any questions please leave them below

cheers

John Boxall

"tronixstuff"

Attachments:
image72-7222.pdf
  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Hi John,

    A very indepth and worth while comparison. You have taken time and the results prove that the Tenma is indeed great value for money especially for the hobbiest and even professional engineers alike

    Many thanks

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • tronixstuff
    tronixstuff over 14 years ago in reply to e14 Contributor

    Thanks Peter, I really enjoyed writing the article.

    Cheers

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • tronixstuff
    tronixstuff over 14 years ago in reply to e14 Contributor

    Thanks Peter, I really enjoyed writing the article.

    Cheers