RoadTests & Reviews
  • Products & Partners
  • More
RoadTests & Reviews
RoadTest Forum road testing the EFM32™︎ Zero Gecko Starter Kit - Part 2
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 0 replies
  • Subscribers 2750 subscribers
  • Views 461 views
  • Users 0 members are here
  • RoadTest
  • zero_gecko_starter_kit
Related

road testing the EFM32™︎ Zero Gecko Starter Kit - Part 2

Jan Cumps
Jan Cumps over 11 years ago

Part 1: Prep for road testing the EFM32Tm Zero Gecko Starter Kit

 

I received the kit two days ago. I've unboxed it and completed my first road test goal.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Unboxing

 

There was not that much to do at package opening time. The box contains two boards in plastic shields bag and a usb cable.

At the bottom of the box was this tiniest Quick Start Guide that I've ever seen - the size of a business card.

Everything was safely packed and secured. The only thing you 'll have to add yourself is a CR2032 battery.

The two break-out connectors on the long sides of the board are not populated. I haven't checked yet what processor pins are routed to there.

 

Getting Started

 

Road Test 1: testing the quick start and demo, how easy is it to get them working

 

Running the pre-loaded example: This worked right out of the box. It's the Space Invaders classic of the 80s. This demo showcases the lcd and the two capacitive touch buttons.

 

Loading and running a demo: Simplicity Studio recognized the zero gecko starter kit and pre-loaded content related to that board. I was able to load the weather station demo from Simplicity Studio in one go. I selected to run it with the power monitor enabled. This demo focuses on the sensor board's capabilities.

 

Building and running the first project: I opened the source of the 'blink' example in the IDE. I used the 'Software Examples' wizard to get the project set up in the Simplicity IDE. The wizard sets up the project properties. It also guides you through your first compile and Debug cycle.

 

I was able to complete all three exercises without reading any documentation. I know the Eclipse environment well, but still the start pages and wizards are a great help to get you going without frustrations. All focus could be spent on learning and experimenting.

All these activities in Road Test 1 worked without errors or issues. The board behaved well. I didn't have a single setup, compile or runtime error.

 

Part 3: checking the different energy modes