RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Basic CNC
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 19 replies
  • Answers 3 answers
  • Subscribers 2753 subscribers
  • Views 2625 views
  • Users 0 members are here
  • cnc control
Related

Basic CNC

raymort
raymort over 10 years ago

Sorry to ask this question, but I have a new CNC MACHINE but I have not a clue how it works so frightened to try and use it without it disintegrating into loads of bits. So I live in Hereford in the UK and would like help from someone who would be prepared to show me. A good supply of brews a good dinner and if one day is not enough then you can stay.

I would be grateful for any help.

 

many thanks

RayMoreton

r.moreton@tesco.net

  • Sign in to reply
  • Cancel
Parents
  • michaelkellett
    0 michaelkellett over 10 years ago

    Can you post a picture and spec of your machine.

    If you want some trial material to cut that's a step up from Oasis flower stuff then buy some ModelBoard- here's a note I sent to someone a while ago:

     

    It was made from this stuff (probably M540):

     

    http://www.alchemie.com/category/products/modelboard/polyurethane-modelboard/ 

     

    but only because that was convenient for prototyping - for production it should be molded and there are a host of suitable plastics you might use - you would need to get advice from the tool designer/plastic molder.

     

    You can make functional things from the right grade of modelboard - one day I mean to make some loudspeaker cabinets from it.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • michaelkellett
    0 michaelkellett over 10 years ago

    Can you post a picture and spec of your machine.

    If you want some trial material to cut that's a step up from Oasis flower stuff then buy some ModelBoard- here's a note I sent to someone a while ago:

     

    It was made from this stuff (probably M540):

     

    http://www.alchemie.com/category/products/modelboard/polyurethane-modelboard/ 

     

    but only because that was convenient for prototyping - for production it should be molded and there are a host of suitable plastics you might use - you would need to get advice from the tool designer/plastic molder.

     

    You can make functional things from the right grade of modelboard - one day I mean to make some loudspeaker cabinets from it.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • raymort
    0 raymort over 10 years ago in reply to michaelkellett

    I don't have a pic at the moment but here is the spec.

     

    1 xRefurbished A3 3 Axis Hybrid BALLSCREW Desktop CNC Machine Router Engraving KIT Router

     

     

    Ballscrew Machine Assembled

    A3 size Machining Area - 500mm x 300mm, Z Axis 155mm

    Footprint: 950mm x 750mm

     

     

    Accuracy/Repeatability: 0.01mm

     

     

    Translation: Ballscrew

    Linear: Hiwin profile rails and carriages

     

     

    MDL NOTE: CUSTOMER TO SUPPLY: Desktop PC, Monitor, Keyboard and Mouse

     

     

    Machine Control Software - Mach3 Full License

    Design Software - VCarve Pro 7

     

     

    Electronic Jogging Handwheel

     

     

    Controller: 3 Axis Controller and x3 NEMA23 3.1Nm Stepper Motors (X, Y and Z)

     

     

    Proximity Home Switch (X, Y and Z) and additional external emergency stop

     

     

    Kress Spindle 1050FME, Kress Motor Mount, Brushed dust hood with connection for 38/63mm out

    3 x Kress Collets: 3mm, 6mm and 8mm

     

     

    Sample Milling Cutters, 4 x T-Nuts, Grease

     

     

    Single phase - standard socket 240V

    One socket required - extension lead supplied

     

     

    Shipping price added during checkout includes 2-3 hours installation and initial training followed by free email and telephone support20%£1,185.00
    1 xVectric VCarve Pro 7 and Mach3 Bundle

    Code: [VCARVEMACH3]

    20%£485.00
    1 xDelivery, Assembly + Training - UK20%£280.00
    1 xNew for 2013

     

     

    CONTROLLER: FEATURES AND SPECIFICATIONS:

    USB (V2.x) from PC/Laptop running Windows XP, Vista or Windows 7 (32 bit or 64bit)

    motor driver connector pin-out is compatible with 10 pin open source interface (Linistepper, PICStep)

    controller works with most step/dir stepper and servo motor drivers available on the market

    buffered IO for maximum performance

    advanced interpolation algorithms

    start, stop, pause and resume execution of program on your machine

    standard RS274/NGC G-code (EMC2 compatible)

    advanced G-codes - G40, G41, G42 (Cutter Radius Compensation) supported

    advanced G-codes - G43, G49 (Tool Length Offsets) supported

    advanced G-codes - G54, G59.3 (Coordinate System Origins) supported

    tested with SolidCAM, MasterCAM, ArtCAM, Vectric, CamBam, MeshCAM ... generated G-code

    Profili 4-axes and 3-axes G-code supported

    import toolpath from DXF files

    import toolpath from PLT/HPGL files

    import toolpath from image files

    import toolpath from NC-Drill (Excellon) files

    import toolpath from Gerber (RS-274X) files

    toolpath simulation

    automatic homing procedure

    advanced toolchange procedures

    automatic tool length measuring

    export toolpath to G-code

    export toolpath to DXF

    SDK (software developers kit) is available

    works on MacOS X (Snow Leopard 10.6.3) with virtual machine emulating Windows XP SP39 axes USB CNC controller Mk2:

    100 kHz maximum step frequency

    7 digital outputs

    12 us minimum pulse width

    manual jog inputs for all axes

    limit inputs for all axes

    5 general inputs

    8 control inputs for pendant or similar device

    SD card support for running g-code without computer

    control external devices with I2C protocol

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • raymort
    0 raymort over 10 years ago in reply to michaelkellett

    Hi, just looked at the site url that you sent me. I will look at the options that are sold.

    I will look now and see if I can find the machine I have. Due to illness I have not been able to use, and

    its been on my bench for 2 years.

    regards RayMort