RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Getting Ready to RoadTest a Low-Side Gate Driver with Truly Differential Inputs That Prevents False Triggering. Are You Interested?
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 6 replies
  • Answers 4 answers
  • Subscribers 2750 subscribers
  • Views 1371 views
  • Users 0 members are here
  • scasny
  • power_featured
Related

Getting Ready to RoadTest a Low-Side Gate Driver with Truly Differential Inputs That Prevents False Triggering. Are You Interested?

rscasny
rscasny over 7 years ago

I'm getting ready to roadtest a 1-channel low-side gate driver EVM that has truly differential inputs to prevent false triggering.  What the truly differential inputs do is to overcome driving issues when DC offset (DC GND shift) or AC voltage drops (AC GND shift) are existing between the driver and the MCU ground potentials. image

 

Common situations characterized by DC and AC GND shifts are, respectively, the driving of high-side devices and the driving in noisy environments with significant stray inductance on the ground path.

 

Some Features

  • 48V half-bridge buck converter tested up to 60W
  • Integrated section to generate and regulate the DC GND shift
  • Possibility to easily regulate the AC GND shift
  • Possibility to compare the 1EDN TDI and standard low side driver in GND shift situation

 

A Word about Low side gate drivers │ EiceDRIVERTm 1EDN TDI

The input signal levels of conventional low-side gate driver ICs are referenced to the ground potential of the gate driver IC. If in the application the ground potential of the gate driver IC shifts excessively false triggering of the gate driver IC can occur.

 

The 1EDN7550 and 1EDN8550 gate driver ICs have truly differential inputs. Their control signal inputs are largely independent from the ground potential. Only the voltage difference between its input contacts is relevant. This prevents false triggering of power MOSFETs.

image

 

Here's a schematic block:

image

 

Here's some documentation

Product Brief / Datasheet

App Note

 

I'm getting 10 units to roadtest. I'd like to get some roadtesters that both have the test equipment and a background in this type of circuitry to test this out. If you are interested, please send me a message at rscasny

 

Thanks.

 

Randall Scasny

RoadTest Program Manager

  • Sign in to reply
  • Cancel
  • rscasny
    0 rscasny over 7 years ago in reply to Gough Lui

    I fixed it

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 7 years ago

    I happen to have a GaN half-bridge on the desk at the moment.

     

    image

     

     

    It's a next step in a blog series I'm writing here on the community: https://www.element14.com/community/groups/power-management/blog/2017/05/14/gan-point-of-load-converter-48v-to-1v-50a-pa…

    I'd certainly be interested in putting the Infineon design.

     

    Here's a board with a GaN half-bridge I made earlier. Blog on element14: Hercules LaunchPad and GaN FETs - Part 3b: BoosterPack Layout - my version

    image

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 7 years ago

    The chips are very interesting parts of which I was already aware of from Infineon direct marketing.

     

    The EV board is very much designed for evaluation in a a fairly abstract (ie not directly related to a specific product design) environment and the app note that goes with it is very comprehensive. So much so, that there seems little point in actually getting the EV board oneself - I would go straight to a product prototype design - using the EV board and the documentation of the chips and board to inform that design.

     

    I'd like to see the parts used to make a 4 switch buck/boost controller (see LTC3780 for example) since this topology, although superficially attractive, seems always to result in truly disgusting noise levels with the power devices utterly failing to turn on and off cleanly. I suspect that the ground bounce immunity of these drivers might be able to make that topology work much better. So an evaluation board, maybe using an FPGA or CPLD to control 4 switches and designed for maybe 6 - 30V in and 12 or 24 V out at 100W (or more) would be a very interesting thing to see. (Of course if it doesn't manage better noise than existing solutions it won't be much use, but I think it could.)

     

    MK

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Gough Lui
    0 Gough Lui over 7 years ago in reply to hlipka

    That definitely helps as the datasheets linked seemed to be for the driver only rather than the eval board as a whole. Time to give it a thorough read image.

     

    - Gough

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • hlipka
    0 hlipka over 7 years ago in reply to Gough Lui

    You can find a picture on the product homepage: https://www.infineon.com/cms/en/product/evaluation-boards/eval_hb_bc_1edn8550b/

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Gough Lui
    0 Gough Lui over 7 years ago

    Just a heads up - I can't seem to load the image - you might need to edit and repost the posting as it seems to be a known permissions issue.

     

    - Gough