RoadTests & Reviews
  • Products & Partners
  • More
RoadTests & Reviews
RoadTest Forum How Would You Roadtest the MaaXBoard?
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 17 replies
  • Answers 9 answers
  • Subscribers 2749 subscribers
  • Views 4081 views
  • Users 0 members are here
  • maaxboard
Related

How Would You Roadtest the MaaXBoard?

rscasny
rscasny over 6 years ago

I was sent some info on a new dev board called the MaaXBoard. image

 

The MaaXBoard is based on the NXP i.MX 8M applications processor, and it's good for embedded computing and applications for AI at the edge, industrial automation, multimedia, and IoT applications -- all topics of interest on element14.

 

The MaaXBoard uses NXP’s i.MX 8M family of applications processors, which are based on the ArmRegistered CortexRegistered-A53 and Cortex-M4 cores, providing audio, voice and video processing. The MaaXBoard has a range of capabilities making it ideal to investigate AI, IoT and multimedia applications, offering designers everything they need to support and create a Linux, Android, Windows 10 IoT Core or other OS-based system. The platform’s on-board peripherals include 2GB of DDR4 memory, a Gigabit Ethernet port, dual USB 3.0 host ports, HDMI output, MIPI-DSI, MPI-CSI, WiFi, Bluetooth Low Energy, MicroSD card slot and eMMC storage.

Here's some tech specs:

  • Processor
    • NXP i.MX 8M Processor with Quad Arm Cortex-A53 and single Cortex-M4F
  • Memory
    • 2GB DDR4 SDRAM
    • 8GB eMMC
    • MicroSD Slot
  • Communications and User Interface
    • Gigabit Ethernet
    • Dual USB 3.0
    • MIPI-DSI
    • MIIP-CSI
    • HDMI
    • Supports up to 4k resolution
    • Wi-Fi 802.11 b/g/n/ac
    • Bluetooth 4.2 (Bluetooth Low Energy)
    • Onboard Ceramic Antenna (Default)
    • External Antenna supported
    • Audio Expansion
  • User I/O
    • 40 Pin Low Speed Expansion Interface
    • Raspberry Pi Hat Compatible
    • Digital I/O voltage: 3.3V
  • Other
    • Voltage Regulators
    • USB Type C 5V/3A Power input
    • Operating Temperature: 0~70°C
  • Mechanical
    • 85mm x 56mm x 12mm form factor

 

Question: How would you roadtest this dev board?

  • Sign in to reply
  • Cancel
Parents
  • gordonmx
    0 gordonmx over 6 years ago

    Do you have a link to the documentation?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • phoenixcomm
    0 phoenixcomm over 6 years ago in reply to gordonmx

    God just use GOOGLE! https://www.variscite.com/product/system-on-module-som/cortex-a53-krait/dart-mx8m-nxp-imx-8m/

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • gordonmx
    0 gordonmx over 6 years ago in reply to phoenixcomm

    You're a little confused.  I'm not God.  Although he may use Goggle I don't believe needs to.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • gordonmx
    0 gordonmx over 6 years ago in reply to phoenixcomm

    You're a little confused.  I'm not God.  Although he may use Goggle I don't believe needs to.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • phoenixcomm
    0 phoenixcomm over 6 years ago in reply to gordonmx

    This is what I wrote: God just use GOOGLE!

    maybe I dropped the comma: as is God, just use GOOGLE!

    or better yet: My God, just use GOOGLE!