Products
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
RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum LPCXpresso LPC1114 review
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 0 replies
  • Subscribers 2750 subscribers
  • Views 769 views
  • Users 0 members are here
  • RoadTest
  • development
  • review
  • kit
Related

LPCXpresso LPC1114 review

ar_sys
ar_sys over 16 years ago
Hi All,

This is my first review and I hope that my ' English translation ' is readable. 
Thanks to element14 to give me the opportunity of test and review the LPCXpresso board.
The hardware out of the package
LPCXpresso join two module in a single PCB as shown in figure.
image
   
The LPC-Link on the PCB left side is the NXP USB-JTAG programming/debug tool with some interesting characteristics: 
- It use a ram-based LPC3154 and load the firmware on every power-up through USB,  allow easily future upgrade to support new devices, new IDE features,  firmware fix-up etc. 
- JTAG signal are buffered with common ICs in a easy to replace package,  a little safeguard in case of target hardware accidental failure.    
- JTAG interface is suitable for programming/debug a wide range of LPC MCU,  need only a cheap adapter cable and can be used after cutting the connections along the J4 middle point. 
  
The target LPC1114FBD48/301,1LPC1114FBD48/301,1 on the PCB right-side, simple but well done: 
- Only the MCU, the XTAL, a LED and a few decoupler capacitors,  the essential to make the MCU 'Ready to Go ' 
- All the MCU pin available through two 100mil spacing row  allow very easy and fast interconnect with user prototype  
- The good pinout compatibility with other currently available LPCXpresso board can result in a reusable prototype hardware for other target. 
 
Set up the envinroment: 
The package do not have a software CD. This solution lowering the price and also allow to start with the most recently update software package and documentation.
On the www.nxp.com/lpcxpresso webpage we can find a link to download the Code-Red IDE. Following the online detailed Getting-started guide we can perform:  
- IDE installaction and activation (pag 8-10) explain how to install and license the IDE.  
- Getting familiar with the LPCXpresso IDE (pag 11-14) shown basic IDE  functionalityes   
- Build, download and debug the blinky apps (pag 16-19) use a simple on board led-blink example to explain  basic Build/debug process. 

Followed the previous steps, we have now a working CORTEX-M0 board with a robust Eclipse based IDE.  
 
Exploring code example: 

The LPC11xx example directory contain 3 zip archive:
 
- CMSISv1p30_LPC11xx  Cortex Microcontroller Software Interface Standard defines for LPC11xx device allowing reusable code template. 
- 1114examples  a full set of example projects, each of that focus on a specific MCU peripherals  
- LPCXpresso1114  a subset of 1114examples with some common peripherals driver build into a single library 
 
Following the example code reduce the effort to learn the on chip peripherals setting, giving  us a start point to manage the device SFR. 
 
I want to remark a very useful IDE feature. It allow to build  a 'semihosting'  project that intercept the write character to stdout and redirect it on the IDE console. See the LPCXpresso1114_consoleprint example for details and limitations.   
   
Conclusion: 
 
- a good designed hardware 
- a featured IDE 
- a good support 
- a cheap price 
 
Definitely, the right platform to evaluate and start to work with NXP LPC1xxx devices.