Products
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
RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Beaglebone in LIDD Mode
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 2751 subscribers
  • Views 744 views
  • Users 0 members are here
Related

Beaglebone in LIDD Mode

Kilohercas
Kilohercas over 13 years ago

Does any one know how to program LCD with SSD1963 controller in LIDD mode?

Since bit banging is slow, even at 1,2GHz overclock (below 10MHz)

But how to do that in raw C in IAR or CCStudio , not some Linux or other nonsense

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply
  • Cancel
  • Kilohercas
    0 Kilohercas over 13 years ago in reply to shabaz

    LCD controller can be interfaced to i80 bus, and that mode is called LIDD

     

    LCD D0-D15: 16 bits of data/address lines
    LCD_VSYNC
    -> RS (also called Command/Data or CD or Address/Data; NOT reset)
    LCD_HSYNC
    -> Write-bar
    LCD_PCLK
    -> Read-bar
    LCD_AC_ENB_CS
    -> Chip Select 0
    LCD_MCLK
    -> Chip Select 1

    but have no idea how to program that in C

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 13 years ago

    Hi Linas,

     

    I'm not sure a LCD with SSD1963 is designed for the LCD controller built-in to the TI chip. Isn't the SSD... type chip used when you want to interface to an address and data bus and write graphics instructions with no need for constant refresh? Whereas the LCD controller on the Beaglebone is intended for refreshing a TFT display without this type of interfacing controller.

    I could be very wrong though.