RoadTests & Reviews
  • Products & Partners
  • More
RoadTests & Reviews
RoadTest Forum Roadtest Thread for the Bluetooth LE Audio Development Kit
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 2744 subscribers
  • Views 5879 views
  • Users 0 members are here
  • RoadTest
  • Bluetooth LE Audio development kit
  • NRF5340-AUDIO-DK
  • nordic semiconductor
Related

Roadtest Thread for the Bluetooth LE Audio Development Kit

srutledge
srutledge over 4 years ago

Use this thread to comment or ask any questions about the Bluetooth LE Audio Development Kit or the RoadTest in general.

Link to the RoadTest

  • Sign in to reply
  • Cancel
Parents
  • BigG
    BigG over 4 years ago

    In order to road test the BLE Audio Development Kit surely you need both a transmitter device and a receiver device, as only one dev board is provided. For example, a separate PC dongle could be provided (although not sure what is available), which receives the audio signal from PC via USB and then we can use this dev kit as the wireless BLE receiver device, or we use the dev kit as the transmitter device and then use a compatible wireless BLE speaker or headset, which is provided, as the receiver. Otherwise the only scenario where just one dev kit works is the configuration where an audio file is on SD card and one attaches a wired speaker to the dev kit, which then removes the BLE audio element. What do you propose. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • BigG
    BigG over 4 years ago

    In order to road test the BLE Audio Development Kit surely you need both a transmitter device and a receiver device, as only one dev board is provided. For example, a separate PC dongle could be provided (although not sure what is available), which receives the audio signal from PC via USB and then we can use this dev kit as the wireless BLE receiver device, or we use the dev kit as the transmitter device and then use a compatible wireless BLE speaker or headset, which is provided, as the receiver. Otherwise the only scenario where just one dev kit works is the configuration where an audio file is on SD card and one attaches a wired speaker to the dev kit, which then removes the BLE audio element. What do you propose. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • rscasny
    rscasny over 4 years ago in reply to BigG

    Thanks. I contacted the sponsor. I'll probably extend the enrollment time until I get an answer from them. Thanks for writing.

    Randall