RoadTests & Reviews
  • Products & Partners
  • More
RoadTests & Reviews
RoadTest Forum Roadtest Thread for the Bluetooth LE Audio Development Kit
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 2744 subscribers
  • Views 5879 views
  • Users 0 members are here
  • RoadTest
  • Bluetooth LE Audio development kit
  • NRF5340-AUDIO-DK
  • nordic semiconductor
Related

Roadtest Thread for the Bluetooth LE Audio Development Kit

srutledge
srutledge over 4 years ago

Use this thread to comment or ask any questions about the Bluetooth LE Audio Development Kit or the RoadTest in general.

Link to the RoadTest

  • Sign in to reply
  • Cancel
Parents
  • Fred27
    Fred27 over 4 years ago

    A quick scan of the  documentation suggests that this can still use the older Bluetooth Classic SBC in addition to the newer Bluetooth LE LC3. I'm no Bluetooth expect, so could be wrong about this.

    I also find it odd that the DSP included on the board has stereo in but only mono out. I understand that the one possible application is to work as a single earbud from a pair. However, it seems odd that the use case of being a complete stereo Bluetooth headset is not possible.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Fred27
    Fred27 over 4 years ago

    A quick scan of the  documentation suggests that this can still use the older Bluetooth Classic SBC in addition to the newer Bluetooth LE LC3. I'm no Bluetooth expect, so could be wrong about this.

    I also find it odd that the DSP included on the board has stereo in but only mono out. I understand that the one possible application is to work as a single earbud from a pair. However, it seems odd that the use case of being a complete stereo Bluetooth headset is not possible.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • weiwei2
    weiwei2 over 4 years ago in reply to Fred27

    and stereo is supported via Connected Isochronous Stream (CIS) also mentioned in the same article developer.nordicsemi.com/.../README.html

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • weiwei2
    weiwei2 over 4 years ago in reply to Fred27

    for the mono out, do you mean this line in developer.nordicsemi.com/.../README.html

    • In the current version of the nRF5340 Audio application, the BIS mode offers only monophonic sound reproduction.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Fred27
    Fred27 over 4 years ago in reply to Fred27

    Actually, I think I misunderstood the wording of the documentation. It seems to be Bluetooth LE only.