RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum How Would You RoadTest a Powerful Microcontroller Designed for EV Charging, e-Bikes and Robotics?
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 22 replies
  • Subscribers 2756 subscribers
  • Views 15660 views
  • Users 0 members are here
  • RoadTest
  • infineon
  • xmc7200
  • pre-roadtest discussion
Related

How Would You RoadTest a Powerful Microcontroller Designed for EV Charging, e-Bikes and Robotics?

rscasny
rscasny over 3 years ago

imageHi All.

I have been in conversation with a roadtest sponsor who is excited to have the community test in the coming year a powerful microcontroller that's designed for industrial applications including VFDs, electrical vehicle (EV) charging, two-wheel electrical vehicles (e-bikes) and robotics. I want to tell you a little about it and give you some resources to review. I'm seeking some ideas of how community members would roadtest the kit. This is important because, in my initial conversation with them, they were wondering what else would be needed to be provided with the kit. Ex. Motor? Sensors? Other?

The kit is based on the Infineon XMC7200 microcontroller and part of the family of XMC7000 microcontrollers, which offer single and dual core options of 350-MHz 32-bit Arm® Cortex®-M7 and a 100-MHz 32-bit Arm® Cortex®-M0+, up to 8 MB of embedded flash and 1 MB of on-chip SRAM. The products operate from 2.7 to 5.5 V and achieve full specification from -40°C to 125°C.

For More Information About The Kit

You would get the following in the kit:

  • XMC7200 evaluation board
  • USB Type-A to Mirco-B cable
  • 12V/3A DC power adapter with additional blades
  • Six jumper wires (five inches each)
  • Quick start guide
  • Other--what else would you need?

Here are some documents for further study:

  • Product Presentation
  • Datasheet
  • Getting Started
  • App Note
  • User Manual
  • Release Notes

Feel free to offer your thoughts and ideas in the comments section below.

  • Sign in to reply
  • Cancel
Parents
  • michaelkellett
    michaelkellett over 3 years ago

    Its an interesting processor and board. There is a lot of stuff in that processor chip - you would be spending a LOT more than 40 hours just reading the data and getting to understand how it works.

    Then you need to think of a decent project and try and implement it.

    Things that stand out for me are the CAN FD and ethernet, you could make a nice CAN FD monitor device with Ethernet connection to PC - I've done that with an ST ARM M7 for single speed CAN and it's a lot of work.

    Any real project using this processor will be a lot of work !

    It would be really nice to have another board that talks CAN FD as part of the kit so it has something to talk to.

    I don't have a current project that would use this part - and while it might be fun to play with it a bit that wouldn't really make a good Road Test.

    For any one who does have a serious project for it the cost of the board is just going to be lost in the noise of the other project costs.

    So the ideal tester will be some one with time on their hands and a lot of skill and experience - not too common a person to find.

    MK

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • michaelkellett
    michaelkellett over 3 years ago

    Its an interesting processor and board. There is a lot of stuff in that processor chip - you would be spending a LOT more than 40 hours just reading the data and getting to understand how it works.

    Then you need to think of a decent project and try and implement it.

    Things that stand out for me are the CAN FD and ethernet, you could make a nice CAN FD monitor device with Ethernet connection to PC - I've done that with an ST ARM M7 for single speed CAN and it's a lot of work.

    Any real project using this processor will be a lot of work !

    It would be really nice to have another board that talks CAN FD as part of the kit so it has something to talk to.

    I don't have a current project that would use this part - and while it might be fun to play with it a bit that wouldn't really make a good Road Test.

    For any one who does have a serious project for it the cost of the board is just going to be lost in the noise of the other project costs.

    So the ideal tester will be some one with time on their hands and a lot of skill and experience - not too common a person to find.

    MK

    • Cancel
    • Vote Up +4 Vote Down