RoadTests & Reviews
  • Products & Partners
  • More
RoadTests & Reviews
RoadTest Forum How Would You RoadTest a Powerful Microcontroller Designed for EV Charging, e-Bikes and Robotics?
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 22 replies
  • Subscribers 2744 subscribers
  • Views 15886 views
  • Users 0 members are here
  • RoadTest
  • infineon
  • xmc7200
  • pre-roadtest discussion
Related

How Would You RoadTest a Powerful Microcontroller Designed for EV Charging, e-Bikes and Robotics?

rscasny
rscasny over 3 years ago

imageHi All.

I have been in conversation with a roadtest sponsor who is excited to have the community test in the coming year a powerful microcontroller that's designed for industrial applications including VFDs, electrical vehicle (EV) charging, two-wheel electrical vehicles (e-bikes) and robotics. I want to tell you a little about it and give you some resources to review. I'm seeking some ideas of how community members would roadtest the kit. This is important because, in my initial conversation with them, they were wondering what else would be needed to be provided with the kit. Ex. Motor? Sensors? Other?

The kit is based on the Infineon XMC7200 microcontroller and part of the family of XMC7000 microcontrollers, which offer single and dual core options of 350-MHz 32-bit Arm® Cortex®-M7 and a 100-MHz 32-bit Arm® Cortex®-M0+, up to 8 MB of embedded flash and 1 MB of on-chip SRAM. The products operate from 2.7 to 5.5 V and achieve full specification from -40°C to 125°C.

For More Information About The Kit

You would get the following in the kit:

  • XMC7200 evaluation board
  • USB Type-A to Mirco-B cable
  • 12V/3A DC power adapter with additional blades
  • Six jumper wires (five inches each)
  • Quick start guide
  • Other--what else would you need?

Here are some documents for further study:

  • Product Presentation
  • Datasheet
  • Getting Started
  • App Note
  • User Manual
  • Release Notes

Feel free to offer your thoughts and ideas in the comments section below.

  • Sign in to reply
  • Cancel
Parents
  • obones
    obones over 3 years ago

    As others, I'm impressed with what the microcontroller is offering, even more so by the evaluation kit board. I mean it has gigabit ethernet, an M.2 slot, numerous connectors, even some compatible with Arduino.

    To be able to test it, I would certainly need some guidance as to what it can do and what the seller is expecting from us. Especially considering that I don't have an EV at hand, nor any robot arm or the like. I do have 5V motors and a few low level ideas, but I don't think this would do any justice to the kit.

    In the end, I feel that this is not targeted to my audience (advanced hobbyist) but I'll be sure to read the reviews from more experienced users.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • robogary
    robogary over 3 years ago in reply to obones

    Not sure this controller needs to be applied to an EV, robot, or an eBike to be an effective and interesting road test.

    The 350Mhz 32 bit maybe could be used as a retrogame console, a really smart LED lamp or other helpful appliance. 

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • robogary
    robogary over 3 years ago in reply to obones

    Not sure this controller needs to be applied to an EV, robot, or an eBike to be an effective and interesting road test.

    The 350Mhz 32 bit maybe could be used as a retrogame console, a really smart LED lamp or other helpful appliance.