RoadTests & Reviews
  • Products & Partners
  • More
RoadTests & Reviews
RoadTest Forum How Would You RoadTest a Powerful Microcontroller Designed for EV Charging, e-Bikes and Robotics?
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 22 replies
  • Subscribers 2744 subscribers
  • Views 15963 views
  • Users 0 members are here
  • RoadTest
  • infineon
  • xmc7200
  • pre-roadtest discussion
Related

How Would You RoadTest a Powerful Microcontroller Designed for EV Charging, e-Bikes and Robotics?

rscasny
rscasny over 3 years ago

imageHi All.

I have been in conversation with a roadtest sponsor who is excited to have the community test in the coming year a powerful microcontroller that's designed for industrial applications including VFDs, electrical vehicle (EV) charging, two-wheel electrical vehicles (e-bikes) and robotics. I want to tell you a little about it and give you some resources to review. I'm seeking some ideas of how community members would roadtest the kit. This is important because, in my initial conversation with them, they were wondering what else would be needed to be provided with the kit. Ex. Motor? Sensors? Other?

The kit is based on the Infineon XMC7200 microcontroller and part of the family of XMC7000 microcontrollers, which offer single and dual core options of 350-MHz 32-bit Arm® Cortex®-M7 and a 100-MHz 32-bit Arm® Cortex®-M0+, up to 8 MB of embedded flash and 1 MB of on-chip SRAM. The products operate from 2.7 to 5.5 V and achieve full specification from -40°C to 125°C.

For More Information About The Kit

You would get the following in the kit:

  • XMC7200 evaluation board
  • USB Type-A to Mirco-B cable
  • 12V/3A DC power adapter with additional blades
  • Six jumper wires (five inches each)
  • Quick start guide
  • Other--what else would you need?

Here are some documents for further study:

  • Product Presentation
  • Datasheet
  • Getting Started
  • App Note
  • User Manual
  • Release Notes

Feel free to offer your thoughts and ideas in the comments section below.

  • Sign in to reply
  • Cancel
Parents
  • colporteur
    colporteur over 3 years ago

    Going to ask a less than knowledgeable question: is this kit a breakout board primarily used to explore the capabilities of the XMC7200 in power applications? The board itself would not be incorporated into a project yes/no?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to colporteur

    Yes. There's no power electronics / charging circuit in this kit. It has the right parts to build the brains for such a system. Not the muscles.

    In the real world, the XMC7200, and some of the peripherals, would be inside your smart charger design. The Debugger, the pcb, and some other supporting parts that make evaluation easier, would not have a place in the final design.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to colporteur

    Yes. There's no power electronics / charging circuit in this kit. It has the right parts to build the brains for such a system. Not the muscles.

    In the real world, the XMC7200, and some of the peripherals, would be inside your smart charger design. The Debugger, the pcb, and some other supporting parts that make evaluation easier, would not have a place in the final design.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • colporteur
    colporteur over 3 years ago in reply to Jan Cumps

    Cool, a ready made breakout board. Outside my RoadTest Review capabilities. Be neat to work on a project that explores the chip deliverables. Thanks for the response.