RoadTests & Reviews
  • Products & Partners
  • More
RoadTests & Reviews
RoadTest Forum How Would You RoadTest a Powerful Microcontroller Designed for EV Charging, e-Bikes and Robotics?
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 22 replies
  • Subscribers 2746 subscribers
  • Views 15876 views
  • Users 0 members are here
  • RoadTest
  • infineon
  • xmc7200
  • pre-roadtest discussion
Related

How Would You RoadTest a Powerful Microcontroller Designed for EV Charging, e-Bikes and Robotics?

rscasny
rscasny over 3 years ago

imageHi All.

I have been in conversation with a roadtest sponsor who is excited to have the community test in the coming year a powerful microcontroller that's designed for industrial applications including VFDs, electrical vehicle (EV) charging, two-wheel electrical vehicles (e-bikes) and robotics. I want to tell you a little about it and give you some resources to review. I'm seeking some ideas of how community members would roadtest the kit. This is important because, in my initial conversation with them, they were wondering what else would be needed to be provided with the kit. Ex. Motor? Sensors? Other?

The kit is based on the Infineon XMC7200 microcontroller and part of the family of XMC7000 microcontrollers, which offer single and dual core options of 350-MHz 32-bit Arm® Cortex®-M7 and a 100-MHz 32-bit Arm® Cortex®-M0+, up to 8 MB of embedded flash and 1 MB of on-chip SRAM. The products operate from 2.7 to 5.5 V and achieve full specification from -40°C to 125°C.

For More Information About The Kit

You would get the following in the kit:

  • XMC7200 evaluation board
  • USB Type-A to Mirco-B cable
  • 12V/3A DC power adapter with additional blades
  • Six jumper wires (five inches each)
  • Quick start guide
  • Other--what else would you need?

Here are some documents for further study:

  • Product Presentation
  • Datasheet
  • Getting Started
  • App Note
  • User Manual
  • Release Notes

Feel free to offer your thoughts and ideas in the comments section below.

  • Sign in to reply
  • Cancel
  • robogary
    robogary over 3 years ago in reply to obones

    Not sure this controller needs to be applied to an EV, robot, or an eBike to be an effective and interesting road test.

    The 350Mhz 32 bit maybe could be used as a retrogame console, a really smart LED lamp or other helpful appliance. 

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • obones
    obones over 3 years ago

    As others, I'm impressed with what the microcontroller is offering, even more so by the evaluation kit board. I mean it has gigabit ethernet, an M.2 slot, numerous connectors, even some compatible with Arduino.

    To be able to test it, I would certainly need some guidance as to what it can do and what the seller is expecting from us. Especially considering that I don't have an EV at hand, nor any robot arm or the like. I do have 5V motors and a few low level ideas, but I don't think this would do any justice to the kit.

    In the end, I feel that this is not targeted to my audience (advanced hobbyist) but I'll be sure to read the reviews from more experienced users.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 3 years ago

    I am planning to purchase an electric cycle next summer so if this road test overlapped with that purchase I would try to do comparison tests between this controller and a commercial controller.

    This powerful module/kit is not a complete charging controller, so there would be a lot of work to design and build it into a useful charging controller. No doubt it could be a much smarter and better connected controller than a normal commercial controller, but it is not clear how much could be accomplished in a typical road test period.

    I have not researched this module enough yet to determine if I would take on such an ambitious project.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • skruglewicz
    skruglewicz over 3 years ago

    Looks like an interesting kit. I was in a challenge for the PSoC RA2 an kit and I’m presently participating in a challenge on hackster.. Im  utilizing the PSoC 4100S Pioneer kit.

    in my experience he’s a very well design kits. Usually the self-contained with the sensors needed to experiment with. This one would probably need extra offboard components to test it.

    What I  usually do for road test  is to scrutinize the documentation and the code examples. Modus toolbox is a complex programming  environment. There is always hello world,

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to robogary

    If you want something a little more challenging, i.e. weekend project as opposed to single evening project, then a motorised line array that allows automatic alignment of each segment of the array for optimal sound coverage using machine vision to detect the current space occupancy.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • robogary
    robogary over 3 years ago in reply to ntewinkel

    I wanna see the tuned port enclosure calculations for this one 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • robogary
    robogary over 3 years ago in reply to beacon_dave

    now thats what I'm talking about !   The 1812 Overture could use a speaker like that. 

    The debut being in Miami I'm sure played some Pitbull on it   https://www.youtube.com/watch?v=zaSZE194D4I

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • ntewinkel
    ntewinkel over 3 years ago in reply to robogary

    Awesomeness Joy 

    I want to see Infineon fund this project for you, @robogary!!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to robogary
    robogary said:
    Massive sound system for the diesel and tread clanking

    You have seen Nik Nowak's 'Sound Tank' haven't you ?

    image

    https://en-uk.sennheiser.com/shape-the-future-of-audio-nik-nowak-sound-tank-performance-gramps-miami

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • robogary
    robogary over 3 years ago

    I would get a used power wheels car (which it already an EV) remove the switch gas pedal, and make it an smart EV. Would need some type of ev charge connector to be realistic.

    My ultimate dream is refitting a power wheels style tank, kick out the kids, and making it RC. Would need at least 1 substantial servo > 20kg*cm for steering. I dont think the kiddie tank has a motor per tread, 50 and 100amp H bridges arent bank breakers for motor drivers. Massive sound system for the diesel and tread clanking.

    Now that would be a fun project. 

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
<>