RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum ROADTEST POLL: Would You Be Interesting in Roadtesting a Data Acquisition Learning Module?
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 40 replies
  • Subscribers 2748 subscribers
  • Views 7222 views
  • Users 0 members are here
  • roadtest survey
  • adalm2000
  • analog devices
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

ROADTEST POLL: Would You Be Interesting in Roadtesting a Data Acquisition Learning Module?

rscasny
rscasny over 3 years ago

adalm2000I'm planning a roadtest on this product. I'd like to gauge your interest in roadtesting it. 

Here's some information about the product:

ADALM2000 is an (M2K) active learning module is an affordable USB-powered data acquisition module that takes the capabilities of the ADALM1000 (M1K) active learning module to the next level. With 12bit ADCs and DACs running at 100MSPS, the ADALM2000 with the Scopy software, brings the power of high performance lab equipment to the palm of your hand, enabling electrical engineering students and hobbyists to explore signals and systems into the tens of MHz without the cost and bulk associated with traditional lab gear. The ADALM2000, when coupled with Analog Devices' ScopyTm graphical application software running on a computer, provides the user with the following high performance instrumentation.

Here are some of its features:

  • Provides access to real circuits and concepts used in an actual real-time engineering environment
  • Available online resources support educator, guide students to learn difficult engineering concepts
  • Hands-on activities stimulate interest and accelerate learning in fundamental engineering concepts
  • Helps to develop critical thinking skills needed for career development
  • 16-ch digital logic analyzer (3.3V CMOS and 1.8V or 5V tolerant, 100MS/s)
  • 16-ch pattern generator (3.3V CMOS, 100MS/s), 16-ch virtual digital I/O
  • 2 input/output digital trigger signals for linking multiple instruments (3.3V CMOS)
  • Digital bus analyzers (SPI, I²C, UART, parallel)
  • 2-ch oscilloscope with differential inputs, 2-ch arbitrary function generator, 2-ch voltmeter

Here are some docs:

Datasheet

Flyer

App Notes

Here's the poll question:

  • Cancel
Parents
  • anniel747
    anniel747 over 3 years ago
    This reply was deleted.
    • Cancel
    • Cancel
  • javagoza
    javagoza over 3 years ago in reply to anniel747

    I agree, it would be great to be able to test ADALM2000 together with ADALP2000. I have the ADALM1000 with the ADALP2000 and it's definitely a great kit to learn on.

    • Cancel
    • Vote Up +4 Vote Down
    • Cancel
Reply
  • javagoza
    javagoza over 3 years ago in reply to anniel747

    I agree, it would be great to be able to test ADALM2000 together with ADALP2000. I have the ADALM1000 with the ADALP2000 and it's definitely a great kit to learn on.

    • Cancel
    • Vote Up +4 Vote Down
    • Cancel
Children
  • shabaz
    shabaz over 3 years ago in reply to javagoza

    Yes definitely! 

    I tried an early predecessor of ADAPL2000 here:  Christmas Gift Ideas part 2 - Analog Kit 

    Very neat kit, I still use the predecessor version to experiment with (and I bought one for a family member too), and that is now a 9 years old kit! : ) The newer ADALP2000 looks much more comprehensive. It is basically a very large portfolio of AD components, but linked to an educational program too. I wish other manufacturers did the same.

    • Cancel
    • Vote Up +3 Vote Down