RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum ROADTEST POLL: Would You Be Interesting in Roadtesting a Data Acquisition Learning Module?
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 40 replies
  • Subscribers 2748 subscribers
  • Views 7221 views
  • Users 0 members are here
  • roadtest survey
  • adalm2000
  • analog devices
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

ROADTEST POLL: Would You Be Interesting in Roadtesting a Data Acquisition Learning Module?

rscasny
rscasny over 3 years ago

adalm2000I'm planning a roadtest on this product. I'd like to gauge your interest in roadtesting it. 

Here's some information about the product:

ADALM2000 is an (M2K) active learning module is an affordable USB-powered data acquisition module that takes the capabilities of the ADALM1000 (M1K) active learning module to the next level. With 12bit ADCs and DACs running at 100MSPS, the ADALM2000 with the Scopy software, brings the power of high performance lab equipment to the palm of your hand, enabling electrical engineering students and hobbyists to explore signals and systems into the tens of MHz without the cost and bulk associated with traditional lab gear. The ADALM2000, when coupled with Analog Devices' ScopyTm graphical application software running on a computer, provides the user with the following high performance instrumentation.

Here are some of its features:

  • Provides access to real circuits and concepts used in an actual real-time engineering environment
  • Available online resources support educator, guide students to learn difficult engineering concepts
  • Hands-on activities stimulate interest and accelerate learning in fundamental engineering concepts
  • Helps to develop critical thinking skills needed for career development
  • 16-ch digital logic analyzer (3.3V CMOS and 1.8V or 5V tolerant, 100MS/s)
  • 16-ch pattern generator (3.3V CMOS, 100MS/s), 16-ch virtual digital I/O
  • 2 input/output digital trigger signals for linking multiple instruments (3.3V CMOS)
  • Digital bus analyzers (SPI, I²C, UART, parallel)
  • 2-ch oscilloscope with differential inputs, 2-ch arbitrary function generator, 2-ch voltmeter

Here are some docs:

Datasheet

Flyer

App Notes

Here's the poll question:

  • Cancel
Parents
  • shabaz
    shabaz over 3 years ago

    I bet this would be extremely popular! The ADALM1000 was a wonderful device but very version 1,0, but this newer ADALM2000 is supported a lot more with software and with educational material (complete training program!) as far as I'm aware. It is pretty much a lab-in-a-box, but surprisingly with enough performance and precision, within a voltage/current range, to do very detailed experiments, like really understanding semiconductors and various component networks, through to testing complete circuits with stimulus and measurements.

    • Cancel
    • Vote Up +2 Vote Down
    • Cancel
Reply
  • shabaz
    shabaz over 3 years ago

    I bet this would be extremely popular! The ADALM1000 was a wonderful device but very version 1,0, but this newer ADALM2000 is supported a lot more with software and with educational material (complete training program!) as far as I'm aware. It is pretty much a lab-in-a-box, but surprisingly with enough performance and precision, within a voltage/current range, to do very detailed experiments, like really understanding semiconductors and various component networks, through to testing complete circuits with stimulus and measurements.