RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum ROADTEST POLL: Would You Be Interesting in Roadtesting a Data Acquisition Learning Module?
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 40 replies
  • Subscribers 2747 subscribers
  • Views 7285 views
  • Users 0 members are here
  • roadtest survey
  • adalm2000
  • analog devices
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

ROADTEST POLL: Would You Be Interesting in Roadtesting a Data Acquisition Learning Module?

rscasny
rscasny over 3 years ago

adalm2000I'm planning a roadtest on this product. I'd like to gauge your interest in roadtesting it. 

Here's some information about the product:

ADALM2000 is an (M2K) active learning module is an affordable USB-powered data acquisition module that takes the capabilities of the ADALM1000 (M1K) active learning module to the next level. With 12bit ADCs and DACs running at 100MSPS, the ADALM2000 with the Scopy software, brings the power of high performance lab equipment to the palm of your hand, enabling electrical engineering students and hobbyists to explore signals and systems into the tens of MHz without the cost and bulk associated with traditional lab gear. The ADALM2000, when coupled with Analog Devices' ScopyTm graphical application software running on a computer, provides the user with the following high performance instrumentation.

Here are some of its features:

  • Provides access to real circuits and concepts used in an actual real-time engineering environment
  • Available online resources support educator, guide students to learn difficult engineering concepts
  • Hands-on activities stimulate interest and accelerate learning in fundamental engineering concepts
  • Helps to develop critical thinking skills needed for career development
  • 16-ch digital logic analyzer (3.3V CMOS and 1.8V or 5V tolerant, 100MS/s)
  • 16-ch pattern generator (3.3V CMOS, 100MS/s), 16-ch virtual digital I/O
  • 2 input/output digital trigger signals for linking multiple instruments (3.3V CMOS)
  • Digital bus analyzers (SPI, I²C, UART, parallel)
  • 2-ch oscilloscope with differential inputs, 2-ch arbitrary function generator, 2-ch voltmeter

Here are some docs:

Datasheet

Flyer

App Notes

Here's the poll question:

  • Cancel
Parents
  • neerajrd82
    neerajrd82 over 3 years ago

    I was looking for below features in my measuring equipment:

    16-channel digital logic analyzer (3.3V CMOS and 1.8V or 5V tolerant, 100MS/s)

    16-channel virtual digital I/O

    Digital Bus Analyzers (SPI, I²C, UART, Parallel)

    Two-channel USB digital oscilloscope

    It meets more than most of my requirement. Therefore, i m interested in road test of this measuring equipment.  

    I already tested similar type of measuring equipment readily available in India as given below link:

    robodo.in/.../usb-logic-analyzer-24m-8-ch-channels-saleae-compatiable

    These features are missing in above equipment as stated below:

    1.Two-channel USB digital oscilloscope.
    2. Two-channel arbitrary function generator.

    3. 16-channel pattern generator (3.3V CMOS, 100MS/s)

    4. Two input/output digital trigger signals for linking multiple instruments (3.3V CMOS)

    5. Network analyzer – Bode, Nyquist, Nichols transfer diagrams of a circuit. Range: 1Hz to 10MHz

    6. Spectrum Analyzer – power spectrum and spectral measurements (noise floor, SFDR, SNR,
    THD, etc.)

    7. Two programmable power supplies (0...+5V , 0...-5V)

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • neerajrd82
    neerajrd82 over 3 years ago

    I was looking for below features in my measuring equipment:

    16-channel digital logic analyzer (3.3V CMOS and 1.8V or 5V tolerant, 100MS/s)

    16-channel virtual digital I/O

    Digital Bus Analyzers (SPI, I²C, UART, Parallel)

    Two-channel USB digital oscilloscope

    It meets more than most of my requirement. Therefore, i m interested in road test of this measuring equipment.  

    I already tested similar type of measuring equipment readily available in India as given below link:

    robodo.in/.../usb-logic-analyzer-24m-8-ch-channels-saleae-compatiable

    These features are missing in above equipment as stated below:

    1.Two-channel USB digital oscilloscope.
    2. Two-channel arbitrary function generator.

    3. 16-channel pattern generator (3.3V CMOS, 100MS/s)

    4. Two input/output digital trigger signals for linking multiple instruments (3.3V CMOS)

    5. Network analyzer – Bode, Nyquist, Nichols transfer diagrams of a circuit. Range: 1Hz to 10MHz

    6. Spectrum Analyzer – power spectrum and spectral measurements (noise floor, SFDR, SNR,
    THD, etc.)

    7. Two programmable power supplies (0...+5V , 0...-5V)