RoadTests & Reviews
  • Products & Partners
  • More
RoadTests & Reviews
RoadTest Forum ROADTEST POLL: Would You Be Interesting in Roadtesting a Data Acquisition Learning Module?
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 40 replies
  • Subscribers 2737 subscribers
  • Views 7586 views
  • Users 0 members are here
  • roadtest survey
  • adalm2000
  • analog devices
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

ROADTEST POLL: Would You Be Interesting in Roadtesting a Data Acquisition Learning Module?

rscasny
rscasny over 3 years ago

adalm2000I'm planning a roadtest on this product. I'd like to gauge your interest in roadtesting it. 

Here's some information about the product:

ADALM2000 is an (M2K) active learning module is an affordable USB-powered data acquisition module that takes the capabilities of the ADALM1000 (M1K) active learning module to the next level. With 12bit ADCs and DACs running at 100MSPS, the ADALM2000 with the Scopy software, brings the power of high performance lab equipment to the palm of your hand, enabling electrical engineering students and hobbyists to explore signals and systems into the tens of MHz without the cost and bulk associated with traditional lab gear. The ADALM2000, when coupled with Analog Devices' ScopyTm graphical application software running on a computer, provides the user with the following high performance instrumentation.

Here are some of its features:

  • Provides access to real circuits and concepts used in an actual real-time engineering environment
  • Available online resources support educator, guide students to learn difficult engineering concepts
  • Hands-on activities stimulate interest and accelerate learning in fundamental engineering concepts
  • Helps to develop critical thinking skills needed for career development
  • 16-ch digital logic analyzer (3.3V CMOS and 1.8V or 5V tolerant, 100MS/s)
  • 16-ch pattern generator (3.3V CMOS, 100MS/s), 16-ch virtual digital I/O
  • 2 input/output digital trigger signals for linking multiple instruments (3.3V CMOS)
  • Digital bus analyzers (SPI, I²C, UART, parallel)
  • 2-ch oscilloscope with differential inputs, 2-ch arbitrary function generator, 2-ch voltmeter

Here are some docs:

Datasheet

Flyer

App Notes

Here's the poll question:

  • Cancel
Parents
  • PaulAub
    PaulAub over 1 year ago

    Oh oh ohhhhhhhh memememememe I have been doing a lot of cool stuff with sdr and the Pluto is a wonderful tinker tool! Particularly I am experimenting in p25, dmr and trunked radio applications that can be adapted to consumer bare metal. Think "what if I could chirp via lora?" This is a fascinating time to be a maker!

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • Willjoseph
    Willjoseph over 1 year ago in reply to PaulAub

    I was caught out to bud. It's a dead thread. It's 3 years old. Was reactivated because someone removed a reply or something. 

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • Willjoseph
    Willjoseph over 1 year ago in reply to PaulAub

    I was caught out to bud. It's a dead thread. It's 3 years old. Was reactivated because someone removed a reply or something. 

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Children
  • kmikemoo
    kmikemoo over 1 year ago in reply to Willjoseph

     Willjoseph Don't write the ADALM2000 off just yet.  It was released in March of 2017 - so it wasn't exactly "new" when we Roadtested it in April of 2023.  Do check out the Roadtests that were done with the unit.
    /products/roadtest/rt/roadtests/619/sign_up_to_roadtest_2#roadtest-reviews-anchor

    There are additional Roadtests for the Pluto.  Also still relevant in 2025.

    The ADALM2000's value as a training device has not diminished one bit and is a wonderful piece of kit for anyone new to electronics.  It a great piece of gear for anyone who is not new to electronics.  Sure, it would be nice to have higher end gear, but if you are just starting out... as you stated... the ADALM2000 is a great place to start.  -Mike