RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum ROADTEST POLL: Would You Be Interesting in Roadtesting a Data Acquisition Learning Module?
  • Blogs
  • RoadTest Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 40 replies
  • Subscribers 2559 subscribers
  • Views 5954 views
  • Users 0 members are here
  • roadtest survey
  • adalm2000
  • analog devices
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

ROADTEST POLL: Would You Be Interesting in Roadtesting a Data Acquisition Learning Module?

rscasny
rscasny over 2 years ago

adalm2000I'm planning a roadtest on this product. I'd like to gauge your interest in roadtesting it. 

Here's some information about the product:

ADALM2000 is an (M2K) active learning module is an affordable USB-powered data acquisition module that takes the capabilities of the ADALM1000 (M1K) active learning module to the next level. With 12bit ADCs and DACs running at 100MSPS, the ADALM2000 with the Scopy software, brings the power of high performance lab equipment to the palm of your hand, enabling electrical engineering students and hobbyists to explore signals and systems into the tens of MHz without the cost and bulk associated with traditional lab gear. The ADALM2000, when coupled with Analog Devices' ScopyTm graphical application software running on a computer, provides the user with the following high performance instrumentation.

Here are some of its features:

  • Provides access to real circuits and concepts used in an actual real-time engineering environment
  • Available online resources support educator, guide students to learn difficult engineering concepts
  • Hands-on activities stimulate interest and accelerate learning in fundamental engineering concepts
  • Helps to develop critical thinking skills needed for career development
  • 16-ch digital logic analyzer (3.3V CMOS and 1.8V or 5V tolerant, 100MS/s)
  • 16-ch pattern generator (3.3V CMOS, 100MS/s), 16-ch virtual digital I/O
  • 2 input/output digital trigger signals for linking multiple instruments (3.3V CMOS)
  • Digital bus analyzers (SPI, I²C, UART, parallel)
  • 2-ch oscilloscope with differential inputs, 2-ch arbitrary function generator, 2-ch voltmeter

Here are some docs:

Datasheet

Flyer

App Notes

Here's the poll question:

  • Cancel

Top Replies

  • scottiebabe
    scottiebabe over 2 years ago in reply to misaz +5
    Yes, there are a lot of tough choices to make when on a limited budget. You can use digilent's waveforms with a sound card to get an idea if this type of product would be useful. I have the OEM version…
  • anniel747
    anniel747 over 2 years ago +4
    Deleted
  • javagoza
    javagoza over 2 years ago in reply to anniel747 +4
    I agree, it would be great to be able to test ADALM2000 together with ADALP2000 . I have the ADALM1000 with the ADALP2000 and it's definitely a great kit to learn on.
  • strb
    strb over 2 years ago

    I voted no but only because I don't have interest to own or test such device at the moment. However I think that it makes for a super roadtest and I'm curious to see what other people can do with it!

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • scottiebabe
    scottiebabe over 2 years ago in reply to scottiebabe

    In other news, I heard about the new AD3 from Adam Taylor

    image

    Wonder what it will cost...

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
  • javagoza
    javagoza over 2 years ago in reply to scottiebabe

    from Arrow

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Cancel
  • scottiebabe
    scottiebabe over 2 years ago in reply to javagoza

    javagoza with the pre-release pricing!! 100 Nice find Slight smile

    • Cancel
    • Vote Up +2 Vote Down
    • Cancel
  • tarna
    tarna over 2 years ago

    Does one need to have been a regular road tester to get to road test it? 

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • misaz
    misaz over 2 years ago in reply to tarna

    No, this was poll asking for intereset. Read test offer was at /products/roadtest/rt/roadtests/628/adi-adalm-pluto#pifragment-4106=9&pifragment-4100=4 but enrollment period is over now.

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
  • colporteur
    colporteur over 2 years ago in reply to tarna

    This post is used to generate interest. It is your chance to think of how you would review the equipment. Put that idea down in an application when the equipment appears in the RoadTest selection forum and you are on your way to being a RoadTester.

    This post also gives you a chance to explore the equipment. Want to know if something is included ask? Think it would be a good idea to add something, make the suggestion.

    The intention of the post is to build interest. Get members thinking about and asking about the gear. Good luck.

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
  • scottiebabe
    scottiebabe over 2 years ago in reply to javagoza

    Congrats javagoza you win the internet!

    image

    Friendly competition from ADI and the NPI has resulted in a price adjustment for the AD2 Slight smile

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • javagoza
    javagoza over 2 years ago in reply to scottiebabe

    Thanks! I will treat the internet with care

    image

    • Cancel
    • Vote Up +4 Vote Down
    • Cancel
  • walkjivefly
    walkjivefly over 2 years ago

    Looks like a useful multifunction device for those on a budget as well as the intended learning audience. I'd be happy to take one for a spin.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
<>