RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum RoadTest POLL: Would You Be Interested in Roadtesting an SDR Active Learning Module
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 28 replies
  • Subscribers 2752 subscribers
  • Views 7595 views
  • Users 0 members are here
  • ADALM-PLUTO
  • adi
  • roadtest survey
  • analog devices
  • software defined radio
  • sdr
Related

RoadTest POLL: Would You Be Interested in Roadtesting an SDR Active Learning Module

rscasny
rscasny over 3 years ago

ADALM-PLUTOI am getting to launch a roadtest on an active learning module used to learn the fundamentals of software-defined radio (SDR), radio frequency (RF), and wireless communications.

I wanted to gauge your interest in this roadtest.

Here's a some info on the product:

ADALM-PLUTO is a software-defined radio active learning module. The easy to use ADALM-PLUTO active learning module (PlutoSDR) helps introduce the fundamentals of software-defined radio (SDR), radio frequency (RF) and wireless communications.

Here are some features:

  • Portable self-contained RF learning module
  • Cost-effective experimentation platform
  • Based on Analog Devices AD9363--Highly Integrated RF Agile Transceiver and Xilinx® Zynq Z-7010 FPGA
  • RF coverage from 325MHz to 3.8GHz, up to 20MHz of instantaneous bandwidth
  • Flexible rate, 12bit ADC and DAC, GNU Radio sink and source blocks
  • MATLAB®, Simulink® support, libiio, a C, C++, C# and Python API
  • One transmitter and one receiver, half or full duplex
  • USB 2.0 powered Interface with Micro-USB 2.0 connector
  • High quality plastic enclosure

Here are some docs:

datasheet 
product overview
user guides 

For more information

Here's the poll questions:

  • Sign in to reply
  • Cancel
Parents
  • obones
    obones over 3 years ago

    Yes, I would definitely be interested with this!
    I mean, I'm already using a RTL SDR Blog receiver to "spy" on the devices emitting in the neighborhood, along with the rtl_433 project that I have even ported to ESP32 as part of experiments I do on the RFLinK32 project.

    Using such a device as the Pluto would allow to go even further to maybe finally let me figure out what the signal is from my "intelligent" water counter and the relays that have pop up in various lamp posts in the streets.

    I'll be sure to apply for this one if it becomes a roadtest.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • obones
    obones over 3 years ago

    Yes, I would definitely be interested with this!
    I mean, I'm already using a RTL SDR Blog receiver to "spy" on the devices emitting in the neighborhood, along with the rtl_433 project that I have even ported to ESP32 as part of experiments I do on the RFLinK32 project.

    Using such a device as the Pluto would allow to go even further to maybe finally let me figure out what the signal is from my "intelligent" water counter and the relays that have pop up in various lamp posts in the streets.

    I'll be sure to apply for this one if it becomes a roadtest.