RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum RoadTest POLL: Would You Be Interested in Roadtesting an SDR Active Learning Module
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 28 replies
  • Subscribers 2749 subscribers
  • Views 7711 views
  • Users 0 members are here
  • ADALM-PLUTO
  • adi
  • roadtest survey
  • analog devices
  • software defined radio
  • sdr
Related

RoadTest POLL: Would You Be Interested in Roadtesting an SDR Active Learning Module

rscasny
rscasny over 3 years ago

ADALM-PLUTOI am getting to launch a roadtest on an active learning module used to learn the fundamentals of software-defined radio (SDR), radio frequency (RF), and wireless communications.

I wanted to gauge your interest in this roadtest.

Here's a some info on the product:

ADALM-PLUTO is a software-defined radio active learning module. The easy to use ADALM-PLUTO active learning module (PlutoSDR) helps introduce the fundamentals of software-defined radio (SDR), radio frequency (RF) and wireless communications.

Here are some features:

  • Portable self-contained RF learning module
  • Cost-effective experimentation platform
  • Based on Analog Devices AD9363--Highly Integrated RF Agile Transceiver and Xilinx® Zynq Z-7010 FPGA
  • RF coverage from 325MHz to 3.8GHz, up to 20MHz of instantaneous bandwidth
  • Flexible rate, 12bit ADC and DAC, GNU Radio sink and source blocks
  • MATLAB®, Simulink® support, libiio, a C, C++, C# and Python API
  • One transmitter and one receiver, half or full duplex
  • USB 2.0 powered Interface with Micro-USB 2.0 connector
  • High quality plastic enclosure

Here are some docs:

datasheet 
product overview
user guides 

For more information

Here's the poll questions:

  • Sign in to reply
  • Cancel
Parents
  • gordonmx
    gordonmx over 3 years ago

    The ADALM-PLUTO sound very interesting, but I have a few questions.

    1) Is a Matlab license included?  It can be a time-limited license, but it would seem that a couple of months would be needed to evaluate the module.

    2) After the evaluation, if I had a specific application. would I still need Matlab to run the module?

    3) Can the Matlab libraries be used with Matlab alternatives like GNU Octave or Scilab?

    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to gordonmx

    There is a 1-month free trial on the Matlab site, which can be upgraded to a Home user license at a (relatively, and theoretically,) "low-ish" charge.

    The ADALM-PLUTO Matlab support package is a Matlab-provided download, I don't think this compatible with GNU Octave, but in theory users could create their own interface to GNU Octave if they wished, but perhaps that is not something for everyone if they just wish to use it without having to do that coding.

    Personally I think if Matlab isn't available, and if coding is desired then one may as well just use Python instead of Octave these days (since Octave isn't a full alternative to Matlab anyway), but I have not used Octave in a very long time.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 3 years ago in reply to gordonmx

    There is a 1-month free trial on the Matlab site, which can be upgraded to a Home user license at a (relatively, and theoretically,) "low-ish" charge.

    The ADALM-PLUTO Matlab support package is a Matlab-provided download, I don't think this compatible with GNU Octave, but in theory users could create their own interface to GNU Octave if they wished, but perhaps that is not something for everyone if they just wish to use it without having to do that coding.

    Personally I think if Matlab isn't available, and if coding is desired then one may as well just use Python instead of Octave these days (since Octave isn't a full alternative to Matlab anyway), but I have not used Octave in a very long time.