RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum ROADTEST POLL: Would You Be in Roadtesting a Dev Board Based on a Wi-Fi 6 Companion IC?
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 2751 subscribers
  • Views 4127 views
  • Users 0 members are here
  • NRF7002-DK
  • roadtest survey
  • nordic
  • nordic semiconductor
  • wi-fi 6
Related

ROADTEST POLL: Would You Be in Roadtesting a Dev Board Based on a Wi-Fi 6 Companion IC?

rscasny
rscasny over 3 years ago

nordic nRF7002 DKI am getting ready to launch a roadtest on a new Nordic Semiconductor Product. I'd like to gauge your interest in roadtesting it.

Here's some information about the product:

The nRF7002 DK is the development kit for the nRF7002 Wi-Fi 6 Companion IC. It contains everything needed to get started developing on a single board. The DK features an nRF5340 multiprotocol System-on-Chip (SoC) as a host processor for the nRF7002.

The DK supports the development of low-power Wi-Fi applications and enables Wi-Fi 6 features like OFDMA, Beamforming, and Target Wake Time.

The nRF7002 is a Wi-Fi 6 companion IC, providing seamless connectivity and Wi-Fi-based locationing (SSID sniffing of local Wi-Fi hubs). It is designed to be used alongside Nordic’s existing nRF52® and nRF53® Series Bluetooth Systems-on-Chip (SoCs), and nRF91® Series cellular IoT Systems-in-Package (SiPs). The nRF7002 can also be used in conjunction with non-Nordic host devices.

To communicate with the host, SPI or QSPI can be used, and an extra coexistence feature allows for seamless coexistence with other protocols like Bluetooth, Thread, or Zigbee. The nRF7002 is integrated and supported in Nordic’s nRF Connect SDK.

The nRF7002 is the first device in Nordic’s portfolio of unique Wi-Fi products that will combine seamlessly with Nordic’s existing ultra-low power technologies. Nordic bring their decades of ultra-low-power wireless IoT and silicon design expertise to Wi-Fi. Wi-Fi 6 brings added benefits to IoT applications, including further efficiency gains supporting long-life, battery-powered Wi-Fi operation.

With Wi-Fi 6, Nordic supports all wireless protocols used in Matter, Bluetooth LE for commissioning, Thread for low-power mesh, and Wi-Fi for high-throughput. Matter is a protocol championed by Apple, Amazon, Google, Nordic Semiconductor, Samsung, and hundreds of other companies in consumer IoT.

Here are a few features:

  • Supports Wi-Fi, Bluetooth Low Energy, Bluetooth mesh, NFC, Thread and Zigbee
  • nRF7002 Wi-Fi Companion IC
  • nRF5340 SoC as host processor
  • 2.4 GHz, 2.4/5 GHz, and NFC antennas
  • User-programmable LEDs(2) and buttons(2)
  • SWF RF connector for direct RF measurements
  • On-board SEGGER J-Link debugger/programmer
  • Arduino Uno Rev3 form factor

Here are some docs:

Datasheet 
Dev Tools and Downloads 

For More Indformation

Please vote in the polls below:

  • Sign in to reply
  • Cancel
Parents
  • dougw
    dougw over 3 years ago

    I think these road test pre-polls are a nice addition to the program, and the resulting discussions can be quite helpful when considering an application.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dougw
    dougw over 3 years ago

    I think these road test pre-polls are a nice addition to the program, and the resulting discussions can be quite helpful when considering an application.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Children
  • rscasny
    rscasny over 3 years ago in reply to dougw

    I will be doing these pre-polls for every roadtest this year. They give me and the sponsor some good feedback and it offers away for members to participate in the selection process. I appreciate the comments as well. 

    • Cancel
    • Vote Up +5 Vote Down