RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum ROADTEST POLL: Would You Be Interesting in Roadtesting a Source Measure Unit?
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 27 replies
  • Subscribers 2751 subscribers
  • Views 5498 views
  • Users 0 members are here
  • test equipment
  • bench wishlist
  • roadtest survey
  • source measure unit
  • SMU4201
Related

ROADTEST POLL: Would You Be Interesting in Roadtesting a Source Measure Unit?

rscasny
rscasny over 3 years ago

source measure unit AIM/TTII'm planning a roadtest on this product. I'd like to gauge your interest in roadtesting it.

Here's some information about the product:

SMU4201 is a SMU4000 series source measure unit. It provides class leading performance at a new and affordable price point for a four quadrant SMU. Combining touch screen technology with an intuitive graphical user interface provides a clear and natural flow through the test and measurement process. Integrating a fast and agile, high power four quadrant Voltage/ Current source and advanced precise Voltage/ Current meters in a compact half rack 2U casing, capable of precisely supplying positive and negative voltages, sourcing or sinking power, while simultaneously measuring both current and voltage for I-V characterizing. With high current and power combined with fast measurements and low glitch auto ranging speed, it is the ideal solution for industrial development as well as educational environments, identifying the SMU as the all-in-one solution for simplifying test applications such as battery charging/discharging, I-V characterizing, semiconductor testing and much more.

Here are some product features:

  • Maximum voltage is ±210V, voltage ranges from 20mV to 200V
  • Powerflex technology achieves full instrument output power across the majority of the voltage range
  • 0.015% basic accuracy with 6½ digit resolution
  • High speed, low glitch auto ranging capability
  • Sense terminals for 4 wire operation and guard capabilities
  • User friendly front panel GUI with on screen numeric or graphical results
  • Internally calculated resistance and power measurements
  • User settable bipolar compliance limits, variable slew rate control
  • High voltage safety interlock, user interface password protected, rear panel interlock control
  • Context sensitive help button

Here are some docs:

Data Sheet
Downloads and Manuals 

For More Information

Here are some poll questions:

  • Sign in to reply
  • Cancel
Parents
  • dougw
    dougw over 3 years ago

    Awesome instrument. Definitely would take a lot of time to review. It is so powerful, so flexible and there are so many applications....

    Pretty tough to test its accuracy but I expect most labs would struggle with that.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dougw
    dougw over 3 years ago

    Awesome instrument. Definitely would take a lot of time to review. It is so powerful, so flexible and there are so many applications....

    Pretty tough to test its accuracy but I expect most labs would struggle with that.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • charlieo21
    charlieo21 over 3 years ago in reply to dougw

    Sometimes when I saw equipment like this in roadtests I thought that I don't the skills or tools to do a proper test, but it's really exciting to think that I could test a high end equipment.