RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum ROADTEST POLL: Would You Be Interesting in Roadtesting a Source Measure Unit?
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 27 replies
  • Subscribers 2747 subscribers
  • Views 5593 views
  • Users 0 members are here
  • test equipment
  • bench wishlist
  • roadtest survey
  • source measure unit
  • SMU4201
Related

ROADTEST POLL: Would You Be Interesting in Roadtesting a Source Measure Unit?

rscasny
rscasny over 3 years ago

source measure unit AIM/TTII'm planning a roadtest on this product. I'd like to gauge your interest in roadtesting it.

Here's some information about the product:

SMU4201 is a SMU4000 series source measure unit. It provides class leading performance at a new and affordable price point for a four quadrant SMU. Combining touch screen technology with an intuitive graphical user interface provides a clear and natural flow through the test and measurement process. Integrating a fast and agile, high power four quadrant Voltage/ Current source and advanced precise Voltage/ Current meters in a compact half rack 2U casing, capable of precisely supplying positive and negative voltages, sourcing or sinking power, while simultaneously measuring both current and voltage for I-V characterizing. With high current and power combined with fast measurements and low glitch auto ranging speed, it is the ideal solution for industrial development as well as educational environments, identifying the SMU as the all-in-one solution for simplifying test applications such as battery charging/discharging, I-V characterizing, semiconductor testing and much more.

Here are some product features:

  • Maximum voltage is ±210V, voltage ranges from 20mV to 200V
  • Powerflex technology achieves full instrument output power across the majority of the voltage range
  • 0.015% basic accuracy with 6½ digit resolution
  • High speed, low glitch auto ranging capability
  • Sense terminals for 4 wire operation and guard capabilities
  • User friendly front panel GUI with on screen numeric or graphical results
  • Internally calculated resistance and power measurements
  • User settable bipolar compliance limits, variable slew rate control
  • High voltage safety interlock, user interface password protected, rear panel interlock control
  • Context sensitive help button

Here are some docs:

Data Sheet
Downloads and Manuals 

For More Information

Here are some poll questions:

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    shabaz over 3 years ago

    Wow! These roadtests are all an engineers' delight. Reviewing and reviews for any of these would be useful and enjoyable, for anyone technically inclined!!
    SMU's are (amongst other thing) like a magnifying glass for understanding semiconductor behavior.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • rscasny
    rscasny over 3 years ago in reply to shabaz

    This is just the beginning. I think this will be a good year for roadtests.

    • Cancel
    • Vote Up +8 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to rscasny

    I'm saving my joker for when a programmable DC load pops up Slight smile

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 3 years ago in reply to anniel747

    Of course this may not be its primary intended application, but there are lots of DC load applications where it could be used effectively. It is a very versatile instrument.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 3 years ago in reply to Jan Cumps

    lol this bad girl will keep you warm at night

    image

    The linus media group seem to be gearing up for something epic...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to dougw

    Hi Doug,

    It can (as a slow DC load), but I think it is low power (26W) and not expandable in this area. Whereas a typical dedicated DC load is in the hundreds of W and much faster.

    SMU is normally for slow static measurements, although this one may blur that since it's a much newer product and has some waveform capabilities.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • anniel747
    anniel747 over 3 years ago in reply to dougw
    This reply was deleted.
    • Cancel
    • Cancel
  • dougw
    dougw over 3 years ago in reply to Jan Cumps

    An SMU can be a very fast, super accurate DC load,Relaxed as I'm sure you are aware.....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Gough Lui
    Gough Lui over 3 years ago in reply to rscasny

    Well ... Aim-TTi certainly do ... Slight smile

    There's also B&K Precision (often rebranded Maynuo, ITech) which are pretty popular. In the low-end, Korad seems to be popular.

    - Gough

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Gough Lui
    Gough Lui over 3 years ago in reply to rscasny

    Well ... Aim-TTi certainly do ... Slight smile

    There's also B&K Precision (often rebranded Maynuo, ITech) which are pretty popular. In the low-end, Korad seems to be popular.

    - Gough