RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum ROADTEST POLL: Would You Be Interesting in Roadtesting a Source Measure Unit?
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 27 replies
  • Subscribers 2747 subscribers
  • Views 5579 views
  • Users 0 members are here
  • test equipment
  • bench wishlist
  • roadtest survey
  • source measure unit
  • SMU4201
Related

ROADTEST POLL: Would You Be Interesting in Roadtesting a Source Measure Unit?

rscasny
rscasny over 3 years ago

source measure unit AIM/TTII'm planning a roadtest on this product. I'd like to gauge your interest in roadtesting it.

Here's some information about the product:

SMU4201 is a SMU4000 series source measure unit. It provides class leading performance at a new and affordable price point for a four quadrant SMU. Combining touch screen technology with an intuitive graphical user interface provides a clear and natural flow through the test and measurement process. Integrating a fast and agile, high power four quadrant Voltage/ Current source and advanced precise Voltage/ Current meters in a compact half rack 2U casing, capable of precisely supplying positive and negative voltages, sourcing or sinking power, while simultaneously measuring both current and voltage for I-V characterizing. With high current and power combined with fast measurements and low glitch auto ranging speed, it is the ideal solution for industrial development as well as educational environments, identifying the SMU as the all-in-one solution for simplifying test applications such as battery charging/discharging, I-V characterizing, semiconductor testing and much more.

Here are some product features:

  • Maximum voltage is ±210V, voltage ranges from 20mV to 200V
  • Powerflex technology achieves full instrument output power across the majority of the voltage range
  • 0.015% basic accuracy with 6½ digit resolution
  • High speed, low glitch auto ranging capability
  • Sense terminals for 4 wire operation and guard capabilities
  • User friendly front panel GUI with on screen numeric or graphical results
  • Internally calculated resistance and power measurements
  • User settable bipolar compliance limits, variable slew rate control
  • High voltage safety interlock, user interface password protected, rear panel interlock control
  • Context sensitive help button

Here are some docs:

Data Sheet
Downloads and Manuals 

For More Information

Here are some poll questions:

  • Sign in to reply
  • Cancel
Parents
  • feiticeir0
    feiticeir0 over 3 years ago

    I haven't the foggiest idea on how to use this ! Slight smile

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to feiticeir0

    It's like a power supply and voltmeter/ammeter all-in-one. However, it is extremely granular, so that you can (say) apply even a fraction of a microvolt, whereas a normal power supply would be in the tens or hundreds of millivolts. You can use it to either power or act as stimulus for (say) components, although it is not limited to that.

    It can be used like a curve tracer if desired, applying a range of voltage (or current) to (say) a transistor of some sort.

    It is best explained with this diagram from the datasheet:

    image

    It's excellent for seeing how (say) semiconductors behave. Lots of the nice charts in datasheets would require such a SMU device to create.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • feiticeir0
    feiticeir0 over 3 years ago in reply to shabaz

    Thank you for the explanation. This is something for hard core electronics engineers ! Slight smile

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to javagoza

    That's a fun product to use! And a very valuable experience for students to be able to tweak things and immediately see the effect, compared to trying to figure out things from diagrams alone. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • javagoza
    javagoza over 3 years ago in reply to javagoza

    shabaz  posted a great intro to the ADALM1000: Getting Started with the Active Learning Module ADALM1000 - Blog - Test & Tools - element14 Community

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • javagoza
    javagoza over 3 years ago in reply to feiticeir0

    You can access a very affordable SMU with the Analog Devices ADALM1000 active learning module
    You can use it to check the characteristics of diodes, BJTs and MOSFET devices. The ADALM1000 has its limitations, the two SMU channels can only produce 0 to +5V voltage with respect to ground. But by combining both channels you can also sweep the voltage from -2.5 V to +2.5 V
    You can use the ADALM1000 to study the electrical characteristics of any component at DC or low frequencies in a voltage range of -5 to +5 V, measuring current from +/- 0.1 to 180 mA, for about 65 EUR. Anytime you need to collect a lot of data to plot or graph performance over time, a programmable SMU is a big help.

    I have been able to carry out with the ADALM10000 many of the experiments that I could not do when I was studying due to lack of resources at my University.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • javagoza
    javagoza over 3 years ago in reply to feiticeir0

    You can access a very affordable SMU with the Analog Devices ADALM1000 active learning module
    You can use it to check the characteristics of diodes, BJTs and MOSFET devices. The ADALM1000 has its limitations, the two SMU channels can only produce 0 to +5V voltage with respect to ground. But by combining both channels you can also sweep the voltage from -2.5 V to +2.5 V
    You can use the ADALM1000 to study the electrical characteristics of any component at DC or low frequencies in a voltage range of -5 to +5 V, measuring current from +/- 0.1 to 180 mA, for about 65 EUR. Anytime you need to collect a lot of data to plot or graph performance over time, a programmable SMU is a big help.

    I have been able to carry out with the ADALM10000 many of the experiments that I could not do when I was studying due to lack of resources at my University.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Children
  • shabaz
    shabaz over 3 years ago in reply to javagoza

    That's a fun product to use! And a very valuable experience for students to be able to tweak things and immediately see the effect, compared to trying to figure out things from diagrams alone. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • javagoza
    javagoza over 3 years ago in reply to javagoza

    shabaz  posted a great intro to the ADALM1000: Getting Started with the Active Learning Module ADALM1000 - Blog - Test & Tools - element14 Community

    • Cancel
    • Vote Up +3 Vote Down