RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum ROADTEST POLL: Would You Be Interesting in Roadtesting a Source Measure Unit?
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 27 replies
  • Subscribers 2751 subscribers
  • Views 5523 views
  • Users 0 members are here
  • test equipment
  • bench wishlist
  • roadtest survey
  • source measure unit
  • SMU4201
Related

ROADTEST POLL: Would You Be Interesting in Roadtesting a Source Measure Unit?

rscasny
rscasny over 3 years ago

source measure unit AIM/TTII'm planning a roadtest on this product. I'd like to gauge your interest in roadtesting it.

Here's some information about the product:

SMU4201 is a SMU4000 series source measure unit. It provides class leading performance at a new and affordable price point for a four quadrant SMU. Combining touch screen technology with an intuitive graphical user interface provides a clear and natural flow through the test and measurement process. Integrating a fast and agile, high power four quadrant Voltage/ Current source and advanced precise Voltage/ Current meters in a compact half rack 2U casing, capable of precisely supplying positive and negative voltages, sourcing or sinking power, while simultaneously measuring both current and voltage for I-V characterizing. With high current and power combined with fast measurements and low glitch auto ranging speed, it is the ideal solution for industrial development as well as educational environments, identifying the SMU as the all-in-one solution for simplifying test applications such as battery charging/discharging, I-V characterizing, semiconductor testing and much more.

Here are some product features:

  • Maximum voltage is ±210V, voltage ranges from 20mV to 200V
  • Powerflex technology achieves full instrument output power across the majority of the voltage range
  • 0.015% basic accuracy with 6½ digit resolution
  • High speed, low glitch auto ranging capability
  • Sense terminals for 4 wire operation and guard capabilities
  • User friendly front panel GUI with on screen numeric or graphical results
  • Internally calculated resistance and power measurements
  • User settable bipolar compliance limits, variable slew rate control
  • High voltage safety interlock, user interface password protected, rear panel interlock control
  • Context sensitive help button

Here are some docs:

Data Sheet
Downloads and Manuals 

For More Information

Here are some poll questions:

  • Sign in to reply
  • Cancel
  • michaelkellett
    michaelkellett over 3 years ago

    I've had my eye on these (there are two versions) since they came out.

    It gets the SMU down to a reasonable price point and my experience of other AIM_TTi products is that it is likely to deliver what it promises. (I have several power supplies and a 3GHz signal generator from them.)

    A good Roadtest will take some time because serious work with an SMU usually invloves both programming and making test fixtures.

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • rsjawale24
    rsjawale24 over 3 years ago

    Another interesting roadtest! 
    I remember using an SMU for the first time during my VLSI technology lab. 
    I have a picture of the wafer somewhere, on which I had designed a memristor and validated its performance using a Keithley SMU.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to dougw

    Hi Doug,

    It can (as a slow DC load), but I think it is low power (26W) and not expandable in this area. Whereas a typical dedicated DC load is in the hundreds of W and much faster.

    SMU is normally for slow static measurements, although this one may blur that since it's a much newer product and has some waveform capabilities.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • anniel747
    anniel747 over 3 years ago in reply to dougw
    [deleted]
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 3 years ago in reply to Jan Cumps

    An SMU can be a very fast, super accurate DC load,Relaxed as I'm sure you are aware.....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • feiticeir0
    feiticeir0 over 3 years ago in reply to shabaz

    Thank you for the explanation. This is something for hard core electronics engineers ! Slight smile

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to feiticeir0

    It's like a power supply and voltmeter/ammeter all-in-one. However, it is extremely granular, so that you can (say) apply even a fraction of a microvolt, whereas a normal power supply would be in the tens or hundreds of millivolts. You can use it to either power or act as stimulus for (say) components, although it is not limited to that.

    It can be used like a curve tracer if desired, applying a range of voltage (or current) to (say) a transistor of some sort.

    It is best explained with this diagram from the datasheet:

    image

    It's excellent for seeing how (say) semiconductors behave. Lots of the nice charts in datasheets would require such a SMU device to create.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • Gough Lui
    Gough Lui over 3 years ago in reply to rscasny

    Well ... Aim-TTi certainly do ... Slight smile

    There's also B&K Precision (often rebranded Maynuo, ITech) which are pretty popular. In the low-end, Korad seems to be popular.

    - Gough

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • feiticeir0
    feiticeir0 over 3 years ago

    I haven't the foggiest idea on how to use this ! Slight smile

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • rscasny
    rscasny over 3 years ago in reply to Jan Cumps

    programmable dc load. Let me see who makes them and I'll ask.

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
<>