RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum ROADTEST POLL: Would You Be Interesting in Roadtesting a Multi-Hub Antenna?
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 14 replies
  • Subscribers 2752 subscribers
  • Views 4284 views
  • Users 0 members are here
  • multi-hub antenna
  • molex
  • 217853-1000
  • 216589-1000
  • roadtest survey
  • antenna
Related

ROADTEST POLL: Would You Be Interesting in Roadtesting a Multi-Hub Antenna?

rscasny
rscasny over 3 years ago

I have been in conversation with the roadtest sponsor about roadtesting a multi-hub antenna.

We both would like to to more activities around antennas, but we don't know much interest there would be in this particular product. Thus, I'm running this poll to gauge your interest in roadtesting it.

Here's some information about the product:

imageMulti-hub 5 in 1 external antenna

A multi-hub 5 in 1 external antenna including 2x 5G/LTE, 2 x WiFi and 1x GNSS. It provides 5G MIMO and Wi-Fi MIMO antenna system within compact antenna box and use in automotive telematics, transportation and remote monitoring applications.

Features

  • Working frequency 698-960MHz/1500-1700MHz /1710-2690MHz/3300-5000MHz for 5G/LTE
    MIMO, Frequency 2400-2500MHz/5000-6000MHz for WIFI MIMO, 1561-1602MHz for GNSS
  • Antenna Size:155x65x20mm with 1000mm Cable Length
  • Connector Type: SMA (M) ST
  • IP67

Here are some docs:

Datasheet

Product Specs

Application Specs

For other information

 imageMulti-hub antenna 7-in-1

A Multi-hub 7-in-1 Antenna including 2 x LTE/5G full band, 2 x LTE/5G high band, 2 x WI-FI, and 1x GNSS. It provides LTE/5G 4 x 4 MIMO, WI-FI 2 x 2 MIMO and GNSS antenna system within compact antenna box and use in automotive telematics, transportation and remote monitoring applications.

Features

  • Working frequency 600-960MHz/1400-1550MHz/1710-2690MHz/3300-5000MHz for 5G MIMO, Frequency 2400-2500MHz/5150-5850MHz/5925-7125MHz for WIFI MIMO, 1561-1602MHz for GNSS
  • Antenna Size:160x115x22.5mm with 1000mm Cable Length
  • Connector Type: SMA (M)
  • IPX7

Here are some docs:

Datasheet

Product Specs

Application Specs

For other information

  • Sign in to reply
  • Cancel
Parents
  • mp2100
    mp2100 over 3 years ago

    I am fascinated by antennas, and that they work as well as they do.  These seem mostly designed for 5G, and I don't have anything with those high frequencies.  I have LoRa boards.  And I have a cheap VNA, only goes up to 2Ghz though.  I said maybe, but doing a thorough test is difficult.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • mp2100
    mp2100 over 3 years ago

    I am fascinated by antennas, and that they work as well as they do.  These seem mostly designed for 5G, and I don't have anything with those high frequencies.  I have LoRa boards.  And I have a cheap VNA, only goes up to 2Ghz though.  I said maybe, but doing a thorough test is difficult.