RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Should you have to pay to opt-in to a RoadTest ?
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 40 replies
  • Subscribers 2751 subscribers
  • Views 7837 views
  • Users 0 members are here
  • RoadTest
  • product review
  • Pay to RoadTest
  • Cost of RoadTest
  • application
  • roadtest review
Related

Should you have to pay to opt-in to a RoadTest ?

cstanton
cstanton over 3 years ago

"No"

Is probably what's already on your fingers ready to type in reply, and that's fine.

Each year I took part in "Reddit Secret Santa", where you're matched against another person, who you find information about, and send them a secret santa gift for Christmas.

Someone matches with you, and you hope that they will send you something, after all, they signed up for the Secret Santa.

A few years in a row, I was 'shafted' and wasn't sent anything, sometimes in these cases, you're matched up with a new Secret Santa and then sent something, unfortunately that didn't happen either.

This caused a bit of an uproar in Reddit, while people were happy if they got anything and knew they weren't necessarily entitled to anything, they felt that it wasn't quite in the spirit of things.

So along came the idea of becoming an 'Elf'. You paid $5 to enter the Reddit Secret Santa, and that put you against other people who had also paid $5, the idea being because you'd all invested a base amount in it, you're more inclined to make sure that the person you're matched with will get a present, and you yourself will get a present, and you're supporting Reddit at the same time. Everyone wins and you're invested in it.

This pretty much worked for Reddit, paying into something seems to 'click' with people that you want to be with others, so you're paying the 'premium' to get into that rather than anyone who can sign up and looking for a freebie without paying it forward. A bit capitalist but some people like to support things.

There are other mechanisms that they use for reputation with Secret Santa, when you successfully enter a Secret Santa you gain a token, you gain another token for sending off your 'Parcel', and you gain another token for marking your parcel as received, and you gain another token when your Secret Santee receives your Parcel. You can then 'spend' these tokens to enter another Reddit Secret Santa. Don't do these? Well, you don't get your tokens. Though even this has mechanisms where "what if you just create another account?" and "how do you get tokens if you want to redeem yourself?" - I'm sure some vetting and mechanism is involved there, too, but ultimately there's also weight to paying to opt-in with like-minded people.

Which puts the thought of "Should you have to pay to opt-in to a RoadTest" ?

We've had members over the years that receive equipment, and they run off with it and don't do a RoadTest. This harms the Community, and it harms the suppliers when they provide the hardware (especially if it's early access hardware).

How would this work? I'm not entirely sure.

Would you have to pay-in to apply to the RoadTest?

Would you only pay-in when you're chosen to write the RoadTest review (so before you receive the hardware), would it be a deposit?

Which is reimbursed when you've wrote the RoadTest Review? (I think I'd prefer the deposit idea out of any of these).

Would we only do this for RoadTest kit over a certain value?

We have no plans whatsoever at implementing anything like this, this's the first time I've brought it up to anyone (including to the Community team itself), it's simply a thought passing my mind. We also don't intend on implementing this from any outcome of this conversation - though if I could at least do the 'token/points' system, I'd consider that, handling money is dangerous, but accountability matters.

But perhaps a bit of reflection on the fact that we don't do this will give some people who consider a RoadTest pause for thought.

Thanks to all members of the Community that enters a RoadTest and writes your RoadTest reviews, and those who keep applying for a RoadTest even if you aren't chosen for that particular item. We appreciate you.

  • Sign in to reply
  • Cancel
Parents
  • michaelkellett
    michaelkellett over 3 years ago

    I don't much like the idea.

    I have one very technical reason - in the UK a competition being free to enter is a big legal consideration on the tax status of prizes. If one had to pay to enter a roadtest this might cause problems. (You'll need a legal opinion to be sure on this one !)

    But in  a more general sense I think road tests are going well as they are. I'm sure that incremental improvements are possible and desireable but I wouldn't make big changes to something that isn't broken.

    I suspect that Randall's running of the programme has a good deal to do with this.

    Most of the Road Test gear comes from suppliers who are trading the production cost of the item for exposure and a review. They also give stuff to "influencers". I think its good that E14 provides an alternative path where people who don't have thousands of followers (or any money) get  a look in.

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • michaelkellett
    michaelkellett over 3 years ago

    I don't much like the idea.

    I have one very technical reason - in the UK a competition being free to enter is a big legal consideration on the tax status of prizes. If one had to pay to enter a roadtest this might cause problems. (You'll need a legal opinion to be sure on this one !)

    But in  a more general sense I think road tests are going well as they are. I'm sure that incremental improvements are possible and desireable but I wouldn't make big changes to something that isn't broken.

    I suspect that Randall's running of the programme has a good deal to do with this.

    Most of the Road Test gear comes from suppliers who are trading the production cost of the item for exposure and a review. They also give stuff to "influencers". I think its good that E14 provides an alternative path where people who don't have thousands of followers (or any money) get  a look in.

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Children
  • obones
    obones over 3 years ago in reply to michaelkellett

    If there is a price to pay, there is indeed a very serious risk of taxation on import, and even "customs fee" required by the carrier. Note that in France this "customs fee" is not paid back to the customs office but goes entirely in the carrier pocket.

    About 8 years ago I was sent a product by a customer who wanted me to fix the bug he was encountering with that specific equipment. Despite the correct "zero dollars / sample" documentation coming with it, the carrier asked for that "customs fee". Hopefully I could get it waived by proving it was a free equipment, but it's quite a tedious process. And I can't imagine how complex it would be to explain to a stubborn carrier representative that the amount of money is just a deposit.

    That being said, I understand the need to avoid "run away" applicants, but I fear that this would be yet another case of burdening the good guys for a minority of rotten apples.