RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Should you have to pay to opt-in to a RoadTest ?
  • Blogs
  • RoadTest Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 40 replies
  • Subscribers 2664 subscribers
  • Views 7219 views
  • Users 0 members are here
  • RoadTest
  • product review
  • Pay to RoadTest
  • Cost of RoadTest
  • application
  • roadtest review
Related

Should you have to pay to opt-in to a RoadTest ?

cstanton
cstanton over 3 years ago

"No"

Is probably what's already on your fingers ready to type in reply, and that's fine.

Each year I took part in "Reddit Secret Santa", where you're matched against another person, who you find information about, and send them a secret santa gift for Christmas.

Someone matches with you, and you hope that they will send you something, after all, they signed up for the Secret Santa.

A few years in a row, I was 'shafted' and wasn't sent anything, sometimes in these cases, you're matched up with a new Secret Santa and then sent something, unfortunately that didn't happen either.

This caused a bit of an uproar in Reddit, while people were happy if they got anything and knew they weren't necessarily entitled to anything, they felt that it wasn't quite in the spirit of things.

So along came the idea of becoming an 'Elf'. You paid $5 to enter the Reddit Secret Santa, and that put you against other people who had also paid $5, the idea being because you'd all invested a base amount in it, you're more inclined to make sure that the person you're matched with will get a present, and you yourself will get a present, and you're supporting Reddit at the same time. Everyone wins and you're invested in it.

This pretty much worked for Reddit, paying into something seems to 'click' with people that you want to be with others, so you're paying the 'premium' to get into that rather than anyone who can sign up and looking for a freebie without paying it forward. A bit capitalist but some people like to support things.

There are other mechanisms that they use for reputation with Secret Santa, when you successfully enter a Secret Santa you gain a token, you gain another token for sending off your 'Parcel', and you gain another token for marking your parcel as received, and you gain another token when your Secret Santee receives your Parcel. You can then 'spend' these tokens to enter another Reddit Secret Santa. Don't do these? Well, you don't get your tokens. Though even this has mechanisms where "what if you just create another account?" and "how do you get tokens if you want to redeem yourself?" - I'm sure some vetting and mechanism is involved there, too, but ultimately there's also weight to paying to opt-in with like-minded people.

Which puts the thought of "Should you have to pay to opt-in to a RoadTest" ?

We've had members over the years that receive equipment, and they run off with it and don't do a RoadTest. This harms the Community, and it harms the suppliers when they provide the hardware (especially if it's early access hardware).

How would this work? I'm not entirely sure.

Would you have to pay-in to apply to the RoadTest?

Would you only pay-in when you're chosen to write the RoadTest review (so before you receive the hardware), would it be a deposit?

Which is reimbursed when you've wrote the RoadTest Review? (I think I'd prefer the deposit idea out of any of these).

Would we only do this for RoadTest kit over a certain value?

We have no plans whatsoever at implementing anything like this, this's the first time I've brought it up to anyone (including to the Community team itself), it's simply a thought passing my mind. We also don't intend on implementing this from any outcome of this conversation - though if I could at least do the 'token/points' system, I'd consider that, handling money is dangerous, but accountability matters.

But perhaps a bit of reflection on the fact that we don't do this will give some people who consider a RoadTest pause for thought.

Thanks to all members of the Community that enters a RoadTest and writes your RoadTest reviews, and those who keep applying for a RoadTest even if you aren't chosen for that particular item. We appreciate you.

  • Sign in to reply
  • Cancel

Top Replies

  • Gough Lui
    Gough Lui over 3 years ago +7
    As a RoadTest veteran with 34 completed (and on-time) RoadTests since my first in 2013, I’ll offer my 2c, as the topic of people running away with equipment and/or producing sub-standard reviews seems…
  • rscasny
    rscasny over 3 years ago +7
    This is a great discussion. Thanks all for participating in it. Just to be honest with you: I am not interested (nor anyone on the element14 team) would want pay-up-front roadtests. Such a policy might…
  • shabaz
    shabaz over 3 years ago +5
    I think it might put off a lot of people, especially students and new grads, but still, sometimes raising something like this can make people brainstorm : ) Maybe the issue can be more generalized, into…
Parents
  • Andrew J
    Andrew J over 3 years ago

    It’s a good question:  I’ve seen some questionable reviews which I felt meant that some one more genuine missed out.  There will always be abusers of any system,  particularly when the participant base is so extensive.  I had previously thought about a deposit-type system but couldn’t see it working for all the reasons mentioned above.  

    An idea I thought might work would be self-qualifying for a roadtester pool.  To get into this pool, a member must submit a roadtest of something that they already own that is sufficiently distinct to any other roadtest of the same thing and of interest to the wider membership.  There’s plenty of examples to draw from and comments on the blog can help someone genuinely interested to improve their review.  It doesn’t even need to be a complicated piece of equipment - I’ve roadtested a cable detector and a set of screwdrivers is up for test - (or maybe it it does to demonstrate commitment??) and could be a series of posts about developing a specific software solution for a SBC, for example.  The point is to show commitment and willingness to get into detail. Anyone who has completed a roadtest before is already in the pool, and anyone who has already blogged a number of times could auto-qualify at E14’s discretion.  Isn’t there/didn’t there use to be a question about community participation?  This may still be abused of course, but does require someone to put some effort in first.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Andrew J
    Andrew J over 3 years ago

    It’s a good question:  I’ve seen some questionable reviews which I felt meant that some one more genuine missed out.  There will always be abusers of any system,  particularly when the participant base is so extensive.  I had previously thought about a deposit-type system but couldn’t see it working for all the reasons mentioned above.  

    An idea I thought might work would be self-qualifying for a roadtester pool.  To get into this pool, a member must submit a roadtest of something that they already own that is sufficiently distinct to any other roadtest of the same thing and of interest to the wider membership.  There’s plenty of examples to draw from and comments on the blog can help someone genuinely interested to improve their review.  It doesn’t even need to be a complicated piece of equipment - I’ve roadtested a cable detector and a set of screwdrivers is up for test - (or maybe it it does to demonstrate commitment??) and could be a series of posts about developing a specific software solution for a SBC, for example.  The point is to show commitment and willingness to get into detail. Anyone who has completed a roadtest before is already in the pool, and anyone who has already blogged a number of times could auto-qualify at E14’s discretion.  Isn’t there/didn’t there use to be a question about community participation?  This may still be abused of course, but does require someone to put some effort in first.

    • Cancel
    • Vote Up +5 Vote Down