RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Should you have to pay to opt-in to a RoadTest ?
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 40 replies
  • Subscribers 2751 subscribers
  • Views 7846 views
  • Users 0 members are here
  • RoadTest
  • product review
  • Pay to RoadTest
  • Cost of RoadTest
  • application
  • roadtest review
Related

Should you have to pay to opt-in to a RoadTest ?

cstanton
cstanton over 3 years ago

"No"

Is probably what's already on your fingers ready to type in reply, and that's fine.

Each year I took part in "Reddit Secret Santa", where you're matched against another person, who you find information about, and send them a secret santa gift for Christmas.

Someone matches with you, and you hope that they will send you something, after all, they signed up for the Secret Santa.

A few years in a row, I was 'shafted' and wasn't sent anything, sometimes in these cases, you're matched up with a new Secret Santa and then sent something, unfortunately that didn't happen either.

This caused a bit of an uproar in Reddit, while people were happy if they got anything and knew they weren't necessarily entitled to anything, they felt that it wasn't quite in the spirit of things.

So along came the idea of becoming an 'Elf'. You paid $5 to enter the Reddit Secret Santa, and that put you against other people who had also paid $5, the idea being because you'd all invested a base amount in it, you're more inclined to make sure that the person you're matched with will get a present, and you yourself will get a present, and you're supporting Reddit at the same time. Everyone wins and you're invested in it.

This pretty much worked for Reddit, paying into something seems to 'click' with people that you want to be with others, so you're paying the 'premium' to get into that rather than anyone who can sign up and looking for a freebie without paying it forward. A bit capitalist but some people like to support things.

There are other mechanisms that they use for reputation with Secret Santa, when you successfully enter a Secret Santa you gain a token, you gain another token for sending off your 'Parcel', and you gain another token for marking your parcel as received, and you gain another token when your Secret Santee receives your Parcel. You can then 'spend' these tokens to enter another Reddit Secret Santa. Don't do these? Well, you don't get your tokens. Though even this has mechanisms where "what if you just create another account?" and "how do you get tokens if you want to redeem yourself?" - I'm sure some vetting and mechanism is involved there, too, but ultimately there's also weight to paying to opt-in with like-minded people.

Which puts the thought of "Should you have to pay to opt-in to a RoadTest" ?

We've had members over the years that receive equipment, and they run off with it and don't do a RoadTest. This harms the Community, and it harms the suppliers when they provide the hardware (especially if it's early access hardware).

How would this work? I'm not entirely sure.

Would you have to pay-in to apply to the RoadTest?

Would you only pay-in when you're chosen to write the RoadTest review (so before you receive the hardware), would it be a deposit?

Which is reimbursed when you've wrote the RoadTest Review? (I think I'd prefer the deposit idea out of any of these).

Would we only do this for RoadTest kit over a certain value?

We have no plans whatsoever at implementing anything like this, this's the first time I've brought it up to anyone (including to the Community team itself), it's simply a thought passing my mind. We also don't intend on implementing this from any outcome of this conversation - though if I could at least do the 'token/points' system, I'd consider that, handling money is dangerous, but accountability matters.

But perhaps a bit of reflection on the fact that we don't do this will give some people who consider a RoadTest pause for thought.

Thanks to all members of the Community that enters a RoadTest and writes your RoadTest reviews, and those who keep applying for a RoadTest even if you aren't chosen for that particular item. We appreciate you.

  • Sign in to reply
  • Cancel
Parents
  • feiticeir0
    feiticeir0 over 3 years ago

    Hi  !

    I love your sentiment and see where you are going and I must agree.

    People who will pay for it - I'm not discussing the amount - will more likely do the road test than those who don't.  Still, most of the time, the products from the road test are more valuable than the price one would pay for it, making it desirable to still pay less for a "freebie" and still don't do the road test ! Slight smile

    Just to put it out there, a alternate solution would be to allow to participate in the road tests just Element14's members that are above certain points - this way is a certain that those members are in for the real thing - since they are members for some time and really participate in the community - and not just for the free stuff. This would exclude some, but this way those who're excluded will participate more for the change to participate in the road test.

    If you fell that this will not work, maybe just do it for some products - the more expensive ones .

    Well, just my two cents.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • embeddedguy
    embeddedguy over 3 years ago in reply to feiticeir0

    Previously element14 road test application form had something that was asking questions to the user that have you participated in road test or already wrote a blog, or asked a question in the forum?

    I think that is a good approach that if person is really sincere he/she would/should have done something before that they can get a free product. Isn't it so?

    The application form now does not seems to have these kinda questions anymore..Grin

    Anyways for the road test, you may wanna have some per-condition to apply.

    With payment and stuff things can get quite complected as well specially for international transfer and charges etc. This will be like more work on both side also from your end it will require more work to manage payments etc.

    So my idea would be to use some active contribution of user to approve them for the road test for not very expensive products..

    For expensive products such as scopes and other instruments, there might be this option?Stuck out tongue

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 3 years ago in reply to embeddedguy
    embeddedguy said:
    Previously element14 road test application form had something that was asking questions to the user that have you participated in road test or already wrote a blog, or asked a question in the forum?

    Thanks to the awareness of the site's capability of reporting we don't need to directly ask these questions.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • cstanton
    cstanton over 3 years ago in reply to embeddedguy
    embeddedguy said:
    Previously element14 road test application form had something that was asking questions to the user that have you participated in road test or already wrote a blog, or asked a question in the forum?

    Thanks to the awareness of the site's capability of reporting we don't need to directly ask these questions.