RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum ROADTEST POLL: Would You Be Interested in Roadtesting the New Low-Cost ZYNQ UltraScale+ MPSOC Dev Kit?
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 2751 subscribers
  • Views 3293 views
  • Users 0 members are here
  • Zynq™ UltraScale+™ MPSoC
  • ZUBoard 1CG
  • roadtest survey
  • amd
Related

ROADTEST POLL: Would You Be Interested in Roadtesting the New Low-Cost ZYNQ UltraScale+ MPSOC Dev Kit?

rscasny
rscasny over 3 years ago

imageI plan on roadtesting this board in May. I'll be getting 10 kits. Let me tell you about the main attraction.

Some element14 members are familiar with the Ultra96-V2 dev kit, which uses the Zynq UltraScale+ MPSoC ZU3EG A484 device. This new board also uses the Zynq UltraScale+ MPSoC, but a different version of device, the AMD ZU+ MPSoC ZU1CG. The ZU1CG device is a low-cost, dual-core entry point to Heterogeneous (Processor + FPGA fabric) Processing. Being a low-cost device opens things up for a lot more developers.

Here are a few details:

The ZUBoard 1CG provides the flexibility and versatility for engineers to experiment with and learn the AMD Zynq ® UltraScale+ Tm architecture. The affordable ZU1CG device features 81K programmable logic cells with a Dual-core Arm ® Cortex ®-A53 MPCore Tm and Dual-core Arm Cortex-R5F MPCore, as well as cache and on-chip memory. The board also features 1GB of ISSI LPDDR4 with non-volatile boot options in the 256Mb ISSI QSPI Flash or a microSD card slot. Microchip PHYs enable both 10/100/1000 Ethernet and USB 2.0 Host. A microUSB port provides on-board JTAG/UART access. Microchip oscillators and ECS crystals provide clocking to the ZU1 device, the on-chip real-time clock, JTAG, and communication interfaces. Power the board through USB-C with a Microchip controller and TDK μPOL Tm power modules.

Here are some links to documentation:

Datasheet 
Getting Started Guide 
Hardware Guide 
Schematic 
Project 

For More Information

Prospective Roadtester Polls

Please vote in these polls. They provide us insights into how you view this roadtest. Thanks.

  • Sign in to reply
  • Cancel
Parents
  • manojroy123
    manojroy123 over 3 years ago

    I have seen it's price . it is more than 2000 USD. How can you call it an inexpensive board

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rscasny
    rscasny over 3 years ago in reply to manojroy123

    I think you are looking at the wrong product.  While some of the ZYNQ UltraScale+ dev boards are expensive, this particular board is thee least expensive

    I see there are difference prices. If you go to AVNET.com, it's $159 ZUBoard-1CG | Avnet Boards

    Make sure you look at the ZU+ CG version. There are two other versions: EG and EV, which are more expensive, I believe.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dang74
    dang74 over 3 years ago in reply to rscasny

    The $159 price point seems like a bargain when you consider its very capable FPGA SoC.  I imagine there will be some pretty impress RoadTests.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dang74
    dang74 over 3 years ago in reply to rscasny

    The $159 price point seems like a bargain when you consider its very capable FPGA SoC.  I imagine there will be some pretty impress RoadTests.