RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Would You Be Interested in Roadtesting KiCad EDA?
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 77 replies
  • Subscribers 2746 subscribers
  • Views 11497 views
  • Users 0 members are here
  • kicad
  • roadtest survey
Related

Would You Be Interested in Roadtesting KiCad EDA?

rscasny
rscasny over 3 years ago

KiCad has a following on the element14 Community, so we figured it would be a good thing to roadtest. It's a little different than what we usually roadtest, so we have a few questions. KiCad is free, so we were wondering what the potential roadtesters would like to see in the roadtest kit. There was a suggestion for the roadtesters to design a Raspberry Pi HAT. But we could also use a Pi/Ardunio library or even someone's own design. 

I have some polls below. I'd appreciate you voting. Thanks.


  • Sign in to reply
  • Cancel
Parents
  • Gough Lui
    Gough Lui over 3 years ago

    I have used KiCad since V5 and it's been relatively good. I mean - I didn't love EAGLE and I generally don't like vendor-lock-in. Being free and open source is a big positive.

    If it is to be RoadTested, I will echo the requests of others, but slightly differently - I'd like to see multiple board manufacturing runs being paid for as part of the deal. This is because (as we usually know) we don't always get the board right the first time. It might also be good to test different board designs (even if we do get it right) say the use of 2-layer, 4-layer or higher, and or materials (e.g. single-sided MCPCB). It would also be nice to understand how well it handles the manufacturing aspects - do users get their BOMs, CPLs right for the manufacturing house - so if assembly and parts are included, that would be even sweeter. Perhaps this last part can be a one-off batch of 5, but the others could be board-only for 2-layer, board-only for 4-layer, board-only for MCPCB (perhaps with a choice of colour and thickness, just in case someone wants to make a connectorless USB gadget).

    As a result, it would become more of a "project" RoadTest ... the costs may vary per participant due to shipping and duties as well, but I can't see the software being given a proper show without bringing it all the way from desk to finalised item(s).

    - Gough

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 3 years ago in reply to Gough Lui
    Gough Lui said:
    I'd like to see multiple board manufacturing runs being paid for as part of the deal

    That sounds more like a roadtest of the board manufacturers.

    Gough Lui said:
    As a result, it would become more of a "project" RoadTest

    I call that feature creep ;)

    When I proposed this idea, one of the comments back was "well this sounds like a design challenge" and it can easily explode to be one, and I had put it forward as being one (design a raspberry pi hat, since we have a raspberry pi design challenge each year) but there's concern over doing that in being able to 'pull in' the right people, and get the right people's attention to have the knowledge to enter that competition (I'll openly admit, that with our current facilities and methods we struggle to get reach for applicants for the really technical competitions and that makes the team uneasy).

    So this would focus more on the software side, with maybe fabrication depending on it, but we wouldn't want to put people off and feel they need to make a completed product. I don't believe testing software should have that as a requirement.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Gough Lui
    Gough Lui over 3 years ago in reply to cstanton
    cstanton said:
    roadtest of the board manufacturers

    Well .. if it all comes from the same manufacturer, then perhaps it's a bit of a sampler of the capabilities. But alas, the way the EDA handles and exports outputs for each board type may be subtly different. What works fine for 2-layer may become tricky for 6-layer. Regardless, I think there should be an allowance for mistakes that can't be "bodge-wired" away ... it happens to me often enough to admit it ...

    cstanton said:
    "well this sounds like a design challenge"

    Well, it's in the name, EDA, the "design" part. Wouldn't be a proper use of EDA if it wasn't to design something ...

    cstanton said:
    focus more on the software side

    I still feel that the purpose of an EDA is to build the files necessary to generate a physical item. If you don't do the final step, you may never know that you have to hand-massage filenames, tick a myriad of cryptic boxes to make it all work ... I see the physical form as "proof of success". Without it, given the software is free, what is the incentive for the RoadTester?

    - Gough

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Gough Lui
    Gough Lui over 3 years ago in reply to cstanton
    cstanton said:
    roadtest of the board manufacturers

    Well .. if it all comes from the same manufacturer, then perhaps it's a bit of a sampler of the capabilities. But alas, the way the EDA handles and exports outputs for each board type may be subtly different. What works fine for 2-layer may become tricky for 6-layer. Regardless, I think there should be an allowance for mistakes that can't be "bodge-wired" away ... it happens to me often enough to admit it ...

    cstanton said:
    "well this sounds like a design challenge"

    Well, it's in the name, EDA, the "design" part. Wouldn't be a proper use of EDA if it wasn't to design something ...

    cstanton said:
    focus more on the software side

    I still feel that the purpose of an EDA is to build the files necessary to generate a physical item. If you don't do the final step, you may never know that you have to hand-massage filenames, tick a myriad of cryptic boxes to make it all work ... I see the physical form as "proof of success". Without it, given the software is free, what is the incentive for the RoadTester?

    - Gough

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • cstanton
    cstanton over 3 years ago in reply to Gough Lui
    Gough Lui said:
    I still feel that the purpose of an EDA is to build the files necessary to generate a physical item.

    I agree with you that getting to that stage would be a part of testing the software. I partly replied to robogary about this here  RE: Would You Be Interested in Roadtesting KiCad EDA? 

    Gough Lui said:
    Without it, given the software is free, what is the incentive for the RoadTester?

    That's why we have the question of what would be expected in a 'kit' for this RoadTest, that would be a part of it.

    I've also considered that we would offer discount code(s) for the online store, or we would order a basket value of parts from the online store.

    And as mentioned, actually fabricating the PCBs. Then there's also being given the platform to share your opinion about the software and for that to be shared.