RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum What Are Your Most Popular Dev Kits or Reference Design Kits?
  • Blogs
  • RoadTest Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 66 replies
  • Subscribers 2652 subscribers
  • Views 6618 views
  • Users 0 members are here
  • What Are Your Most Popular Dev Kits or Reference Design Kits?
Related

What Are Your Most Popular Dev Kits or Reference Design Kits?

rscasny
rscasny over 2 years ago

I was asked this question the other day. What Are Your Most Popular Dev Kits or Reference Design Kits? On impulse, I would venture to say the Raspberry Pi, Beaglebone. I'm sure there are others. Sensor kits, FPGA kits, Motor Contr0ol kits, Power kits, come to mind, but I'm not sure which ones element14 would consider "popular."

So, I figured I would ask you.  What are your most popular kits?  If you have the time, please leave a comment below. 

Thanks

Randall Scasny

-element14 Community

  • Sign in to reply
  • Cancel

Top Replies

  • taifur
    taifur over 2 years ago +4
    Arduino Uno and Raspberry Pi is my favorite.
  • ZGoode
    ZGoode over 2 years ago +3
    Personally, I'm a big fan of any boards that use the standard layouts such as Arduino Uno or Adafruit Feather. As such, the Nucleo boards from STMicro are always great to work with since they are Arduino…
  • misaz
    misaz over 2 years ago +3
    STM32 Nucleos are very popular. I have seen them everywhere where the serious MCUs designs are made. I think that there are two key things for making board popular: Price to performance ratio …
Parents
  • Fred27
    Fred27 over 2 years ago

    I'm not sure I can put my finger on a "most popular" as it all depends on what I'm trying to achieve.

    TI's MSP430 line got me into microcontrollers so I'll always have a soft spot for those. I dipped into Nordic's nRF series for work - I was creating a stand-in for another company's hardware and decided to use the same base for my mock device. I've been a bit on-and-off with those but might well pick that as a go-to if I needed a microcontroller for a project, Either that or a Pico.

    The Raspberry Pi is always good if you need an SBC to run Linux. My team at work are mostly Microsoft based, but .NET Core runs really well on a Pi. However, having to design some new hardware when the Pi was hard to get meant the BeagleBone Black got the job. They're great in certain situations too. (If you're a golf fan and you watched the Ryder Cup recently, it was some BeagleBones that the marshalls were using to switch the enormous on-course video screens between the scoreboard and TV feed.)

    Whilst I was getting into FPGAs, the Xilinx (now AMD) range were great.

    None of these would be good if you picked the wrong one for the job. A microcontroller, SBC and FPGA are all so different.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Fred27
    Fred27 over 2 years ago

    I'm not sure I can put my finger on a "most popular" as it all depends on what I'm trying to achieve.

    TI's MSP430 line got me into microcontrollers so I'll always have a soft spot for those. I dipped into Nordic's nRF series for work - I was creating a stand-in for another company's hardware and decided to use the same base for my mock device. I've been a bit on-and-off with those but might well pick that as a go-to if I needed a microcontroller for a project, Either that or a Pico.

    The Raspberry Pi is always good if you need an SBC to run Linux. My team at work are mostly Microsoft based, but .NET Core runs really well on a Pi. However, having to design some new hardware when the Pi was hard to get meant the BeagleBone Black got the job. They're great in certain situations too. (If you're a golf fan and you watched the Ryder Cup recently, it was some BeagleBones that the marshalls were using to switch the enormous on-course video screens between the scoreboard and TV feed.)

    Whilst I was getting into FPGAs, the Xilinx (now AMD) range were great.

    None of these would be good if you picked the wrong one for the job. A microcontroller, SBC and FPGA are all so different.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • javagoza
    javagoza over 2 years ago in reply to Fred27

    I miss content and challenges with TI development boards on element14. I also got into modern microcontrollers with a TI development board, the ARM Cortex-M4F Based MCU TM4C123G LaunchPad Evaluation Kit with which I took the course UT.6.02x Embedded Systems - Shape the World by Jonathan Valvano and Ramesh Yerraballi: https://users.ece.utexas.edu/~valvano/Volume1/E-Book/

    This was my final project:

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    I then followed the TI Robotics Systems Learning Kit (TI-RSLK) courses with the TI MSP432 LaunchPad: https://university.ti.com/en/faculty/ti-robotics-system-learning-kit/ti-robotics-system-learning-kit/curriculum-design-launch

    I also have several TI MSP430G2553 LaunchPad from when my eldest daughter was studying digital electronics with the MSP430 in PDIP package.

    I have left these development boards aside because I follow what element14 sells. Now my interest is focused on FPGAs and Arduinos.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • BigG
    BigG over 2 years ago in reply to Fred27

    Interesting that you use .NET Core. It is not something that comes up much on Element14. So I stick with Linux OS.

    I have always wondered if any .NET developers use these SBC's and what they're like: https://www.ghielectronics.com/sitcore/sbc/

    I recall their early FEZ dev boards, but they never gained traction in terms of popularity stakes (although I see they have newer options on the website).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Fred27
    Fred27 over 2 years ago in reply to BigG

    I used the .NET MicroFramework in the past and TinyCLR on the Fez seems similar. It was a fun way in to embedded for me at the time, but I wouldn't recommend it now.

    .NET Core on Linux works really well - whether it's on a Pi, BeagleBone or desktop. There are NuGet packages for using GPIO. You can always call into Linux C libraries if you need to, but it's a bit more complex.

    I've recently written code for a touchscreen controller for use in conferences. It has an Electron front end and C# behind. It will run just as well on a Pi with a 7" touchscreen or a Windows PC with a 14" touchscreen monitor. Genuine portability of the code between the two.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • misaz
    misaz over 2 years ago in reply to BigG

    I also run .NET Core apps on Raspberry Pi, but in case of ASP.NET Core webservers I was facing out of memory on Raspberry Pi 3. Now with 4B with 2 GiB and more RAM it is not problem anymore.

    .NET Micro Framework was my begining with IoT. Sadly, the project died. Microsoft currently works on AoT compiler for .NET which may be possibly used in future as a come back to embedded world but as I understand, it is not priority for Microsoft.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • BigG
    BigG over 2 years ago in reply to misaz

    Yes, I remember .NET Micro Framework but never got to try it.

    I have yet to work out the value of using .NET apps in light of Python offering so much more these days. I therefore see .NET as more application specific in terms of a use case.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to javagoza

    Yes. i'm a TI fanboy. They virtually retreated from all communities