RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Seeking Your Interest in Roadtesting a Digital Isolator Board
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 36 replies
  • Subscribers 2745 subscribers
  • Views 5509 views
  • Users 0 members are here
  • digital isolators
  • adi
  • roadtest survey
Related

Seeking Your Interest in Roadtesting a Digital Isolator Board

rscasny
rscasny over 2 years ago

Hi All.

imageI had a call with one of suppliers who is interested in roadtesting one of its digital isolator boards. We have not done much with digital isolators in the roadtest program. But given the need for circuit isolation and the safety they provide, I wanted the community to roadtest this product. In addition, another reason was the learning experience the roadtesters can provide community members on this product.

Here is some basic information on this board:

The evaluation kits are designed to evaluate the MAX22563−MAX22566, a family of reinforced, six-channel, galvanic digital isolators in a 20-pin SSOP package.

Two types of evaluation boards are available:

  • The MAX22565CAEVKIT# is fully assembled and tested, and comes populated with the MAX22565CAAP+ (Not used in this roadtest)
  • The MAX2256XAEVKIT# is a generic board that has U1 unpopulated, allowing to select a device from the MAX22563−MAX22566 family. This is the kit that will be used for this roadtest. The MAX2256XAEVKIT# comes with U1 unpopulated and supports the following digital isolators: MAX22563BAAP+, MAX22563CAAP+, MAX22564BAAP+, MAX22564CAAP+, MAX22565BAAP+, MAX22565CAAP+, MAX22566BAAP+, and MAX22566CAAP+.

imageEquipment needed for roadtesting:

You need some test equipment to roadtest the MAX2256XA EV kit:
• MAX22563−MAX22566 device if U1 is unpopulated on EV kit. (The roadtester and I will get together to order the desired device needed.)
• Two DC power supplies with output range of 1.71V to 5.5V
• Signal/function generator
• Oscilloscope
Note: The EV kit should be powered from two independent isolated power supplies with nominal output voltage in the range from 1.71V to 5.5V. To evaluate the electrical parameters of the device without any isolation between the two sides, a single power supply can also be used.

Element14 would not provide the test equipment.

Roadtesters would need to have the bench equipment for this roadtest. If you are an electronic design engineer, you likely have access to most of these equipment. This seems like a lot to ask, and it is. But I think this is a valuable roadtest to offer the community. The reviews the roadtesters write would not only be good learning experiences, but would also provide customers more than a datasheet to select a digital isolator when the need arises. 

Here's some documentation on the board:

Datasheet
Manufacturer's page

For Additional Information

Here's a couple of polls for which to vote:



  • Sign in to reply
  • Cancel
Parents
  • misaz
    misaz over 2 years ago

    I think the X kit without chip soldered is complication for RoadTest because it need RoadTester to have SMD soldering skills and can introduce several issues to board (cold joint, shorts, unconnected joints). It increases requirements on needed equipment even more and also some faults can affect board performance. MAX22563−MAX22566 differs in direction of channels. I think the MAX22565CAEVKIT with presoldered isolator with 5ch in one direction and 1ch in opposite direction is better choice for RoadTest. And if somebody for some reason need different channel configuration he/she can simply desolder the default chip efficiently turning kit to X variant and proceed with custom chip.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • misaz
    misaz over 2 years ago

    I think the X kit without chip soldered is complication for RoadTest because it need RoadTester to have SMD soldering skills and can introduce several issues to board (cold joint, shorts, unconnected joints). It increases requirements on needed equipment even more and also some faults can affect board performance. MAX22563−MAX22566 differs in direction of channels. I think the MAX22565CAEVKIT with presoldered isolator with 5ch in one direction and 1ch in opposite direction is better choice for RoadTest. And if somebody for some reason need different channel configuration he/she can simply desolder the default chip efficiently turning kit to X variant and proceed with custom chip.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • rscasny
    rscasny over 2 years ago in reply to misaz

    I see your point. But I also see why they "may" have chosen the MAX2256XAEVKIT#. The sponsor makes a range of these chips, so they likely hoped that different roadtests would use different U1s. In addition, if a customer purchased the X version, he would have to determine the chip he needed, which would make them study the sponsor's products more, which would be important to them. In other words, the X version requires more work and simulates the actual customer experience. That's my impression.

    Now, the key question is: can someone solder a 20-pin SSOP with the tools they currently possess? If I hear 'no' from everyone, then I'll have to go back to the sponsor and get the other version of the board. (I have the X versions of the board; I'll have to order the C version.