RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Seeking Your Interest in Roadtesting a Raspberry Pi Add-on Board for developing Ethernet-capable field devices
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 2748 subscribers
  • Views 2728 views
  • Users 0 members are here
  • roadtester survey
  • ANALOG DEVICES EVAL-CN0575-RPIZ
Related

Seeking Your Interest in Roadtesting a Raspberry Pi Add-on Board for developing Ethernet-capable field devices

rscasny
rscasny over 2 years ago

Hi all. It's been awhile since I created a pre-roadtest discussion. It's good to be back. Let me tell you about this product.

As usual. I've been in discussion with a supplier about roadtesting an add-on board for the Raspberry Pi.  Ot's called the EVAL-CN0575-RPIZ. On a nutshell, the CN0575 is a platform for developing Ethernet-capable field devices and applications. More information follows.

I wanted to get your feedback on two questions:

  • What do you need to roadtest it?
  • How interested are you in roadtesting it?

Let me start at the beginning and give you some information about the board:

The EVAL-CN0575-RPIZ is a 10BASE-T1L MAC/PHY interface with Single Pair Power over Ethernet (SPoE) for development of field devices and applications on a Raspberry Pi platform board. The SPoE powered device (PD) and isolated flyback regulator provide 5 V power to the platform board and attached application circuitry. SPoE Class 12 (8.4 W, 24 V nominal) and Class 13 (7.7 W, 55 V nominal) are supported.

Designed for use on the Raspberry Pi platform, the CN0575 hardware features a 40-pin GPIO header, and follows the same mechanical dimensions as a standard HAT.

To allow board stacking and development of field device applications using Raspberry Pi HATs, an additional GPIO header with extended leads is included with each evaluation board. However, the CN0575 can also be used on its own as a basic temperature sensing field device with remote user input/output via an onboard button and LED.

image image image

Here is the documentation:

Datasheet

Circuit Notes

User Guide

For More Information

What do you need to roadtest this product?

I was reading through the circuit evaluation section of the user guide. It says that one needs the following equipment for testing:

  • EVAL-CN0575-RPIZ
  • EVAL-ADIN1100-EBZ
  • 24 V (Class 12) or 55 V (Class 13) power supply
  • Raspberry Pi computer (Model 3B+ or above)
  • Host PC (Windows/Linux/Mac)
  • CN0575 demo Python script
  • Plug-in screw-terminal connector
  • Single-pair of 18 AWG (max) wires
  • Category 5e Ethernet cable with RJ45 connectors
  • USB-A to micro-USB-B cable

Seems like a lot of gear. Do you need all this hardware or can you test it another way? I'm trying to determine what I would need to provide beyond the EVAL-CN0575-RPIZ.

Prospective RoadTest Poll

  • Sign in to reply
  • Cancel
Parents
  • BigG
    BigG over 2 years ago

    Those Single Pair Ethernet (Patch) cables are not cheap, and would not be something that I would commonly use like a standard cat5e/cat6 patch cable. For example, the ones from Phoenix Contact are around +$12 for a 1 metre and +$16 for a 2 metre cable

    https://www.phoenixcontact.com/en-ie/products/data-cable-preassembled-spe-t1-ccp-sf20awg22ccp-sf-1183808

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • JWx
    JWx over 2 years ago in reply to BigG

    If I understand correctly, twisted pair can be connected to the screwed green connector - eliminating the need of special cable...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • JWx
    JWx over 2 years ago in reply to BigG

    If I understand correctly, twisted pair can be connected to the screwed green connector - eliminating the need of special cable...