RoadTests & Reviews
  • Products & Partners
  • More
RoadTests & Reviews
RoadTest Forum Seeking Your Opinion - Which Version of the Arduino Opta Micro-PLC Would You Prefer to Roadtest
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 13 replies
  • Subscribers 2741 subscribers
  • Views 4051 views
  • Users 0 members are here
  • roadtester survey
  • micro-PLC
  • industrial automation
  • Opta
  • arduino
Related

Seeking Your Opinion - Which Version of the Arduino Opta Micro-PLC Would You Prefer to Roadtest

rscasny
rscasny over 2 years ago

imageHi All. I will be roadtesting Arduino's micro-PLC, the Opta, in the near future.

Arduino has been expanding its industrial automation product offerings in the last few years and the Opta fits right into that.

If this is your first exposure to the Opta, let me give you a few facts.

Fact 1 - The Opta is a micro PLC with Industrial IoT capabilities, supporting Arduino programming experience and PLC standard languages. Its STM32H747XI dual-core Arm® Cortex®-M7 +M4 MCU allows users to perform real-time control, monitoring and implement predictive maintenance.

Fact 2 - Secure and durable by design, it supports OTA firmware updates and ensures data security from the hardware to the Cloud thanks to the onboard secure element and X.509 Standard compliance. Various connectivity options are available, along with real-time dashboards combined with the Arduino Cloud (or third-party services).

There are three versions of the Opta:

  • Opta Lite
  • Opta RS485 
  • OptaWiFi 

Poll - Preferred Features



Here is some documentation:

  • Datasheet 
  • Pinout 
  • User Manual 
  • Arduino PLC IDE
  • Tutorials 

Poll - Preferred Variant

Invitation to Comment

If you have the time, I'd like to learn how you would apply this micro-PLC. Just a paragraph would do. Thanks.

  • Sign in to reply
  • Cancel
  • mhd720
    mhd720 over 2 years ago

    Lite is more than sufficient, but RS-485 would be neat. Wifi is not industrial ;)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • tarna
    tarna over 2 years ago

    I am building an automated egg incubator and hatchery for my farm, I have started my project using a standard stc-3028 module which is both limited on switching outputs but also in programmability and continuous calibration. This would answer all of my problems. With the benefit of OTA updates and remote monitoring ootb. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Morgan-Hastings
    Morgan-Hastings over 2 years ago

    I teach at a Trade School for electricians and engineers. I’m looking for a simple, but capable PLC platform to teach the IEC 61131 languages on both Mac and windows PCs that won’t bankrupt my school.

    personally I have plans to set up scale industrial machine models and demonstrate how PLCs can simplify control arrangements.

    i would be honoured to test and review the Opta PLCs.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • embeddedguy
    embeddedguy over 2 years ago

    I would like to work on OTA update feature of the Arduino. Perhaps it is with Arduino Cloud that one can update the firmware remotely.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • vlasov01
    vlasov01 over 2 years ago

    It can be a great controller for a pool motor and salt chlorinator to reduce energy consumption. In addition, it can monitor the health of the motor by detecting anomalies (sound, temperature, vibration)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • balajivan1995
    balajivan1995 over 2 years ago

    Dual core STM32 sounds fun until you realize you have to create independent applications for CM4 core and CM7 core. You have to make sure both cores wake up one after another. Inter processor communication is not as easy as implemented by ESP32 which has modified the Freertos to suit its purpose. You will have to learn how to incorporate Openamp or ring buffer to share messages between the core. Hope Arduino has abstracted all these hard part.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • robogary
    robogary over 2 years ago

    Interface to a VFD using field bus with a little bit of io as a cost reduction exercise 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 2 years ago

    for me easily the most intriguing aspect of these products is the marriage of Arduino programming to PLC applications. Since I am familiar with PLC technology and concepts as well as Arduino IDE, it would be interesting to explore their synergy.

    However I don't have any immediate plans for that level of infrastructure around my house. Maybe if I had the resources to design a completely self-sufficient habitat / eco system I would be all over this.

    At work I am on the development end of things rather than the automated production end of things, so it isn't my main focus there either.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • kmikemoo
    kmikemoo over 2 years ago

    RS485 read of MODBUS registers and display on a webserver for monitoring equipment status from multiple points on an intranet.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • DAB
    DAB over 2 years ago

    Interesting device with a lot of capabilities.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>