RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Seeking Your Feedback on RoadTesting an e-Fuse IC Eval Kit
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 14 replies
  • Subscribers 2745 subscribers
  • Views 3196 views
  • Users 0 members are here
  • roadtest survey
Related

Seeking Your Feedback on RoadTesting an e-Fuse IC Eval Kit

rscasny
rscasny over 2 years ago

imageWhen I was first approached about roadtesting an e-Fuse Eval kit, I had the following thought bubble up from deep in my mind: Why would we roadtest a fuse?

Then, I went to dear Google and asked it about the growth of e-Fuses. I'm not going to quote any particular study, but the use of e-Fuses is growing considerably.

So, I agreed to the roadtest because e-Fuses have a lot of tech in them for their size and I feel the community should explore them. Perhaps even compare them to ye old fashioned trip-wire fuse. It's perhaps something a new member, first time roadtester, or the curious-at-heart would be interested in spending some "quality" time with.

In any event, I wanted to get your thoughts on roadtesting e-Fuses.

Here's some facts about the product:

EVB-TCKE805NA is a TCKE805NAe-Fuse IC evaluation board (EVB). It is an evaluation board for supporting TCKE8xx series-design. The passive components required to operate IC are mounted, enabling easy operation check and characterization. The evaluation board features:
• Input voltage range from 4.4V to 18V
• Output limit current range from 0.5A to 5.0A adjustable
• Adjustable slew rate
• Active high enable control
• Auto retry function
• Auto discharge
• Available in 3x3mm WSON10B package

Here's the schematic

image

Here's the documentation:

Instruction Manual

Here's my poll:

  • Sign in to reply
  • Cancel
Parents
  • rsc
    rsc over 2 years ago

    I could see adding one of these to a raspberry pi project for both the fuse and on/off functions.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rsc
    rsc over 2 years ago

    I could see adding one of these to a raspberry pi project for both the fuse and on/off functions.