RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Seeking Your Interest in RoadTesting an IR light angle sensor board
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 14 replies
  • Subscribers 2745 subscribers
  • Views 2963 views
  • Users 0 members are here
  • roadtester poll
Related

Seeking Your Interest in RoadTesting an IR light angle sensor board

rscasny
rscasny over 2 years ago

imageI have had a conversation with a supplier interesting in having the element14 community roadtest its IR light angle sensor board. I don't recall us previously roadtesting this type of sensor (or at least recently within the past year), so let me give you a few facts about it.

If you have the time to explore the device, I'd appreciate you voting in my poll below. Of course, you are free to leave a comment. Many thinks.

Randall
element14 Community Team

Here's a few facts about the board:

EVAL-ADPD2140Z is an evaluation kit to evaluate the ADPD2140 IR light angle sensor, collect data from the ADPD2140, and evaluate gesture recognition and triangulation capabilities. The evaluation kit requires the EVAL-ADPDM3Z evaluation board and the Applications Wavetool, a graphical user interface (GUI) that provides users with low level and high level configurability, real-time data analysis, and user datagram protocol (UDP) transfer capability, which allows the EVAL-ADPDM3Z evaluation board to interface to a PC. The USB port of the PC powers the EVAL-ADPDM3Z evaluation board and provides power to the EVAL-ADPD2140Z evaluation board. On-board voltage regulators provide voltage supplies for the ADPD2140.

Here's some documentation

  • UG-1358: ADPD2140 Evaluation Board User Guide
  • UG-1282: EVAL-ADPDM3Z Evaluation Board User Guide
  • Reference Design CN0569 Infrared Gesture Recognition Module

Here's the poll:

  • Sign in to reply
  • Cancel
Parents
  • embeddedguy
    embeddedguy over 2 years ago

    Interesting sensor and new technology. But still there is not a possibility to use it with microcontroller of  our choice. Also, there is only software that is available to download and "Just evaluate" the sensor as it is. Hence, I voted with No.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 2 years ago in reply to embeddedguy

    The sensor board has I2C and supply connections, to allow it to be connected to other hardware instead of the supplied microcontroller board, to allow users to develop their own code.

    But, it may require a level converter (I believe the voltages levels are 1.8V).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 2 years ago in reply to embeddedguy

    The sensor board has I2C and supply connections, to allow it to be connected to other hardware instead of the supplied microcontroller board, to allow users to develop their own code.

    But, it may require a level converter (I believe the voltages levels are 1.8V).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • embeddedguy
    embeddedguy over 2 years ago in reply to shabaz

    Oh, Now I see, there is SCL visible on the board in the image above. Thanks